<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Semaphore Usage in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/Semaphore-Usage/m-p/986162#M1335</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking in the FreeRTOS example from the S32K144 every time I tried to use a semaphore if it's one of the LPUART RTOS handler or one created in the code, every time I need to call for a &lt;EM&gt;takeSemaphore&amp;nbsp;&lt;/EM&gt;the code redirects to the API&amp;nbsp;&lt;EM&gt;vPortRaiseBASEPRI,&amp;nbsp;&lt;/EM&gt;does anyone know the correct usage of semaphores or the reason why this function is being called?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the Freertos example from SDK 3.0.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Mar 2020 20:15:30 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2020-03-18T20:15:30Z</dc:date>
    <item>
      <title>Semaphore Usage</title>
      <link>https://community.nxp.com/t5/S32-SDK/Semaphore-Usage/m-p/986162#M1335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking in the FreeRTOS example from the S32K144 every time I tried to use a semaphore if it's one of the LPUART RTOS handler or one created in the code, every time I need to call for a &lt;EM&gt;takeSemaphore&amp;nbsp;&lt;/EM&gt;the code redirects to the API&amp;nbsp;&lt;EM&gt;vPortRaiseBASEPRI,&amp;nbsp;&lt;/EM&gt;does anyone know the correct usage of semaphores or the reason why this function is being called?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the Freertos example from SDK 3.0.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 20:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Semaphore-Usage/m-p/986162#M1335</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-03-18T20:15:30Z</dc:date>
    </item>
    <item>
      <title>Re: Semaphore Usage</title>
      <link>https://community.nxp.com/t5/S32-SDK/Semaphore-Usage/m-p/986163#M1336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have figured about what was wrong about this error, this happens due to the lack of heap and stack of the&amp;nbsp;task, so to avoid this increment the&amp;nbsp;configMINIMAL_STACK_SIZE and the Total heap size&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/101339iBB05CF32B7CF18D3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Mar 2020 20:49:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Semaphore-Usage/m-p/986163#M1336</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-03-31T20:49:56Z</dc:date>
    </item>
  </channel>
</rss>