<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックVSDK 1.3 does not compile with Linux 4.19</title>
    <link>https://community.nxp.com/t5/S32-SDK/VSDK-1-3-does-not-compile-with-Linux-4-19/m-p/953443#M1206</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello I recently tried to compile the BSP 22.0 with the recommended Yocto Setup (Debian 4.9.168) for the S32V234-sbc with VSDK extensions and the build fails for the sequencer recipe. The error log is attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I fixed this with this and created the attached patch. The question is, how do I verify that my changes are correct. Are there tests I can run which will verify the functionality of the sequencer?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Sep 2019 11:55:36 GMT</pubDate>
    <dc:creator>gert-janrozing</dc:creator>
    <dc:date>2019-09-05T11:55:36Z</dc:date>
    <item>
      <title>VSDK 1.3 does not compile with Linux 4.19</title>
      <link>https://community.nxp.com/t5/S32-SDK/VSDK-1-3-does-not-compile-with-Linux-4-19/m-p/953443#M1206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello I recently tried to compile the BSP 22.0 with the recommended Yocto Setup (Debian 4.9.168) for the S32V234-sbc with VSDK extensions and the build fails for the sequencer recipe. The error log is attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I fixed this with this and created the attached patch. The question is, how do I verify that my changes are correct. Are there tests I can run which will verify the functionality of the sequencer?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2019 11:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/VSDK-1-3-does-not-compile-with-Linux-4-19/m-p/953443#M1206</guid>
      <dc:creator>gert-janrozing</dc:creator>
      <dc:date>2019-09-05T11:55:36Z</dc:date>
    </item>
  </channel>
</rss>