<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32 DS auto rename the output flash image? in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32-DS-auto-rename-the-output-flash-image/m-p/953088#M1202</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see - I didn't get that you like to add time stamp into file name - sorry. So, in this case - you need to add your commands into shell script - in attachment. Copy script into folder where your&amp;nbsp; .elf file is generated (for example Debug_FLASH) and add script and project name as an argument into post build steps:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64860i180507D4875F133A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After build you can find .srec file like this:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65168iFFB5A94565BA8478/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Oct 2019 10:54:29 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2019-10-08T10:54:29Z</dc:date>
    <item>
      <title>S32 DS auto rename the output flash image?</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-DS-auto-rename-the-output-flash-image/m-p/953085#M1199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I want to rename the flash image file's name after build the project. I find that in project settings, Build Steps menu have post-build steps command. But I can't find the format of the command, or introduce of this function.&lt;/P&gt;&lt;P&gt;The format of the flash image is "ProjectName"_"BuildTime".s19, such as MotorDriver_20190228_221006.s19.&lt;/P&gt;&lt;P&gt;Could you help me?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Oct 2019 14:29:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-DS-auto-rename-the-output-flash-image/m-p/953085#M1199</guid>
      <dc:creator>cg0</dc:creator>
      <dc:date>2019-10-07T14:29:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS auto rename the output flash image?</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-DS-auto-rename-the-output-flash-image/m-p/953086#M1200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately there is a bug (already logged) - post build steps are executed prior s-record file is generated. You can generate s-record with your own name in post build step:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56466i7A82642EF8FB0951/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 08:32:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-DS-auto-rename-the-output-flash-image/m-p/953086#M1200</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-10-08T08:32:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS auto rename the output flash image?</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-DS-auto-rename-the-output-flash-image/m-p/953087#M1201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jiri&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;           It works. but the name now can only be fixed name or use $&lt;SPAN __jive_macro_name="ProjName"&gt;&lt;/SPAN&gt; which still is a fixed name.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;           Could the file name auto changed according to the date and time when build the project? although the will lead the file big, but it can be under control.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 08:56:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-DS-auto-rename-the-output-flash-image/m-p/953087#M1201</guid>
      <dc:creator>cg0</dc:creator>
      <dc:date>2019-10-08T08:56:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS auto rename the output flash image?</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-DS-auto-rename-the-output-flash-image/m-p/953088#M1202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see - I didn't get that you like to add time stamp into file name - sorry. So, in this case - you need to add your commands into shell script - in attachment. Copy script into folder where your&amp;nbsp; .elf file is generated (for example Debug_FLASH) and add script and project name as an argument into post build steps:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64860i180507D4875F133A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After build you can find .srec file like this:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65168iFFB5A94565BA8478/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 10:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-DS-auto-rename-the-output-flash-image/m-p/953088#M1202</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-10-08T10:54:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS auto rename the output flash image?</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-DS-auto-rename-the-output-flash-image/m-p/953089#M1203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello Jiri&lt;/P&gt;&lt;P&gt;           Thanks a lot. Yes, this is what I want to achieve.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Oct 2019 02:03:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-DS-auto-rename-the-output-flash-image/m-p/953089#M1203</guid>
      <dc:creator>cg0</dc:creator>
      <dc:date>2019-10-09T02:03:23Z</dc:date>
    </item>
  </channel>
</rss>