<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flexio_I2C_Non_Blocking problem in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/Flexio-I2C-Non-Blocking-problem/m-p/929780#M1109</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I'm working on S32_116 target specially with I2C Flexio peripheral and I have a confusion about I2C Non-Blocking driver.as I have read Doxygen Documentation of this module there's two types of Transmission,Blocking and Non-Blocking and I want to use the Non-Blocking one.so there's an API called "MasterGetStatus" as described in documentation this API must be called once at least to send a byte but when I call it once after Calling API "MasterSendData" and watching the Bus on Digital analyzer it turns out that it sends a bit or something weird.&lt;/P&gt;&lt;P&gt;so my Question is what Exactly This API "MasterGetStatus" did if it's Called once ,cause after testing it turns out that it didn't send a byte at all and what If i want to call "masterGetStatus" in a periodic task every 8ms to handle the transmission cause I have tried it also but the transmission Failed.&lt;/P&gt;&lt;P&gt;Thank you&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Oct 2019 08:35:49 GMT</pubDate>
    <dc:creator>mohamed_ahmed-a</dc:creator>
    <dc:date>2019-10-17T08:35:49Z</dc:date>
    <item>
      <title>Flexio_I2C_Non_Blocking problem</title>
      <link>https://community.nxp.com/t5/S32-SDK/Flexio-I2C-Non-Blocking-problem/m-p/929780#M1109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I'm working on S32_116 target specially with I2C Flexio peripheral and I have a confusion about I2C Non-Blocking driver.as I have read Doxygen Documentation of this module there's two types of Transmission,Blocking and Non-Blocking and I want to use the Non-Blocking one.so there's an API called "MasterGetStatus" as described in documentation this API must be called once at least to send a byte but when I call it once after Calling API "MasterSendData" and watching the Bus on Digital analyzer it turns out that it sends a bit or something weird.&lt;/P&gt;&lt;P&gt;so my Question is what Exactly This API "MasterGetStatus" did if it's Called once ,cause after testing it turns out that it didn't send a byte at all and what If i want to call "masterGetStatus" in a periodic task every 8ms to handle the transmission cause I have tried it also but the transmission Failed.&lt;/P&gt;&lt;P&gt;Thank you&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Oct 2019 08:35:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Flexio-I2C-Non-Blocking-problem/m-p/929780#M1109</guid>
      <dc:creator>mohamed_ahmed-a</dc:creator>
      <dc:date>2019-10-17T08:35:49Z</dc:date>
    </item>
    <item>
      <title>Re: Flexio_I2C_Non_Blocking problem</title>
      <link>https://community.nxp.com/t5/S32-SDK/Flexio-I2C-Non-Blocking-problem/m-p/929781#M1110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;It seems to be already answered here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/515437"&gt;FLexIO_I2C_Driver problem&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2019 11:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Flexio-I2C-Non-Blocking-problem/m-p/929781#M1110</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-11-13T11:29:43Z</dc:date>
    </item>
  </channel>
</rss>