<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックVisionSDK_S32V2_RTM_1_3_0 problems</title>
    <link>https://community.nxp.com/t5/S32-SDK/VisionSDK-S32V2-RTM-1-3-0-problems/m-p/924957#M1090</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While reading VisionSDK_S32V2_RTM_1_3_0 userguide. Some questions occurred at 3.3.1 and 3.3.2.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.3.1 General Preparation&lt;BR /&gt;Export necessary environment variables:&lt;BR /&gt;o export ARCH=arm&lt;BR /&gt;▪ Target architecture&lt;BR /&gt;o export CROSS_COMPILE=aarch64-linux-gnu-&lt;BR /&gt;▪ Compiler prefix specification&lt;BR /&gt;o export LINUX_S32V234_DIR=/linux/sources/directory/for/s32v234/&amp;nbsp; &amp;nbsp; //THIS ONEEEEEEEEEEE&amp;nbsp;&amp;nbsp;&lt;BR /&gt;▪ optional, only for s32v234 Linux build&lt;BR /&gt;▪ Path to the Linux sources (same kernel as is running on the board)&lt;BR /&gt;o export PATH=/path/to/your/compiler/binaries:$PATH&amp;nbsp; //THIS ONEEEEEEE&lt;BR /&gt;▪ Path to the compiler binaries&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can some one give me an real example?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.3.2 Building the Kernel Modules&lt;BR /&gt;Following kernel modules can be built:&lt;BR /&gt;• apex.ko:&lt;BR /&gt;s32v234_sdk/libs/apex/drivers/kernel/build-v234ce-gnu-linux-d&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I got this&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;'' Please define LINUX_S32V234_DIR pointing to kernel directory . ''&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If it the same thing as 3.3.1 , a real example plz.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jul 2019 08:44:06 GMT</pubDate>
    <dc:creator>alan13341313</dc:creator>
    <dc:date>2019-07-16T08:44:06Z</dc:date>
    <item>
      <title>VisionSDK_S32V2_RTM_1_3_0 problems</title>
      <link>https://community.nxp.com/t5/S32-SDK/VisionSDK-S32V2-RTM-1-3-0-problems/m-p/924957#M1090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While reading VisionSDK_S32V2_RTM_1_3_0 userguide. Some questions occurred at 3.3.1 and 3.3.2.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.3.1 General Preparation&lt;BR /&gt;Export necessary environment variables:&lt;BR /&gt;o export ARCH=arm&lt;BR /&gt;▪ Target architecture&lt;BR /&gt;o export CROSS_COMPILE=aarch64-linux-gnu-&lt;BR /&gt;▪ Compiler prefix specification&lt;BR /&gt;o export LINUX_S32V234_DIR=/linux/sources/directory/for/s32v234/&amp;nbsp; &amp;nbsp; //THIS ONEEEEEEEEEEE&amp;nbsp;&amp;nbsp;&lt;BR /&gt;▪ optional, only for s32v234 Linux build&lt;BR /&gt;▪ Path to the Linux sources (same kernel as is running on the board)&lt;BR /&gt;o export PATH=/path/to/your/compiler/binaries:$PATH&amp;nbsp; //THIS ONEEEEEEE&lt;BR /&gt;▪ Path to the compiler binaries&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can some one give me an real example?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.3.2 Building the Kernel Modules&lt;BR /&gt;Following kernel modules can be built:&lt;BR /&gt;• apex.ko:&lt;BR /&gt;s32v234_sdk/libs/apex/drivers/kernel/build-v234ce-gnu-linux-d&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I got this&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;'' Please define LINUX_S32V234_DIR pointing to kernel directory . ''&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If it the same thing as 3.3.1 , a real example plz.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 08:44:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/VisionSDK-S32V2-RTM-1-3-0-problems/m-p/924957#M1090</guid>
      <dc:creator>alan13341313</dc:creator>
      <dc:date>2019-07-16T08:44:06Z</dc:date>
    </item>
    <item>
      <title>Re: VisionSDK_S32V2_RTM_1_3_0 problems</title>
      <link>https://community.nxp.com/t5/S32-SDK/VisionSDK-S32V2-RTM-1-3-0-problems/m-p/924958#M1091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On my Linux machine, I have the kernel provided by Automotive BSP in &lt;BR /&gt;this directory:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/home/adas/work/S32V/BSP/21.0/build_s32v234sbc/tmp/work/s32v234sbc-fsl-linux/linux-s32/4.19-r0/git/&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so LINUX_S32V234_DIR shell variable assignment will look like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;export LINUX_S32V234_DIR=/home/adas/work/S32V/BSP/21.0/build_s32v234sbc/tmp/work/s32v234sbc-fsl-linux/linux-s32/4.19-r0/git/&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;VSDK installed the tools for Linux target to&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/home/adas/work/S32V/VisionSDK_S32V2_RTM_1_3_0_HF1/compilers/gcc-6.3.1-linaro-Xarmv8-linux/i686-linux/bin/&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;VSDK installer updates your ~/.profile automatically so all tools&lt;BR /&gt;should be there in your PATH. You need to update it manually only &lt;BR /&gt;if you have broken your environment:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;export PATH=/home/adas/work/S32V/VisionSDK_S32V2_RTM_1_3_0_HF1/compilers/gcc-6.3.1-linaro-Xarmv8-linux/i686-linux/bin:$PATH&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note, merely copying this to your machine is unlikely to work since the&lt;BR /&gt;exact paths depend on where and how you installed various packages and, if you are working with Yocto,&lt;BR /&gt;what you specified after -m to&amp;nbsp; nxp-setup-alb.sh&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jul 2019 11:17:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/VisionSDK-S32V2-RTM-1-3-0-problems/m-p/924958#M1091</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2019-07-25T11:17:15Z</dc:date>
    </item>
  </channel>
</rss>