<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックQuestions about receiving various CAN Msgs</title>
    <link>https://community.nxp.com/t5/S32-SDK/Questions-about-receiving-various-CAN-Msgs/m-p/909356#M1008</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are considering using multiple MAILBOXs to handle the received Multi CAN Msg.&lt;BR /&gt;However, the test result shows that MAILBOX (0,1) with maximum 2ea including Tx/Rx can be used and 'STATUS_CAN_BUFF_OUT_OF_RANGE' is generated when using more than this.&lt;BR /&gt;ex) &lt;BR /&gt;#define RX_BUFF_IDX 0U, #define TX_BUFF_IDX 1U - ok&lt;BR /&gt;#define RX_BUFF_IDX 0U, #define RX_BUFF_IDX_2 1U - ok&lt;BR /&gt;#define RX_BUFF_IDX 0U, #define RX_BUFF_IDX_2 1U, #define RX_BUFF_IDX_3 2U - fail&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I receive various CAN Msgs?&lt;BR /&gt;I was refer to example code of can_pal_s32k144&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 May 2019 07:30:37 GMT</pubDate>
    <dc:creator>jm_shin</dc:creator>
    <dc:date>2019-05-27T07:30:37Z</dc:date>
    <item>
      <title>Questions about receiving various CAN Msgs</title>
      <link>https://community.nxp.com/t5/S32-SDK/Questions-about-receiving-various-CAN-Msgs/m-p/909356#M1008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are considering using multiple MAILBOXs to handle the received Multi CAN Msg.&lt;BR /&gt;However, the test result shows that MAILBOX (0,1) with maximum 2ea including Tx/Rx can be used and 'STATUS_CAN_BUFF_OUT_OF_RANGE' is generated when using more than this.&lt;BR /&gt;ex) &lt;BR /&gt;#define RX_BUFF_IDX 0U, #define TX_BUFF_IDX 1U - ok&lt;BR /&gt;#define RX_BUFF_IDX 0U, #define RX_BUFF_IDX_2 1U - ok&lt;BR /&gt;#define RX_BUFF_IDX 0U, #define RX_BUFF_IDX_2 1U, #define RX_BUFF_IDX_3 2U - fail&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I receive various CAN Msgs?&lt;BR /&gt;I was refer to example code of can_pal_s32k144&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2019 07:30:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Questions-about-receiving-various-CAN-Msgs/m-p/909356#M1008</guid>
      <dc:creator>jm_shin</dc:creator>
      <dc:date>2019-05-27T07:30:37Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about receiving various CAN Msgs</title>
      <link>https://community.nxp.com/t5/S32-SDK/Questions-about-receiving-various-CAN-Msgs/m-p/909357#M1009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;try to increase number of available MBs in CAN component inspector.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83907i80DC50E8B8F1B864/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2019 11:40:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Questions-about-receiving-various-CAN-Msgs/m-p/909357#M1009</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-05-27T11:40:03Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about receiving various CAN Msgs</title>
      <link>https://community.nxp.com/t5/S32-SDK/Questions-about-receiving-various-CAN-Msgs/m-p/909358#M1010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Petr Stancik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for quick response.&lt;BR /&gt;I increased the&amp;nbsp;'Number of buffers' as shown below but the problem was not resolved. (2-&amp;gt;8)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83933iBD4D75E9C5385922/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;We still return the same 'STATUS_CAN_BUFF_OUT_OF_RANGE' state when MAILBOX (0,1) with over 2ea including Tx/Rx be used.&lt;/P&gt;&lt;P&gt;Could you please guide to solving this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 00:16:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Questions-about-receiving-various-CAN-Msgs/m-p/909358#M1010</guid>
      <dc:creator>jm_shin</dc:creator>
      <dc:date>2019-05-28T00:16:58Z</dc:date>
    </item>
  </channel>
</rss>