<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32DS erases everything in the output folder when building the project in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-erases-everything-in-the-output-folder-when-building-the/m-p/1590195#M9688</link>
    <description>&lt;P&gt;Hi guys, how can I turn off the feature in S32DS that erases everything in the output folder when building the project as I have some files there like the bootloader hex file and the tools that merge the bootloader with the application hex file and it is really not convenient to copy them back every time?&lt;/P&gt;&lt;P&gt;Thanks in advance for the help&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 31 Jan 2023 02:39:53 GMT</pubDate>
    <dc:creator>jimd2023</dc:creator>
    <dc:date>2023-01-31T02:39:53Z</dc:date>
    <item>
      <title>S32DS erases everything in the output folder when building the project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-erases-everything-in-the-output-folder-when-building-the/m-p/1590195#M9688</link>
      <description>&lt;P&gt;Hi guys, how can I turn off the feature in S32DS that erases everything in the output folder when building the project as I have some files there like the bootloader hex file and the tools that merge the bootloader with the application hex file and it is really not convenient to copy them back every time?&lt;/P&gt;&lt;P&gt;Thanks in advance for the help&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 31 Jan 2023 02:39:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-erases-everything-in-the-output-folder-when-building-the/m-p/1590195#M9688</guid>
      <dc:creator>jimd2023</dc:creator>
      <dc:date>2023-01-31T02:39:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS erases everything in the output folder when building the project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-erases-everything-in-the-output-folder-when-building-the/m-p/1599009#M9740</link>
      <description>&lt;P&gt;Hello Jim,&lt;/P&gt;
&lt;P&gt;If you are referring to the folder 'Debug_RAM', for example, then only the files which are a product of the build are erased and replaced. If you rename the files they should remain in the folder.&lt;/P&gt;
&lt;P&gt;What version of S32DS are you using?&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Tue, 14 Feb 2023 16:52:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-erases-everything-in-the-output-folder-when-building-the/m-p/1599009#M9740</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2023-02-14T16:52:46Z</dc:date>
    </item>
  </channel>
</rss>