<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックSimulink - RAppID bootloader</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Simulink-RAppID-bootloader/m-p/1585489#M9669</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a question&lt;BR /&gt;I'm using the RAppID bootloader tool to program, by CAN, the MPC5744P micro-controller. Simulink demos and examples are working correctly. However, some models doesn't start when programming them using the bootloader. The Code got struck in the bootloader sector, which starts at address 0x00F98000, and doesn't jump to the application. these models use some logic and APIs implemented in C and get imported in the Simulink model.&lt;/P&gt;&lt;P&gt;Why does this behavior happen? and Are there any configurations or concerns needed when using the RAppID bootloader ??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Sun, 22 Jan 2023 09:38:37 GMT</pubDate>
    <dc:creator>abdelrhman</dc:creator>
    <dc:date>2023-01-22T09:38:37Z</dc:date>
    <item>
      <title>Simulink - RAppID bootloader</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Simulink-RAppID-bootloader/m-p/1585489#M9669</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a question&lt;BR /&gt;I'm using the RAppID bootloader tool to program, by CAN, the MPC5744P micro-controller. Simulink demos and examples are working correctly. However, some models doesn't start when programming them using the bootloader. The Code got struck in the bootloader sector, which starts at address 0x00F98000, and doesn't jump to the application. these models use some logic and APIs implemented in C and get imported in the Simulink model.&lt;/P&gt;&lt;P&gt;Why does this behavior happen? and Are there any configurations or concerns needed when using the RAppID bootloader ??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Sun, 22 Jan 2023 09:38:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Simulink-RAppID-bootloader/m-p/1585489#M9669</guid>
      <dc:creator>abdelrhman</dc:creator>
      <dc:date>2023-01-22T09:38:37Z</dc:date>
    </item>
  </channel>
</rss>