<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Create bare metal code for LED blinking on S32K144 using the S32DS . in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Create-bare-metal-code-for-LED-blinking-on-S32K144-using-the/m-p/1576108#M9581</link>
    <description>&lt;P&gt;I have tried same code using provided sample code , it is working.&lt;/P&gt;&lt;P&gt;I want to create new project in the S32 DS without using the example code for for the blinking LED.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 02 Jan 2023 13:23:18 GMT</pubDate>
    <dc:creator>VW</dc:creator>
    <dc:date>2023-01-02T13:23:18Z</dc:date>
    <item>
      <title>Create bare metal code for LED blinking on S32K144 using the S32DS .</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Create-bare-metal-code-for-LED-blinking-on-S32K144-using-the/m-p/1576108#M9581</link>
      <description>&lt;P&gt;I have tried same code using provided sample code , it is working.&lt;/P&gt;&lt;P&gt;I want to create new project in the S32 DS without using the example code for for the blinking LED.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jan 2023 13:23:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Create-bare-metal-code-for-LED-blinking-on-S32K144-using-the/m-p/1576108#M9581</guid>
      <dc:creator>VW</dc:creator>
      <dc:date>2023-01-02T13:23:18Z</dc:date>
    </item>
    <item>
      <title>Re: Create bare metal code for LED blinking on S32K144 using the S32DS .</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Create-bare-metal-code-for-LED-blinking-on-S32K144-using-the/m-p/1576167#M9584</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210639"&gt;@VW&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Take a look to the&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5413.pdf" target="_blank" rel="noopener"&gt;S32K1xx Series Cookbook&lt;/A&gt;, this will be useful for you.&amp;nbsp;&lt;/P&gt;
&lt;DIV class="body taskbody"&gt;
&lt;DIV class="section context"&gt;
&lt;P class="p"&gt;To create a new project in S32DS&amp;nbsp;&lt;SPAN&gt;without using an example&lt;/SPAN&gt;:&lt;/P&gt;
&lt;OL&gt;
&lt;LI class="p"&gt;Click File &amp;gt; New &amp;gt; S32DS Application Project or S32DS Library Project on the menu bar.The first page of the wizard appears.&lt;/LI&gt;
&lt;LI class="p"&gt;Specify the name of the new project in the Project name text box.&amp;nbsp;Note: The Location field shows the default project location. If youwant to change this location, clear the Use default location checkbox, click Browse and specify a different location.Click OK.&lt;/LI&gt;
&lt;LI class="p"&gt;Select the target processor from the Processors panel.&lt;/LI&gt;
&lt;LI class="p"&gt;Click Next. The second page of the wizard appears.&lt;/LI&gt;
&lt;LI class="p"&gt;Check the project settings, select the cores and parameters. Click Finish. The new project appears in the Project Explorer view. Note: Thewizard creates one or multiple projects, depending on the number of selectedcores.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;</description>
      <pubDate>Mon, 02 Jan 2023 18:31:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Create-bare-metal-code-for-LED-blinking-on-S32K144-using-the/m-p/1576167#M9584</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-01-02T18:31:15Z</dc:date>
    </item>
    <item>
      <title>Re: Create bare metal code for LED blinking on S32K144 using the S32DS .</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Create-bare-metal-code-for-LED-blinking-on-S32K144-using-the/m-p/1576304#M9586</link>
      <description>&lt;P&gt;Thank you for the inputs.&lt;/P&gt;&lt;P&gt;I will check with your provided inputs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jan 2023 04:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Create-bare-metal-code-for-LED-blinking-on-S32K144-using-the/m-p/1576304#M9586</guid>
      <dc:creator>VW</dc:creator>
      <dc:date>2023-01-03T04:30:57Z</dc:date>
    </item>
  </channel>
</rss>