<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: s32k314 qspi sample code</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/s32k314-qspi-sample-code/m-p/1569979#M9542</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210023"&gt;@vasanth-sr&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;At this point in time, S32DS 3.5 is not broadly supported on the S32K3 family.&amp;nbsp;We do recommend to stay at version 3.4 until further notice.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
    <pubDate>Wed, 14 Dec 2022 21:12:23 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2022-12-14T21:12:23Z</dc:date>
    <item>
      <title>s32k314 qspi sample code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/s32k314-qspi-sample-code/m-p/1569578#M9541</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;how can i get the sample code of Qspi for s32k3xx.&lt;/P&gt;&lt;P&gt;i imported the s32k344 sample code from the RTD 2.0.1,But i am not able to add the peripheral's&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;vasanth.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 09:36:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/s32k314-qspi-sample-code/m-p/1569578#M9541</guid>
      <dc:creator>vasanth-sr</dc:creator>
      <dc:date>2022-12-14T09:36:36Z</dc:date>
    </item>
    <item>
      <title>Re: s32k314 qspi sample code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/s32k314-qspi-sample-code/m-p/1569979#M9542</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210023"&gt;@vasanth-sr&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;At this point in time, S32DS 3.5 is not broadly supported on the S32K3 family.&amp;nbsp;We do recommend to stay at version 3.4 until further notice.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 21:12:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/s32k314-qspi-sample-code/m-p/1569979#M9542</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2022-12-14T21:12:23Z</dc:date>
    </item>
    <item>
      <title>Re: s32k314 qspi sample code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/s32k314-qspi-sample-code/m-p/1569985#M9543</link>
      <description>&lt;P&gt;Hello Vasanth,&lt;/P&gt;
&lt;P&gt;The peripherals are added using the Peripherals Tool. The QSPI Tool that you show in the images is an advanced tool which can be used to create customized parameters for the QuadSPI to be used by the BootROM. This is not supported for S32K3xx family of devices.&lt;/P&gt;
&lt;P&gt;The available example applications are provided in the New Project from Example wizard:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mikedoidge_0-1671053176793.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/204496iCAC090427A869FF5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mikedoidge_0-1671053176793.png" alt="mikedoidge_0-1671053176793.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;mikedoidge_0-1671053176793.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;For specific details on the availability of QSPI example, I refer you to&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/83222"&gt;@namnguyenviet&lt;/a&gt;&amp;nbsp;for further details.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 21:27:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/s32k314-qspi-sample-code/m-p/1569985#M9543</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2022-12-14T21:27:38Z</dc:date>
    </item>
  </channel>
</rss>