<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Why not work Update Code in S32DS in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Why-not-work-Update-Code-in-S32DS/m-p/1565013#M9506</link>
    <description>&lt;P&gt;As I mention I did modify and add configuration in Configuration tool. After this right down corner show Code generation process bar. But when I click the Update Code Icon the dialog does not show changed contents.&lt;/P&gt;</description>
    <pubDate>Tue, 06 Dec 2022 08:11:56 GMT</pubDate>
    <dc:creator>dnewbe</dc:creator>
    <dc:date>2022-12-06T08:11:56Z</dc:date>
    <item>
      <title>Why not work Update Code in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Why-not-work-Update-Code-in-S32DS/m-p/1553632#M9415</link>
      <description>&lt;P&gt;Hi Dear S32DS Expert.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm use S32DS for S32 Platform Version 3.4 and SDK is PlatformSDK_S32K3_2022_07.&lt;/P&gt;&lt;P&gt;I did modify my project in Configuration Tools of S32DS. After modify the Update Code dialog not show quickly which file will be change. Sometimes I wait until the Update Code dialog show change. But Now I hardly can't see changed files of this dialog.&lt;/P&gt;&lt;P&gt;So I did switch other project and return to my project. Or close a S32DS and re-laucnch S32DS. This case sometime work but sometime not work.&lt;/P&gt;&lt;P&gt;Why this Update Code not work ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Nov 2022 03:19:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Why-not-work-Update-Code-in-S32DS/m-p/1553632#M9415</guid>
      <dc:creator>dnewbe</dc:creator>
      <dc:date>2022-11-15T03:19:48Z</dc:date>
    </item>
    <item>
      <title>Re: Why not work Update Code in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Why-not-work-Update-Code-in-S32DS/m-p/1556009#M9435</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;If you can identify a repeatable set of steps to reproduce the issue, then we can help you. Before then, it is extremely difficult to identify any solution.&lt;/P&gt;
&lt;P&gt;Please provide a consistent method to reproduce your issue.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Thu, 17 Nov 2022 20:41:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Why-not-work-Update-Code-in-S32DS/m-p/1556009#M9435</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2022-11-17T20:41:01Z</dc:date>
    </item>
    <item>
      <title>Re: Why not work Update Code in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Why-not-work-Update-Code-in-S32DS/m-p/1565013#M9506</link>
      <description>&lt;P&gt;As I mention I did modify and add configuration in Configuration tool. After this right down corner show Code generation process bar. But when I click the Update Code Icon the dialog does not show changed contents.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 08:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Why-not-work-Update-Code-in-S32DS/m-p/1565013#M9506</guid>
      <dc:creator>dnewbe</dc:creator>
      <dc:date>2022-12-06T08:11:56Z</dc:date>
    </item>
    <item>
      <title>Re: Why not work Update Code in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Why-not-work-Update-Code-in-S32DS/m-p/1565435#M9508</link>
      <description>&lt;P&gt;Hello Yongki,&lt;/P&gt;
&lt;P&gt;From your description, it is difficult to determine what might be the cause. I am unable to reproduce the issue. More details are needed.&lt;/P&gt;
&lt;P&gt;1) Is the issue only reproducible for this particular project or does it occur also for other projects? What about the example projects included with the RTD SDK? What about a newly created project from the New Project Wizard?&lt;/P&gt;
&lt;P&gt;2) If this issue can happen on an example project or a new project, what steps must be followed to create the issue?&lt;/P&gt;
&lt;P&gt;3) If the issue only occurs on your project, could you share the project with us so we could try to reproduce the issue on our side and investigate the cause?&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 21:44:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Why-not-work-Update-Code-in-S32DS/m-p/1565435#M9508</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2022-12-06T21:44:52Z</dc:date>
    </item>
    <item>
      <title>Re: Why not work Update Code in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Why-not-work-Update-Code-in-S32DS/m-p/1568951#M9534</link>
      <description>&lt;P&gt;To mikedoidge&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Today I install another S32DS ver 3.5.&lt;/P&gt;&lt;P&gt;Previous version is S32DS 3.4 that have two SDK PlatformSDK_2207 and&amp;nbsp;SDK PlatformSDK_2207 version.&lt;/P&gt;&lt;P&gt;I think my problem is two SDK version haved.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So now I have no that problem. I say thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Dec 2022 10:34:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Why-not-work-Update-Code-in-S32DS/m-p/1568951#M9534</guid>
      <dc:creator>dnewbe</dc:creator>
      <dc:date>2022-12-13T10:34:40Z</dc:date>
    </item>
  </channel>
</rss>