<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRAppID Bootloader Tool</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/RAppID-Bootloader-Tool/m-p/1498154#M9328</link>
    <description>&lt;P&gt;Hi all, this might seem a silly question so apologies, but I am really struggling to understand these:&lt;/P&gt;&lt;P&gt;1. What is the difference between the RAppID BL tool and dragging and dropping an MOT file intl the S32K144 EVB board just using the Windows explorer? What is the advantage/usage of this tool?&lt;/P&gt;&lt;P&gt;2. What is the hardware required to use this tool? Do I connect my S32K144 board using the micro USB cable to my PC directly or do I need an interface such as the PE micro multilink?&lt;/P&gt;&lt;P&gt;3. What are those "COM port" specifications on the tool for? Do I use these to specify how to connect to the board (i.e. direct USB or PE micro) or is it for something else?&lt;/P&gt;&lt;P&gt;4. If PE micro multilink adaptor required, where do I connect this? SWD or SDA connector (both look the same, and seems to be for programming).&lt;/P&gt;&lt;P&gt;That's all, I know its a lot of questions but I am really struggling to understand this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance for your kind help and best regards.&lt;/P&gt;</description>
    <pubDate>Fri, 29 Jul 2022 16:49:30 GMT</pubDate>
    <dc:creator>whinojo</dc:creator>
    <dc:date>2022-07-29T16:49:30Z</dc:date>
    <item>
      <title>RAppID Bootloader Tool</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/RAppID-Bootloader-Tool/m-p/1498154#M9328</link>
      <description>&lt;P&gt;Hi all, this might seem a silly question so apologies, but I am really struggling to understand these:&lt;/P&gt;&lt;P&gt;1. What is the difference between the RAppID BL tool and dragging and dropping an MOT file intl the S32K144 EVB board just using the Windows explorer? What is the advantage/usage of this tool?&lt;/P&gt;&lt;P&gt;2. What is the hardware required to use this tool? Do I connect my S32K144 board using the micro USB cable to my PC directly or do I need an interface such as the PE micro multilink?&lt;/P&gt;&lt;P&gt;3. What are those "COM port" specifications on the tool for? Do I use these to specify how to connect to the board (i.e. direct USB or PE micro) or is it for something else?&lt;/P&gt;&lt;P&gt;4. If PE micro multilink adaptor required, where do I connect this? SWD or SDA connector (both look the same, and seems to be for programming).&lt;/P&gt;&lt;P&gt;That's all, I know its a lot of questions but I am really struggling to understand this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance for your kind help and best regards.&lt;/P&gt;</description>
      <pubDate>Fri, 29 Jul 2022 16:49:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/RAppID-Bootloader-Tool/m-p/1498154#M9328</guid>
      <dc:creator>whinojo</dc:creator>
      <dc:date>2022-07-29T16:49:30Z</dc:date>
    </item>
    <item>
      <title>Re: RAppID Bootloader Tool</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/RAppID-Bootloader-Tool/m-p/1546459#M9340</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;thank you for your questions. See below my comments:&lt;/P&gt;
&lt;P&gt;1. Rappid BL and OpenSDA (drag/drop loading) are two different loaders&lt;/P&gt;
&lt;P&gt;Rappid BL firmware (.rbf file) resists on the target MCU (S32K144) and it is executed after reset.&lt;/P&gt;
&lt;P&gt;OpenSDA firmware (.sda file)is located in a different chip(OpenSDA MCU) and behaves as USB &amp;lt;-&amp;gt; jtag converter (kind of "lite" version of PE Multilink integrated on the board)&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/document/guide/get-started-with-the-s32k144evb:NGS-S32K144EVB" target="_blank"&gt;https://www.nxp.com/document/guide/get-started-with-the-s32k144evb:NGS-S32K144EVB&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;RAppid BL advantage is you can program the target mcu over CAN/UART but it requires to be pre-programmed on the chip. OpenSDA is in fact "independent" Jtag debug probe.&lt;/P&gt;
&lt;P&gt;2. to program a file to the S32K mcu over RappidBL you need just usb cable (UART mode) or Vector CANCase/Card XL (CAN Mode) converter.&lt;/P&gt;
&lt;P&gt;3. Com Port is only the selector of a correct COM port to be communicated with the target over UART/USB. When USB cabel is plugged into S32K1xx board a new Com port should appear on your machine (could be checked in the device manager) and you should select this port.&lt;/P&gt;
&lt;P&gt;4. No additional PE multilink required. You can program bootloader by OpenSDA (drag/drop). Anyway if you'd need fo some reason to program mcu from P&amp;amp;E external probe you can use J14 SWD connector.&lt;/P&gt;
&lt;P&gt;The other one (SDA) is for updating firmware/bootloader in OpenSDA chip - I'd recommend you not to use OpenSDA&amp;nbsp; JTAG connector untill you fully understand what you do.&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;Stan&lt;/P&gt;</description>
      <pubDate>Mon, 31 Oct 2022 18:46:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/RAppID-Bootloader-Tool/m-p/1546459#M9340</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2022-10-31T18:46:10Z</dc:date>
    </item>
  </channel>
</rss>