<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: S32DS installation error</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1540169#M9253</link>
    <description>&lt;P&gt;1) Ensure you have administrator access on your PC&lt;/P&gt;&lt;P&gt;2) Select the option 'Windows 7 compatibility mode' on the file properties for the install file&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The above options gave negative results.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any other solution?&lt;/P&gt;</description>
    <pubDate>Wed, 19 Oct 2022 15:12:19 GMT</pubDate>
    <dc:creator>michelangeliousas</dc:creator>
    <dc:date>2022-10-19T15:12:19Z</dc:date>
    <item>
      <title>S32DS installation error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1539112#M9242</link>
      <description />
      <pubDate>Tue, 18 Oct 2022 08:34:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1539112#M9242</guid>
      <dc:creator>michelangeliousas</dc:creator>
      <dc:date>2022-10-18T08:34:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS installation error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1539377#M9245</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It appears you are attempting to install S32 Design Studio 3.4 onto Windows 11. This is not an officially supported installation configuration, however, we have some customers who have successfully achieved this, so we will attempt to provide some support.&lt;/P&gt;
&lt;P&gt;Here are my suggestions:&lt;/P&gt;
&lt;P&gt;1) Ensure you have administrator access on your PC&lt;/P&gt;
&lt;P&gt;2) Select the option 'Windows 7 compatibility mode' on the file properties for the install file&lt;/P&gt;
&lt;P&gt;3) Check for the installation log file located at: "C:\NXP\S32DS.3.4\_S32 Design Studio for S32 Platform 3.4_installation\". Then share it with us.&lt;/P&gt;
&lt;P&gt;4) Check the post&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-345241" target="_blank" rel="noopener"&gt;Troubleshooting: Activation fails with error message FNP ERROR 0&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp;and look into the solution for error 2.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Oct 2022 14:00:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1539377#M9245</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2022-10-18T14:00:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS installation error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1540166#M9252</link>
      <description />
      <pubDate>Wed, 19 Oct 2022 15:08:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1540166#M9252</guid>
      <dc:creator>michelangeliousas</dc:creator>
      <dc:date>2022-10-19T15:08:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS installation error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1540169#M9253</link>
      <description>&lt;P&gt;1) Ensure you have administrator access on your PC&lt;/P&gt;&lt;P&gt;2) Select the option 'Windows 7 compatibility mode' on the file properties for the install file&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The above options gave negative results.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any other solution?&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 15:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1540169#M9253</guid>
      <dc:creator>michelangeliousas</dc:creator>
      <dc:date>2022-10-19T15:12:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS installation error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1540197#M9254</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207667"&gt;@michelangeliousas&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;After reviewing the log file, I can see the installation has failed due to the failed command 'cllSvrUtility.exe', as shown in the log file excerpt here:&lt;/P&gt;
&lt;P&gt;==== 32-bit license service installation log start: ====&lt;BR /&gt;Returned: 1&lt;BR /&gt;Console: &lt;BR /&gt;C:\Users\˜smak24\AppData\Local\Temp\I1666191822\Windows&amp;gt;cd "C:\Users\Ýsmak24\AppData\Local\Temp\046509.tmp\cll\i86"&lt;/P&gt;
&lt;P&gt;C:\Users\˜smak24\AppData\Local\Temp\I1666191822\Windows&amp;gt;cllSvrUtility.exe -installService LAXCompiler&lt;/P&gt;
&lt;P&gt;Errors: Sistem belirtilen yolu bulam?yor.&lt;BR /&gt;'cllSvrUtility.exe' is not recognized as an internal or external command,&lt;BR /&gt;operable program or batch file.&lt;/P&gt;
&lt;P&gt;==== 32-bit license service installation log end. ====&lt;/P&gt;
&lt;P&gt;Something prevents the change directory command to perform. Since this fails, the current directory is not changed and thus the&amp;nbsp;'cllSvrUtility.exe' is not recognized.&lt;/P&gt;
&lt;P&gt;I see that there is an unusual character in the folder name which is from the userid. Could you please check if your IT department could help you to execute the installer under a userid that does not contain unusual characters? I would also suggest that they use an account that is also administrator level access.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 15:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1540197#M9254</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2022-10-19T15:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS installation error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1540231#M9256</link>
      <description>&lt;P&gt;It was understood that there was a problem caused by a user naming error. Thank you for your support.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 16:32:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-installation-error/m-p/1540231#M9256</guid>
      <dc:creator>michelangeliousas</dc:creator>
      <dc:date>2022-10-19T16:32:32Z</dc:date>
    </item>
  </channel>
</rss>