<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC5777C Module could not be erased in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5777C-Module-could-not-be-erased/m-p/1515041#M8999</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm using MPC5777C, P&amp;amp;E Micro Multilink FX and s32 design studio. Everything works fine until yesterday, whereas I try to flash a program but get a module that could not be erased bug. Then I realize the program could have a potential link program. So I tried to flash a blank project to the processor after that, but the processor seems is locked, and any project gives me the same result (Module could not be erased), the fault log is as follows:&lt;/P&gt;&lt;P&gt;Connection from "127.0.0.1" via 127.0.0.1. Connection from port "4593" to 7224&lt;BR /&gt;Copyright 2018 P&amp;amp;E Microcomputer Systems,Inc.&lt;BR /&gt;Command Line :E:\S32_design_studio_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\pegdbserver_power_console -device=MPC5777C -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -po?&lt;BR /&gt;P&amp;amp;E Interface detected - Flash Version 10.46&lt;BR /&gt;Flash Data in range 0x00800000-0x00800007.&lt;BR /&gt;Flash Data in range 0x00800400-0x008008B7.&lt;BR /&gt;Flash Data in range 0x008008C0-0x008015E8.&lt;BR /&gt;Flash Data in range 0x008015EC-0x008015FF.&lt;BR /&gt;Flash Data in range 0x00810000-0x00810103.&lt;BR /&gt;Flash Data in range 0x00811000-0x008119AF.&lt;BR /&gt;Flash Data in range 0x00C00400-0x00C006ED.&lt;BR /&gt;Flash Data in range 0x00C10000-0x00C100F3.&lt;BR /&gt;Flash Data in range 0x00C11000-0x00C11763.&lt;BR /&gt;Flash Data in range 0x00C11770-0x00C11C47.&lt;BR /&gt;&lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;Initializing Ram Block 0x00300000-0x00307FFF.&lt;BR /&gt;MPC5777C Device detected.&lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;CMD&amp;gt;CM E:\S32_design_studio_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&amp;amp;E\nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;Initializing Ram Block 0x00300000-0x00307FFF.&lt;BR /&gt;MPC5777C Device detected.&lt;BR /&gt;&lt;BR /&gt;DOUBLE BUFFERING enabled.&lt;BR /&gt;Initialized.&lt;BR /&gt;&lt;BR /&gt;;version 1.04, 12/13/2016, Copyright P&amp;amp;E Microcomputer Systems, &lt;A href="http://www.pemicro.com" target="_blank"&gt;www.pemicro.com&lt;/A&gt; [5777C_8meg_highspeed]&lt;BR /&gt;&lt;BR /&gt;;device NXP, MPC5777C, 1x32x2048k, desc=CFlash_highspeed&lt;BR /&gt;&lt;BR /&gt;;begin_cs device=$30800000, length=$00800000, ram=$00300000&lt;BR /&gt;&lt;BR /&gt;Loading programming algorithm ...&lt;BR /&gt;Done.&lt;BR /&gt;Programming sequency is : erase, blank check, program, and verify {default}&lt;BR /&gt;CMD&amp;gt;VC&lt;BR /&gt;Verifying object file CRC-16 to device ranges ...&lt;BR /&gt;block 00800000-00800007 ...&lt;BR /&gt;Ok.&lt;BR /&gt;block 00800400-008008B7 ...&lt;BR /&gt;Ok.&lt;BR /&gt;block 008008C0-008015E8 ...&lt;BR /&gt;Calculated CRC-16 does not match block. (File = $C683, Device = $F15B)&lt;BR /&gt;Current content of flash does not match application to be programmed&lt;BR /&gt;&lt;BR /&gt;CMD&amp;gt;EM&lt;BR /&gt;&lt;BR /&gt;Erasing.&lt;BR /&gt;Module could not be erased.&lt;BR /&gt;Error Erasing flash of device&lt;BR /&gt;Error occured during Flash programming.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;&lt;BR /&gt;Starting reset script (E:\S32_design_studio_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&amp;amp;E\s32e200_mpc5777c.mac) ...&lt;BR /&gt;REM This script is compatible with MPC5777C devices.&lt;BR /&gt;REM Clean GPRs to remove residual data after using algorithm&lt;BR /&gt;REM Setup MMU for for Periph B Modules&lt;BR /&gt;REM Base address = $FFE0_0000&lt;BR /&gt;REM TLB0, 2 MByte Memory Space, Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU to put internal Flash at 0...&lt;BR /&gt;REM Virtual address 0x0 -&amp;gt; Physical address = $0000_0000&lt;BR /&gt;REM TLB1, 16 MByte Memory Space, Not Guarded, Cachable, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for External Memory&lt;BR /&gt;REM Base address = $2000_0000&lt;BR /&gt;REM TLB2, 16 MByte Memory Space, Not Guarded, Cachable, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for Internal SRAM&lt;BR /&gt;REM Base address = $4000_0000&lt;BR /&gt;REM TLB3, 512 KByte Memory Space, Not Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for Periph A Modules&lt;BR /&gt;REM Base address = $C3E0_0000&lt;BR /&gt;REM TLB4, 2 MByte Memory Space, Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Initialize all of the Main SRAM - 512KB&lt;BR /&gt;Initializing RAM from $40000000 to $4007FFFF.&lt;BR /&gt;Initializing Ram Block 0x40000000-0x4007FFFF.&lt;BR /&gt;&lt;BR /&gt;Reset script (E:\S32_design_studio_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&amp;amp;E\s32e200_mpc5777c.mac) completed.&lt;BR /&gt;&lt;BR /&gt;MPC5777C Device detected.&lt;/P&gt;&lt;P&gt;PEmicro GDB Launch Failure : Error during flash programming. Terminating debug session.&lt;/P&gt;&lt;P&gt;It seems my processor is locked somehow, Now I don't know what to do, Any help would be appreciated.&lt;/P&gt;&lt;P&gt;#MPC5777C&amp;nbsp; #s32&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Luke&lt;/P&gt;</description>
    <pubDate>Wed, 31 Aug 2022 23:37:44 GMT</pubDate>
    <dc:creator>lukezhang</dc:creator>
    <dc:date>2022-08-31T23:37:44Z</dc:date>
    <item>
      <title>MPC5777C Module could not be erased</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5777C-Module-could-not-be-erased/m-p/1515041#M8999</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm using MPC5777C, P&amp;amp;E Micro Multilink FX and s32 design studio. Everything works fine until yesterday, whereas I try to flash a program but get a module that could not be erased bug. Then I realize the program could have a potential link program. So I tried to flash a blank project to the processor after that, but the processor seems is locked, and any project gives me the same result (Module could not be erased), the fault log is as follows:&lt;/P&gt;&lt;P&gt;Connection from "127.0.0.1" via 127.0.0.1. Connection from port "4593" to 7224&lt;BR /&gt;Copyright 2018 P&amp;amp;E Microcomputer Systems,Inc.&lt;BR /&gt;Command Line :E:\S32_design_studio_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\pegdbserver_power_console -device=MPC5777C -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -po?&lt;BR /&gt;P&amp;amp;E Interface detected - Flash Version 10.46&lt;BR /&gt;Flash Data in range 0x00800000-0x00800007.&lt;BR /&gt;Flash Data in range 0x00800400-0x008008B7.&lt;BR /&gt;Flash Data in range 0x008008C0-0x008015E8.&lt;BR /&gt;Flash Data in range 0x008015EC-0x008015FF.&lt;BR /&gt;Flash Data in range 0x00810000-0x00810103.&lt;BR /&gt;Flash Data in range 0x00811000-0x008119AF.&lt;BR /&gt;Flash Data in range 0x00C00400-0x00C006ED.&lt;BR /&gt;Flash Data in range 0x00C10000-0x00C100F3.&lt;BR /&gt;Flash Data in range 0x00C11000-0x00C11763.&lt;BR /&gt;Flash Data in range 0x00C11770-0x00C11C47.&lt;BR /&gt;&lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;Initializing Ram Block 0x00300000-0x00307FFF.&lt;BR /&gt;MPC5777C Device detected.&lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;CMD&amp;gt;CM E:\S32_design_studio_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&amp;amp;E\nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;Initializing Ram Block 0x00300000-0x00307FFF.&lt;BR /&gt;MPC5777C Device detected.&lt;BR /&gt;&lt;BR /&gt;DOUBLE BUFFERING enabled.&lt;BR /&gt;Initialized.&lt;BR /&gt;&lt;BR /&gt;;version 1.04, 12/13/2016, Copyright P&amp;amp;E Microcomputer Systems, &lt;A href="http://www.pemicro.com" target="_blank"&gt;www.pemicro.com&lt;/A&gt; [5777C_8meg_highspeed]&lt;BR /&gt;&lt;BR /&gt;;device NXP, MPC5777C, 1x32x2048k, desc=CFlash_highspeed&lt;BR /&gt;&lt;BR /&gt;;begin_cs device=$30800000, length=$00800000, ram=$00300000&lt;BR /&gt;&lt;BR /&gt;Loading programming algorithm ...&lt;BR /&gt;Done.&lt;BR /&gt;Programming sequency is : erase, blank check, program, and verify {default}&lt;BR /&gt;CMD&amp;gt;VC&lt;BR /&gt;Verifying object file CRC-16 to device ranges ...&lt;BR /&gt;block 00800000-00800007 ...&lt;BR /&gt;Ok.&lt;BR /&gt;block 00800400-008008B7 ...&lt;BR /&gt;Ok.&lt;BR /&gt;block 008008C0-008015E8 ...&lt;BR /&gt;Calculated CRC-16 does not match block. (File = $C683, Device = $F15B)&lt;BR /&gt;Current content of flash does not match application to be programmed&lt;BR /&gt;&lt;BR /&gt;CMD&amp;gt;EM&lt;BR /&gt;&lt;BR /&gt;Erasing.&lt;BR /&gt;Module could not be erased.&lt;BR /&gt;Error Erasing flash of device&lt;BR /&gt;Error occured during Flash programming.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;&lt;BR /&gt;Starting reset script (E:\S32_design_studio_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&amp;amp;E\s32e200_mpc5777c.mac) ...&lt;BR /&gt;REM This script is compatible with MPC5777C devices.&lt;BR /&gt;REM Clean GPRs to remove residual data after using algorithm&lt;BR /&gt;REM Setup MMU for for Periph B Modules&lt;BR /&gt;REM Base address = $FFE0_0000&lt;BR /&gt;REM TLB0, 2 MByte Memory Space, Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU to put internal Flash at 0...&lt;BR /&gt;REM Virtual address 0x0 -&amp;gt; Physical address = $0000_0000&lt;BR /&gt;REM TLB1, 16 MByte Memory Space, Not Guarded, Cachable, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for External Memory&lt;BR /&gt;REM Base address = $2000_0000&lt;BR /&gt;REM TLB2, 16 MByte Memory Space, Not Guarded, Cachable, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for Internal SRAM&lt;BR /&gt;REM Base address = $4000_0000&lt;BR /&gt;REM TLB3, 512 KByte Memory Space, Not Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for Periph A Modules&lt;BR /&gt;REM Base address = $C3E0_0000&lt;BR /&gt;REM TLB4, 2 MByte Memory Space, Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Initialize all of the Main SRAM - 512KB&lt;BR /&gt;Initializing RAM from $40000000 to $4007FFFF.&lt;BR /&gt;Initializing Ram Block 0x40000000-0x4007FFFF.&lt;BR /&gt;&lt;BR /&gt;Reset script (E:\S32_design_studio_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&amp;amp;E\s32e200_mpc5777c.mac) completed.&lt;BR /&gt;&lt;BR /&gt;MPC5777C Device detected.&lt;/P&gt;&lt;P&gt;PEmicro GDB Launch Failure : Error during flash programming. Terminating debug session.&lt;/P&gt;&lt;P&gt;It seems my processor is locked somehow, Now I don't know what to do, Any help would be appreciated.&lt;/P&gt;&lt;P&gt;#MPC5777C&amp;nbsp; #s32&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Luke&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 23:37:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5777C-Module-could-not-be-erased/m-p/1515041#M8999</guid>
      <dc:creator>lukezhang</dc:creator>
      <dc:date>2022-08-31T23:37:44Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C Module could not be erased</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5777C-Module-could-not-be-erased/m-p/1515629#M9004</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;you can try to use different programming algorithm:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jiri_kral_1-1662039422949.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/192170iF2B309442C42B122/image-size/large?v=v2&amp;amp;px=999" role="button" title="jiri_kral_1-1662039422949.png" alt="jiri_kral_1-1662039422949.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jiri_kral_1-1662039422949.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jiri_kral_2-1662039456700.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/192171i485DA83CF8B417E3/image-size/large?v=v2&amp;amp;px=999" role="button" title="jiri_kral_2-1662039456700.png" alt="jiri_kral_2-1662039456700.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jiri_kral_2-1662039456700.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jiri_kral_0-1662039301970.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/192169i8B0836A4730923B6/image-size/large?v=v2&amp;amp;px=999" role="button" title="jiri_kral_0-1662039301970.png" alt="jiri_kral_0-1662039301970.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jiri_kral_0-1662039301970.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Also updating PE Micro plugin may help:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Install-update-from-3rd-party-vendor/ta-p/1101851" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Install-update-from-3rd-party-vendor/ta-p/1101851&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Sep 2022 13:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5777C-Module-could-not-be-erased/m-p/1515629#M9004</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2022-09-01T13:38:09Z</dc:date>
    </item>
  </channel>
</rss>