<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can I download the code without source file?Like .hex file. in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Can-I-download-the-code-without-source-file-Like-hex-file/m-p/638797#M899</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I program with S32 Design Studio for ARM v1.2. Now I want to program the ship without source file,just like the file .hex of Keil?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Apr 2017 09:18:33 GMT</pubDate>
    <dc:creator>wuxiesi</dc:creator>
    <dc:date>2017-04-25T09:18:33Z</dc:date>
    <item>
      <title>Can I download the code without source file?Like .hex file.</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Can-I-download-the-code-without-source-file-Like-hex-file/m-p/638797#M899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I program with S32 Design Studio for ARM v1.2. Now I want to program the ship without source file,just like the file .hex of Keil?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Apr 2017 09:18:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Can-I-download-the-code-without-source-file-Like-hex-file/m-p/638797#M899</guid>
      <dc:creator>wuxiesi</dc:creator>
      <dc:date>2017-04-25T09:18:33Z</dc:date>
    </item>
    <item>
      <title>Re: Can I download the code without source file?Like .hex file.</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Can-I-download-the-code-without-source-file-Like-hex-file/m-p/638798#M900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you be more specific about the debug interface you are using? (Segger/Pemirco Multilink/OpenSDA..)&lt;/P&gt;&lt;P&gt;I'd recommend you to install the latest version v1.3 :&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-333485"&gt;S32 Design Studio for ARM v1.3 (Windows/Linux) released!&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest version includes flash configuration that you can use to program your elf/s-record to the MCU.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14291i7458C098139AC356/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14188i50580AC4FCEC8F70/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;With OpenSDA interface you can program your binary s-record file by drag&amp;amp;drop the file to the mass storage that appears when the board is plugged into USB socket.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14234i252CD768A0DF83C0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Apr 2017 13:43:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Can-I-download-the-code-without-source-file-Like-hex-file/m-p/638798#M900</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2017-04-25T13:43:54Z</dc:date>
    </item>
    <item>
      <title>Re: Can I download the code without source file?Like .hex file.</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Can-I-download-the-code-without-source-file-Like-hex-file/m-p/638799#M901</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your informations.I use&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Pemirco Multilink debug.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have installed the lasted version v1.3,and follow your step.However,I can't find any&amp;nbsp;file ending in '.srec' &amp;nbsp;in my project library.So, what should I do to creat a '.stec' file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also ,I try to execute the '.elf' file,and I will get a error like this:&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14744i0CFC77BF205DCA8E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Can you explain more clearly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So grateful!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Apr 2017 05:46:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Can-I-download-the-code-without-source-file-Like-hex-file/m-p/638799#M901</guid>
      <dc:creator>wuxiesi</dc:creator>
      <dc:date>2017-04-27T05:46:09Z</dc:date>
    </item>
    <item>
      <title>Re: Can I download the code without source file?Like .hex file.</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Can-I-download-the-code-without-source-file-Like-hex-file/m-p/638800#M902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;to get srec file you need to enable it in project properties.&lt;/P&gt;&lt;P&gt;Right click on your project name -&amp;gt; properties -&amp;gt; C/C++ Build -&amp;gt; Settings &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14423i2EEF0212FB239BFF/image-size/large?v=v2&amp;amp;px=999" title="s32ds_2017-04-27_10-31-01.png" alt="s32ds_2017-04-27_10-31-01.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find srec file inside Debug/Release directory (depends on your configuration).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In which step you get the error message? During upload the elf file into MCU?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Apr 2017 08:37:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Can-I-download-the-code-without-source-file-Like-hex-file/m-p/638800#M902</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2017-04-27T08:37:43Z</dc:date>
    </item>
    <item>
      <title>Re: Can I download the code without source file?Like .hex file.</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Can-I-download-the-code-without-source-file-Like-hex-file/m-p/638801#M903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your help.I found the way to solve the problem in Help Contents,as your method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the error may be caused by &amp;nbsp;lost the GDB Client Settings,when I add the gdb.exe path,it is gone.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14843i59BE38FFBC93F798/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Apr 2017 10:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Can-I-download-the-code-without-source-file-Like-hex-file/m-p/638801#M903</guid>
      <dc:creator>wuxiesi</dc:creator>
      <dc:date>2017-04-27T10:21:02Z</dc:date>
    </item>
  </channel>
</rss>