<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックBootloader CAN</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-CAN/m-p/1509051#M8960</link>
    <description>&lt;P&gt;It flashed using CAN rbf " MPC5744P_S32DS_UART1_CAN0.rbf" when I changed the following&amp;nbsp;&lt;/P&gt;&lt;P&gt;flash_rchw : org = 0x00FA0000, len = 0x4&lt;BR /&gt;cpu0_reset_vec : org = 0x00FA0004, len = 0x4&lt;BR /&gt;delay_us : org = 0x00FA0008, len = 0x4&lt;BR /&gt;appkey_addr : org = 0x00FA000C, len = 0x4&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;But the applications doesn't work&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;when I Flashed using serial UART 0 the previous version of the rbf "MPC574xP_S32DS_UART0_CAN0_OpenSDA_RevE.rbf"&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;the application worked when I write as&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;flash_rchw : org = 0x00FC0000, len = 0x4&lt;BR /&gt;cpu0_reset_vec : org = 0x00FC0004, len = 0x4&lt;BR /&gt;delay_us : org = 0x00FC0008, len = 0x4&lt;BR /&gt;appkey_addr : org = 0x00FC000C, len = 0x4&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;any help with that ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Sun, 21 Aug 2022 09:21:22 GMT</pubDate>
    <dc:creator>rehab_hassan</dc:creator>
    <dc:date>2022-08-21T09:21:22Z</dc:date>
    <item>
      <title>Bootloader CAN</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-CAN/m-p/1509051#M8960</link>
      <description>&lt;P&gt;It flashed using CAN rbf " MPC5744P_S32DS_UART1_CAN0.rbf" when I changed the following&amp;nbsp;&lt;/P&gt;&lt;P&gt;flash_rchw : org = 0x00FA0000, len = 0x4&lt;BR /&gt;cpu0_reset_vec : org = 0x00FA0004, len = 0x4&lt;BR /&gt;delay_us : org = 0x00FA0008, len = 0x4&lt;BR /&gt;appkey_addr : org = 0x00FA000C, len = 0x4&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;But the applications doesn't work&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;when I Flashed using serial UART 0 the previous version of the rbf "MPC574xP_S32DS_UART0_CAN0_OpenSDA_RevE.rbf"&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;the application worked when I write as&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;flash_rchw : org = 0x00FC0000, len = 0x4&lt;BR /&gt;cpu0_reset_vec : org = 0x00FC0004, len = 0x4&lt;BR /&gt;delay_us : org = 0x00FC0008, len = 0x4&lt;BR /&gt;appkey_addr : org = 0x00FC000C, len = 0x4&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;any help with that ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Sun, 21 Aug 2022 09:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-CAN/m-p/1509051#M8960</guid>
      <dc:creator>rehab_hassan</dc:creator>
      <dc:date>2022-08-21T09:21:22Z</dc:date>
    </item>
  </channel>
</rss>