<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックMPC 5775B GPIO Interrupt</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/MPC-5775B-GPIO-Interrupt/m-p/1496148#M8850</link>
    <description>&lt;P&gt;I want to get a user input from Push Buttons using interrupt on PIN PG3 to PG8 but there is no IRQ option to enable for these Pins.&lt;BR /&gt;Do MPC 5775 controller have only selected interrupt pins or i am doing something wrong.&lt;/P&gt;</description>
    <pubDate>Wed, 27 Jul 2022 07:12:58 GMT</pubDate>
    <dc:creator>DDosi</dc:creator>
    <dc:date>2022-07-27T07:12:58Z</dc:date>
    <item>
      <title>MPC 5775B GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC-5775B-GPIO-Interrupt/m-p/1496148#M8850</link>
      <description>&lt;P&gt;I want to get a user input from Push Buttons using interrupt on PIN PG3 to PG8 but there is no IRQ option to enable for these Pins.&lt;BR /&gt;Do MPC 5775 controller have only selected interrupt pins or i am doing something wrong.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 07:12:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC-5775B-GPIO-Interrupt/m-p/1496148#M8850</guid>
      <dc:creator>DDosi</dc:creator>
      <dc:date>2022-07-27T07:12:58Z</dc:date>
    </item>
    <item>
      <title>Re: MPC 5775B GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC-5775B-GPIO-Interrupt/m-p/1496266#M8851</link>
      <description>&lt;P&gt;In the past I made example code for these. You may download it here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-SIUL-External-IRQ-GHS714/ta-p/1116848" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-SIUL-External-IRQ-GHS714/ta-p/1116848&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 09:09:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC-5775B-GPIO-Interrupt/m-p/1496266#M8851</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-07-27T09:09:54Z</dc:date>
    </item>
  </channel>
</rss>