<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックS32V234 M4 example</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32V234-M4-example/m-p/1474266#M8721</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am able to build for M4 target with freeRTOS using an example provided by the development kit.&lt;/P&gt;&lt;P&gt;I wish to burn/copy the elf to the board itself and see it runs.&lt;/P&gt;&lt;P&gt;What is the procedure in order to do so? I didnt find any way to use the elf file for the M4.&lt;/P&gt;&lt;P&gt;I am able to connect to the board using serial and ssh (linux core) and boot sequence from A53 (default configuration).&lt;/P&gt;&lt;P&gt;No debugging tool.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
    <pubDate>Wed, 15 Jun 2022 08:12:45 GMT</pubDate>
    <dc:creator>SagiSalomon</dc:creator>
    <dc:date>2022-06-15T08:12:45Z</dc:date>
    <item>
      <title>S32V234 M4 example</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32V234-M4-example/m-p/1474266#M8721</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am able to build for M4 target with freeRTOS using an example provided by the development kit.&lt;/P&gt;&lt;P&gt;I wish to burn/copy the elf to the board itself and see it runs.&lt;/P&gt;&lt;P&gt;What is the procedure in order to do so? I didnt find any way to use the elf file for the M4.&lt;/P&gt;&lt;P&gt;I am able to connect to the board using serial and ssh (linux core) and boot sequence from A53 (default configuration).&lt;/P&gt;&lt;P&gt;No debugging tool.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 08:12:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32V234-M4-example/m-p/1474266#M8721</guid>
      <dc:creator>SagiSalomon</dc:creator>
      <dc:date>2022-06-15T08:12:45Z</dc:date>
    </item>
  </channel>
</rss>