<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックFlash Configuration option missing</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-Configuration-option-missing/m-p/1452789#M8522</link>
    <description>&lt;P&gt;In "HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio" a Flash Configuration option under option 1 to flash a MCU with a compiled binary.&lt;BR /&gt;&lt;BR /&gt;This option however seems to be missing in the version of Design Studio I'm using:&lt;/P&gt;&lt;P&gt;S32 Design Studio for S32 Platform&lt;BR /&gt;Build id: 201217 (Update 3)&lt;/P&gt;&lt;P&gt;OS: Windows 10, v.10.0, x86_64 / win32&lt;BR /&gt;Java version: 1.8.0_202&lt;/P&gt;</description>
    <pubDate>Wed, 04 May 2022 14:56:28 GMT</pubDate>
    <dc:creator>ameershira</dc:creator>
    <dc:date>2022-05-04T14:56:28Z</dc:date>
    <item>
      <title>Flash Configuration option missing</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-Configuration-option-missing/m-p/1452789#M8522</link>
      <description>&lt;P&gt;In "HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio" a Flash Configuration option under option 1 to flash a MCU with a compiled binary.&lt;BR /&gt;&lt;BR /&gt;This option however seems to be missing in the version of Design Studio I'm using:&lt;/P&gt;&lt;P&gt;S32 Design Studio for S32 Platform&lt;BR /&gt;Build id: 201217 (Update 3)&lt;/P&gt;&lt;P&gt;OS: Windows 10, v.10.0, x86_64 / win32&lt;BR /&gt;Java version: 1.8.0_202&lt;/P&gt;</description>
      <pubDate>Wed, 04 May 2022 14:56:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Flash-Configuration-option-missing/m-p/1452789#M8522</guid>
      <dc:creator>ameershira</dc:creator>
      <dc:date>2022-05-04T14:56:28Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Configuration option missing</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-Configuration-option-missing/m-p/1453036#M8523</link>
      <description>&lt;P&gt;Hello Ameer,&lt;/P&gt;
&lt;P&gt;You are correct. The article&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-download-separate-elf-srec-hex-file-to-microcontroller/ta-p/1127159" target="_self"&gt; HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio&lt;/A&gt;&amp;nbsp;is for use with S32 Design Studio for Arm or S32 Design Studio for Power Architecture. It is not applicable to S32 Design Studio for S32 Platform.&lt;/P&gt;
&lt;P&gt;To flash an executable to target for S32 Design Studio for S32 Platform you have options:&lt;/P&gt;
&lt;P&gt;1) S32 Debugger Flash Programmer&lt;/P&gt;
&lt;P&gt;2) S32 Flash Tool&lt;/P&gt;
&lt;P&gt;3) PE Micro GDB (for S32K1 family)&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Wed, 04 May 2022 21:43:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Flash-Configuration-option-missing/m-p/1453036#M8523</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2022-05-04T21:43:54Z</dc:date>
    </item>
  </channel>
</rss>