<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: S32K144 Signal Generator</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1451512#M8505</link>
    <description>&lt;P&gt;So could you help me generating any signal from GPIO?&lt;BR /&gt;By that I mean giving some ideas or steps I have to provide in order to make my program work.&amp;nbsp;&lt;BR /&gt;Thank you for your advice&lt;/P&gt;</description>
    <pubDate>Fri, 29 Apr 2022 22:48:22 GMT</pubDate>
    <dc:creator>RV777</dc:creator>
    <dc:date>2022-04-29T22:48:22Z</dc:date>
    <item>
      <title>S32K144 Signal Generator</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1449425#M8491</link>
      <description>&lt;P&gt;Hello. I'm new into all of this and wanted to ask some questions.&lt;BR /&gt;I need to create Signal Generator right now, the signal has to be from any GPIO pin.&lt;BR /&gt;I'm using:&amp;nbsp;&lt;BR /&gt;S32DS&lt;BR /&gt;S32K144EVB board:&amp;nbsp;&lt;A href="https://www.nxp.com/document/guide/get-started-with-the-s32k144evb:NGS-S32K144EVB" target="_blank"&gt;https://www.nxp.com/document/guide/get-started-with-the-s32k144evb:NGS-S32K144EVB&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;So my idea was to:&lt;BR /&gt;- create new application project where I drag functions from components of my project,&lt;/P&gt;&lt;P&gt;- I chose&amp;nbsp;CLOCK_DRV_Init(&amp;amp;clockMan1_InitConfig0); to initialize the clock,&lt;/P&gt;&lt;P&gt;-&amp;nbsp;PINS_DRV_Init(PTA, g_pin_mux_InitConfigArr); - initialize PTA registers from where I will use J2-16 PTA14 GPIO pin,&lt;BR /&gt;- then I somehow need to set them to output I guess (because the signal will be generated from the board to outside of it),&lt;/P&gt;&lt;P&gt;- the signal has to be ~1000Mhz so I need to choose the right functions to make the signal with this kind of frequency,&lt;/P&gt;&lt;P&gt;- to read the value (and check if this works) I will use the example with ftm_signal_measurement_s32k144 example.&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;BR /&gt;Have a good programming time &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Apr 2022 22:04:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1449425#M8491</guid>
      <dc:creator>RV777</dc:creator>
      <dc:date>2022-04-26T22:04:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Signal Generator</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1449491#M8492</link>
      <description>&lt;P&gt;Hi RV777,&lt;/P&gt;
&lt;P&gt;I am sorry to tell you that the S32K1x is not able to generate &lt;STRONG&gt;1000MHz&lt;/STRONG&gt; signal, it's out of the specification "5.6 AC electrical specifications at 5 V range" of&amp;nbsp;&lt;A id="relatedDocsClickPDF_1" class="dtmcustomrulelink" href="https://www.nxp.com/docs/en/data-sheet/S32K-DS.pdf" target="_blank" rel="noopener" data-dtmaction="Design Resources Section - Documentation - Results Link Click" data-dtmsubaction="S32K1xx MCU Family - Data Sheet - NXP - Data Sheet - English"&gt;&lt;SPAN&gt;S32K1xx MCU Family - Data Sheet&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="5.6 AC electrical specifications at 5 V range.png" style="width: 883px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/178076i1E8378D0BE0062FD/image-size/large?v=v2&amp;amp;px=999" role="button" title="5.6 AC electrical specifications at 5 V range.png" alt="5.6 AC electrical specifications at 5 V range.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;By the way, oc_pal_s32k144 is able to generate signal too. You don't need to toggle GPIO by software.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 27 Apr 2022 01:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1449491#M8492</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-04-27T01:40:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Signal Generator</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1450942#M8500</link>
      <description>&lt;P&gt;The thing is, I am using 12V.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Apr 2022 22:22:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1450942#M8500</guid>
      <dc:creator>RV777</dc:creator>
      <dc:date>2022-04-28T22:22:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Signal Generator</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1450959#M8501</link>
      <description>&lt;P&gt;Yes, the board can be powered by 12V through J16, but the power supply voltage range of S32K144 can only be 2.7-5.5v.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Table 3. Voltage and current operating requirements for S32K1xx series.png" style="width: 862px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/178368iF7F6DCCB6A6D8C75/image-size/large?v=v2&amp;amp;px=999" role="button" title="Table 3. Voltage and current operating requirements for S32K1xx series.png" alt="Table 3. Voltage and current operating requirements for S32K1xx series.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Apr 2022 01:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1450959#M8501</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-04-29T01:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Signal Generator</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1451512#M8505</link>
      <description>&lt;P&gt;So could you help me generating any signal from GPIO?&lt;BR /&gt;By that I mean giving some ideas or steps I have to provide in order to make my program work.&amp;nbsp;&lt;BR /&gt;Thank you for your advice&lt;/P&gt;</description>
      <pubDate>Fri, 29 Apr 2022 22:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1451512#M8505</guid>
      <dc:creator>RV777</dc:creator>
      <dc:date>2022-04-29T22:48:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Signal Generator</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1451536#M8506</link>
      <description>&lt;P&gt;&lt;SPAN&gt;You don't need to toggle GPIO by software.&amp;nbsp;oc_pal_s32k144 is able to generate signal. The signal is output from a pin too.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;But S32K144 can not output such high(1000MHz) frequency signal. So You may need to change the MCU.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 30 Apr 2022 01:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K144-Signal-Generator/m-p/1451536#M8506</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-04-30T01:19:39Z</dc:date>
    </item>
  </channel>
</rss>