<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic s32ds ubuntu 18 in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/s32ds-ubuntu-18/m-p/1444246#M8448</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have just follow the instruction to install s32ds in linux ubuntu 18, all steps, and special care in the java ones, but when I am executing the binary &lt;STRONG&gt;"S32DS.3.4_b201217_linux.x86_64.bin&lt;/STRONG&gt;" I have got this error,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Preparing to install&lt;BR /&gt;Extracting the installation resources from the installer archive...&lt;BR /&gt;Configuring the installer for this system's environment...&lt;/P&gt;&lt;P&gt;Launching installer...&lt;/P&gt;&lt;P&gt;An internal LaunchAnywhere application error has occured and this application cannot proceed. (LAX)&lt;/P&gt;&lt;P&gt;Stack Trace:&lt;BR /&gt;java.lang.IllegalArgumentException: Malformed \uxxxx encoding.&lt;BR /&gt;at java.util.Properties.loadConvert(Properties.java:574)&lt;BR /&gt;at java.util.Properties.load0(Properties.java:391)&lt;BR /&gt;at java.util.Properties.load(Properties.java:317)&lt;BR /&gt;at com.zerog.common.java.util.PropertiesUtil.loadProperties(Unknown Source)&lt;BR /&gt;at com.zerog.lax.LAX.&amp;lt;init&amp;gt;(Unknown Source)&lt;BR /&gt;at com.zerog.lax.LAX.main(Unknown Source)&lt;/P&gt;&lt;P&gt;What could I do?&lt;/P&gt;&lt;P&gt;many thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 14 Apr 2022 16:06:01 GMT</pubDate>
    <dc:creator>mauriruizl81</dc:creator>
    <dc:date>2022-04-14T16:06:01Z</dc:date>
    <item>
      <title>s32ds ubuntu 18</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/s32ds-ubuntu-18/m-p/1444246#M8448</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have just follow the instruction to install s32ds in linux ubuntu 18, all steps, and special care in the java ones, but when I am executing the binary &lt;STRONG&gt;"S32DS.3.4_b201217_linux.x86_64.bin&lt;/STRONG&gt;" I have got this error,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Preparing to install&lt;BR /&gt;Extracting the installation resources from the installer archive...&lt;BR /&gt;Configuring the installer for this system's environment...&lt;/P&gt;&lt;P&gt;Launching installer...&lt;/P&gt;&lt;P&gt;An internal LaunchAnywhere application error has occured and this application cannot proceed. (LAX)&lt;/P&gt;&lt;P&gt;Stack Trace:&lt;BR /&gt;java.lang.IllegalArgumentException: Malformed \uxxxx encoding.&lt;BR /&gt;at java.util.Properties.loadConvert(Properties.java:574)&lt;BR /&gt;at java.util.Properties.load0(Properties.java:391)&lt;BR /&gt;at java.util.Properties.load(Properties.java:317)&lt;BR /&gt;at com.zerog.common.java.util.PropertiesUtil.loadProperties(Unknown Source)&lt;BR /&gt;at com.zerog.lax.LAX.&amp;lt;init&amp;gt;(Unknown Source)&lt;BR /&gt;at com.zerog.lax.LAX.main(Unknown Source)&lt;/P&gt;&lt;P&gt;What could I do?&lt;/P&gt;&lt;P&gt;many thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Apr 2022 16:06:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/s32ds-ubuntu-18/m-p/1444246#M8448</guid>
      <dc:creator>mauriruizl81</dc:creator>
      <dc:date>2022-04-14T16:06:01Z</dc:date>
    </item>
    <item>
      <title>Re: s32ds ubuntu 18</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/s32ds-ubuntu-18/m-p/1445840#M8457</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;did you met all the requirements for Linux OS mentioned in Install Guide (installing 32 libraries and so on)?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jiri&lt;/P&gt;</description>
      <pubDate>Tue, 19 Apr 2022 14:37:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/s32ds-ubuntu-18/m-p/1445840#M8457</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2022-04-19T14:37:19Z</dc:date>
    </item>
    <item>
      <title>Re: s32ds ubuntu 18</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/s32ds-ubuntu-18/m-p/1445874#M8458</link>
      <description>&lt;P&gt;Hello, yes, sorry I found out what was going on, I had a string&amp;nbsp; "\u" in the PS1 environment variable, remove that and it went Ok. many thanks&lt;/P&gt;</description>
      <pubDate>Tue, 19 Apr 2022 15:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/s32ds-ubuntu-18/m-p/1445874#M8458</guid>
      <dc:creator>mauriruizl81</dc:creator>
      <dc:date>2022-04-19T15:54:34Z</dc:date>
    </item>
  </channel>
</rss>