<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32 Design Studio for Power Architecture Version 2.1 in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-for-Power-Architecture-Version-2-1/m-p/1440475#M8434</link>
    <description>&lt;P&gt;Dear&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;The processor I use is MPC5777C, the debuger I use is Multilink_Universal_FX, and the IDE I use is S32 Design Studio for Power Architecture Version 2.1.I created the project to be able to debug in RAM and flash.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; But I can't download the generated .elf file to flash using the flash from file tool.Attached is the .elf file generated by the project.The compilation information of the console is as follows：&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;“Connection from "127.0.0.1" via 127.0.0.1. Connection from port "49779" to 7224&lt;BR /&gt;Copyright 2018 P&amp;amp;E Microcomputer Systems,Inc.&lt;BR /&gt;Command Line :D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\pegdbserver_power_console -device=MPC5777C -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -port�&lt;BR /&gt;P&amp;amp;E Interface detected - Flash Version 10.81&lt;BR /&gt;Flash Data in range 0x00800000-0x00800007.&lt;BR /&gt;Flash Data in range 0x00800400-0x008006ED.&lt;BR /&gt;Flash Data in range 0x00810000-0x008100F3.&lt;BR /&gt;Flash Data in range 0x00811000-0x00811763.&lt;BR /&gt;Flash Data in range 0x00811770-0x0081B453.&lt;BR /&gt;&lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;Initializing Ram Block 0x00300000-0x00307FFF.&lt;BR /&gt;MPC5777C Device detected.&lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;CMD&amp;gt;CM D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&amp;amp;E\nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;Initializing Ram Block 0x00300000-0x00307FFF.&lt;BR /&gt;MPC5777C Device detected.&lt;BR /&gt;&lt;BR /&gt;DOUBLE BUFFERING enabled.&lt;BR /&gt;Initialized.&lt;BR /&gt;&lt;BR /&gt;;version 1.04, 12/13/2016, Copyright P&amp;amp;E Microcomputer Systems, &lt;A href="http://www.pemicro.com" target="_blank"&gt;www.pemicro.com&lt;/A&gt; [5777C_8meg_highspeed]&lt;BR /&gt;&lt;BR /&gt;;device NXP, MPC5777C, 1x32x2048k, desc=CFlash_highspeed&lt;BR /&gt;&lt;BR /&gt;;begin_cs device=$30800000, length=$00800000, ram=$00300000&lt;BR /&gt;&lt;BR /&gt;Loading programming algorithm ...&lt;BR /&gt;Done.&lt;BR /&gt;Programming sequency is : erase, blank check, program, and verify {default}&lt;BR /&gt;CMD&amp;gt;VC&lt;BR /&gt;Verifying object file CRC-16 to device ranges ...&lt;BR /&gt;block 00800000-00800007 ...&lt;BR /&gt;Ok.&lt;BR /&gt;block 00800400-008006ED ...&lt;BR /&gt;Ok.&lt;BR /&gt;block 00810000-008100F3 ...&lt;BR /&gt;Ok.&lt;BR /&gt;block 00811000-00811763 ...&lt;BR /&gt;Ok.&lt;BR /&gt;block 00811770-0081B453 ...&lt;BR /&gt;Ok.&lt;BR /&gt;Checksum Verification Successful. (Cumulative CRC-16=$9609)&lt;BR /&gt;Application verified in memory. No need to reprogram.&lt;BR /&gt;&lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;Initializing Ram Block 0x00300000-0x00307FFF.&lt;BR /&gt;MPC5777C Device detected.&lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;&lt;BR /&gt;Starting reset script (D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&amp;amp;E\s32e200_mpc5777c.mac) ...&lt;BR /&gt;REM This script is compatible with MPC5777C devices.&lt;BR /&gt;REM Clean GPRs to remove residual data after using algorithm&lt;BR /&gt;REM Setup MMU for for Periph B Modules&lt;BR /&gt;REM Base address = $FFE0_0000&lt;BR /&gt;REM TLB0, 2 MByte Memory Space, Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU to put internal Flash at 0...&lt;BR /&gt;REM Virtual address 0x0 -&amp;gt; Physical address = $0000_0000&lt;BR /&gt;REM TLB1, 16 MByte Memory Space, Not Guarded, Cachable, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for External Memory&lt;BR /&gt;REM Base address = $2000_0000&lt;BR /&gt;REM TLB2, 16 MByte Memory Space, Not Guarded, Cachable, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for Internal SRAM&lt;BR /&gt;REM Base address = $4000_0000&lt;BR /&gt;REM TLB3, 512 KByte Memory Space, Not Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for Periph A Modules&lt;BR /&gt;REM Base address = $C3E0_0000&lt;BR /&gt;REM TLB4, 2 MByte Memory Space, Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Initialize all of the Main SRAM - 512KB&lt;BR /&gt;Initializing RAM from $40000000 to $4007FFFF.&lt;BR /&gt;Initializing Ram Block 0x40000000-0x4007FFFF.&lt;BR /&gt;&lt;BR /&gt;Reset script (D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&amp;amp;E\s32e200_mpc5777c.mac) completed.&lt;BR /&gt;&lt;BR /&gt;&lt;FONT color="#FF6600"&gt;&lt;STRONG&gt;MPC5777C Device detected. &lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF6600"&gt;&lt;STRONG&gt;No breakpoints currently set. &lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF6600"&gt;&lt;STRONG&gt;Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "49779" from 7224&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;STRONG&gt;&lt;FONT color="#FF6600"&gt;Target Disconnected&lt;/FONT&gt;.&lt;/STRONG&gt;&lt;BR /&gt;”&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176235i3BD06DA55E46BD35/image-size/medium?v=v2&amp;amp;px=400" role="button" title="1.PNG" alt="1.PNG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="2.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176236iDD19149859A0A4FE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="2.PNG" alt="2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I really need your help, thank you very much for your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; respectly&lt;/P&gt;</description>
    <pubDate>Thu, 07 Apr 2022 09:53:38 GMT</pubDate>
    <dc:creator>PENGHAN</dc:creator>
    <dc:date>2022-04-07T09:53:38Z</dc:date>
    <item>
      <title>S32 Design Studio for Power Architecture Version 2.1</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-for-Power-Architecture-Version-2-1/m-p/1440475#M8434</link>
      <description>&lt;P&gt;Dear&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;The processor I use is MPC5777C, the debuger I use is Multilink_Universal_FX, and the IDE I use is S32 Design Studio for Power Architecture Version 2.1.I created the project to be able to debug in RAM and flash.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; But I can't download the generated .elf file to flash using the flash from file tool.Attached is the .elf file generated by the project.The compilation information of the console is as follows：&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;“Connection from "127.0.0.1" via 127.0.0.1. Connection from port "49779" to 7224&lt;BR /&gt;Copyright 2018 P&amp;amp;E Microcomputer Systems,Inc.&lt;BR /&gt;Command Line :D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\pegdbserver_power_console -device=MPC5777C -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -port�&lt;BR /&gt;P&amp;amp;E Interface detected - Flash Version 10.81&lt;BR /&gt;Flash Data in range 0x00800000-0x00800007.&lt;BR /&gt;Flash Data in range 0x00800400-0x008006ED.&lt;BR /&gt;Flash Data in range 0x00810000-0x008100F3.&lt;BR /&gt;Flash Data in range 0x00811000-0x00811763.&lt;BR /&gt;Flash Data in range 0x00811770-0x0081B453.&lt;BR /&gt;&lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;Initializing Ram Block 0x00300000-0x00307FFF.&lt;BR /&gt;MPC5777C Device detected.&lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;CMD&amp;gt;CM D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&amp;amp;E\nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;Initializing Ram Block 0x00300000-0x00307FFF.&lt;BR /&gt;MPC5777C Device detected.&lt;BR /&gt;&lt;BR /&gt;DOUBLE BUFFERING enabled.&lt;BR /&gt;Initialized.&lt;BR /&gt;&lt;BR /&gt;;version 1.04, 12/13/2016, Copyright P&amp;amp;E Microcomputer Systems, &lt;A href="http://www.pemicro.com" target="_blank"&gt;www.pemicro.com&lt;/A&gt; [5777C_8meg_highspeed]&lt;BR /&gt;&lt;BR /&gt;;device NXP, MPC5777C, 1x32x2048k, desc=CFlash_highspeed&lt;BR /&gt;&lt;BR /&gt;;begin_cs device=$30800000, length=$00800000, ram=$00300000&lt;BR /&gt;&lt;BR /&gt;Loading programming algorithm ...&lt;BR /&gt;Done.&lt;BR /&gt;Programming sequency is : erase, blank check, program, and verify {default}&lt;BR /&gt;CMD&amp;gt;VC&lt;BR /&gt;Verifying object file CRC-16 to device ranges ...&lt;BR /&gt;block 00800000-00800007 ...&lt;BR /&gt;Ok.&lt;BR /&gt;block 00800400-008006ED ...&lt;BR /&gt;Ok.&lt;BR /&gt;block 00810000-008100F3 ...&lt;BR /&gt;Ok.&lt;BR /&gt;block 00811000-00811763 ...&lt;BR /&gt;Ok.&lt;BR /&gt;block 00811770-0081B453 ...&lt;BR /&gt;Ok.&lt;BR /&gt;Checksum Verification Successful. (Cumulative CRC-16=$9609)&lt;BR /&gt;Application verified in memory. No need to reprogram.&lt;BR /&gt;&lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;Initializing Ram Block 0x00300000-0x00307FFF.&lt;BR /&gt;MPC5777C Device detected.&lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000377&lt;BR /&gt;Device ID revision is $00000001&lt;BR /&gt;&lt;BR /&gt;Starting reset script (D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&amp;amp;E\s32e200_mpc5777c.mac) ...&lt;BR /&gt;REM This script is compatible with MPC5777C devices.&lt;BR /&gt;REM Clean GPRs to remove residual data after using algorithm&lt;BR /&gt;REM Setup MMU for for Periph B Modules&lt;BR /&gt;REM Base address = $FFE0_0000&lt;BR /&gt;REM TLB0, 2 MByte Memory Space, Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU to put internal Flash at 0...&lt;BR /&gt;REM Virtual address 0x0 -&amp;gt; Physical address = $0000_0000&lt;BR /&gt;REM TLB1, 16 MByte Memory Space, Not Guarded, Cachable, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for External Memory&lt;BR /&gt;REM Base address = $2000_0000&lt;BR /&gt;REM TLB2, 16 MByte Memory Space, Not Guarded, Cachable, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for Internal SRAM&lt;BR /&gt;REM Base address = $4000_0000&lt;BR /&gt;REM TLB3, 512 KByte Memory Space, Not Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for Periph A Modules&lt;BR /&gt;REM Base address = $C3E0_0000&lt;BR /&gt;REM TLB4, 2 MByte Memory Space, Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Initialize all of the Main SRAM - 512KB&lt;BR /&gt;Initializing RAM from $40000000 to $4007FFFF.&lt;BR /&gt;Initializing Ram Block 0x40000000-0x4007FFFF.&lt;BR /&gt;&lt;BR /&gt;Reset script (D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&amp;amp;E\s32e200_mpc5777c.mac) completed.&lt;BR /&gt;&lt;BR /&gt;&lt;FONT color="#FF6600"&gt;&lt;STRONG&gt;MPC5777C Device detected. &lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF6600"&gt;&lt;STRONG&gt;No breakpoints currently set. &lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF6600"&gt;&lt;STRONG&gt;Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "49779" from 7224&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;STRONG&gt;&lt;FONT color="#FF6600"&gt;Target Disconnected&lt;/FONT&gt;.&lt;/STRONG&gt;&lt;BR /&gt;”&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176235i3BD06DA55E46BD35/image-size/medium?v=v2&amp;amp;px=400" role="button" title="1.PNG" alt="1.PNG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="2.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176236iDD19149859A0A4FE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="2.PNG" alt="2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I really need your help, thank you very much for your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; respectly&lt;/P&gt;</description>
      <pubDate>Thu, 07 Apr 2022 09:53:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-for-Power-Architecture-Version-2-1/m-p/1440475#M8434</guid>
      <dc:creator>PENGHAN</dc:creator>
      <dc:date>2022-04-07T09:53:38Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design Studio for Power Architecture Version 2.1</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-for-Power-Architecture-Version-2-1/m-p/1441458#M8435</link>
      <description>&lt;P&gt;Hello Penghan,&lt;/P&gt;
&lt;P&gt;It's not clear what the issue is here. The log you provided shows a successful flashing event from using the Flash from File utility. The images you shared are displaying the result of successfully starting a debug session. Each of these is from separate, unrelated, actions. Are you trying to flash or debug? Both appear to be working well.&lt;/P&gt;
&lt;P&gt;Perhaps there is some misunderstanding?&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Fri, 08 Apr 2022 18:35:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-for-Power-Architecture-Version-2-1/m-p/1441458#M8435</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2022-04-08T18:35:12Z</dc:date>
    </item>
  </channel>
</rss>