<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRAppID bootloader tool</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/RAppID-bootloader-tool/m-p/1436943#M8409</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I have used with success the RAppID Bootloader utility via CAN bus (using a Vector CAN to USB hardware) to download my application in the flash of an MPC5644A using the BAM module.&lt;/P&gt;&lt;P&gt;I understand the commucation between RAppID and microcontroller is done via CCP protocol once the .rba algorithm is downloaded to the RAM via the BAM.&lt;/P&gt;&lt;P&gt;As I would like to build my own software / hardware application to interface to the .rba algorithm (instead of using RAppID Bootloader Utility and Vector hardware),&amp;nbsp; I would like to know, if it is possible, which are the parameters of the last CCP command sended to the microcontroller to start the application.&lt;/P&gt;&lt;P&gt;In my example, I have this as the last command:&lt;/P&gt;&lt;P&gt;0x20, 0x82, 0x08, 0x00, 0x38, 0x01, 0x10, 0xAA&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;0x20 is the CCP command code (DIAG_SERVICE command).&lt;/P&gt;&lt;P&gt;0x82 is the CCP message counter.&lt;/P&gt;&lt;P&gt;0x0800 (Motorola format) or 0x0008 (Intel format) is the CCP diagnostic service number (&lt;STRONG&gt;is it always the same?&lt;/STRONG&gt;)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;what are the meanings of the parameters ( 0x38, 0x01, 0x10, 0xAA)?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot in advance to you all,&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;</description>
    <pubDate>Thu, 31 Mar 2022 09:14:27 GMT</pubDate>
    <dc:creator>Gelby</dc:creator>
    <dc:date>2022-03-31T09:14:27Z</dc:date>
    <item>
      <title>RAppID bootloader tool</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/RAppID-bootloader-tool/m-p/1436943#M8409</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I have used with success the RAppID Bootloader utility via CAN bus (using a Vector CAN to USB hardware) to download my application in the flash of an MPC5644A using the BAM module.&lt;/P&gt;&lt;P&gt;I understand the commucation between RAppID and microcontroller is done via CCP protocol once the .rba algorithm is downloaded to the RAM via the BAM.&lt;/P&gt;&lt;P&gt;As I would like to build my own software / hardware application to interface to the .rba algorithm (instead of using RAppID Bootloader Utility and Vector hardware),&amp;nbsp; I would like to know, if it is possible, which are the parameters of the last CCP command sended to the microcontroller to start the application.&lt;/P&gt;&lt;P&gt;In my example, I have this as the last command:&lt;/P&gt;&lt;P&gt;0x20, 0x82, 0x08, 0x00, 0x38, 0x01, 0x10, 0xAA&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;0x20 is the CCP command code (DIAG_SERVICE command).&lt;/P&gt;&lt;P&gt;0x82 is the CCP message counter.&lt;/P&gt;&lt;P&gt;0x0800 (Motorola format) or 0x0008 (Intel format) is the CCP diagnostic service number (&lt;STRONG&gt;is it always the same?&lt;/STRONG&gt;)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;what are the meanings of the parameters ( 0x38, 0x01, 0x10, 0xAA)?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot in advance to you all,&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;</description>
      <pubDate>Thu, 31 Mar 2022 09:14:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/RAppID-bootloader-tool/m-p/1436943#M8409</guid>
      <dc:creator>Gelby</dc:creator>
      <dc:date>2022-03-31T09:14:27Z</dc:date>
    </item>
  </channel>
</rss>