<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: MPC5775E/D Examples and How Tos</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5775E-D-Examples-and-How-Tos/m-p/1425390#M8312</link>
    <description>&lt;P&gt;All the files can be found in SDK folder inside S32DS installation folder.&lt;/P&gt;
&lt;P&gt;An example itself then contains only files needed for that example. The files are generated and added when you click on "Generate code" button in the processor expert. So, when you add new peripheral and change configuration (or also when you load new example), it's necessary to click on "Generate code".&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 09 Mar 2022 15:51:42 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2022-03-09T15:51:42Z</dc:date>
    <item>
      <title>MPC5775E/D Examples and How Tos</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5775E-D-Examples-and-How-Tos/m-p/1424092#M8293</link>
      <description>&lt;P&gt;I'm looking at the suggested links from the MPC5775E-EVB pages and looking for examples. When I get to the Examples page, there are no examples for the MPC5775E. The closest is the 5775K. Is this an error or are there just no examples for the 5775E?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="bchang32_0-1646681909238.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/172675i87612662ACA43F41/image-size/medium?v=v2&amp;amp;px=400" role="button" title="bchang32_0-1646681909238.png" alt="bchang32_0-1646681909238.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Mar 2022 19:40:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5775E-D-Examples-and-How-Tos/m-p/1424092#M8293</guid>
      <dc:creator>bchang32</dc:creator>
      <dc:date>2022-03-07T19:40:18Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775E/D Examples and How Tos</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5775E-D-Examples-and-How-Tos/m-p/1424396#M8300</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;yes, there are no examples for MPC5775E on that page. The closest alternative for MPC5775E is MPC5777C and you can use examples for MPC5777C.&lt;/P&gt;
&lt;P&gt;If you want to use SDK in S32 Design Studio, you can also check examples for MPC5777C. When you create new application project, it offers to use SDK - and it's SDK for MPC5777C which is compatible with MPC5775E.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 08 Mar 2022 07:52:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5775E-D-Examples-and-How-Tos/m-p/1424396#M8300</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-03-08T07:52:44Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775E/D Examples and How Tos</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5775E-D-Examples-and-How-Tos/m-p/1424765#M8306</link>
      <description>&lt;P&gt;Ok, I am looking at the MPC5777C for examples, but I did notice that it appears that there are a handful of unresolved inclusions like Cpu.h, clockMan1.h, pin_mux.h, spi1.h, spi2.h, dmacontroller1.h.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there supposed to be a directory for these header files?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;EDIT: I noticed some of the examples have them, but others dont. eqadc_mpc5777c has the include files while others like adc_pal_eqadc_mpc5777C and spi_pal_mpc5777c doesnt. Are these just errors and the example maker forgot to include? I'm pretty sure I need the spi1 and spi2 headers for the examples.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Mar 2022 19:21:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5775E-D-Examples-and-How-Tos/m-p/1424765#M8306</guid>
      <dc:creator>bchang32</dc:creator>
      <dc:date>2022-03-08T19:21:04Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775E/D Examples and How Tos</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5775E-D-Examples-and-How-Tos/m-p/1425390#M8312</link>
      <description>&lt;P&gt;All the files can be found in SDK folder inside S32DS installation folder.&lt;/P&gt;
&lt;P&gt;An example itself then contains only files needed for that example. The files are generated and added when you click on "Generate code" button in the processor expert. So, when you add new peripheral and change configuration (or also when you load new example), it's necessary to click on "Generate code".&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Mar 2022 15:51:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5775E-D-Examples-and-How-Tos/m-p/1425390#M8312</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-03-09T15:51:42Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775E/D Examples and How Tos</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5775E-D-Examples-and-How-Tos/m-p/1425541#M8314</link>
      <description>&lt;P&gt;Ahh I see now thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I had to click the "Generate Processor Expert Code" under the Project tab in the S32DS SDK.&lt;BR /&gt;&lt;BR /&gt;I may be running a newer version? My "Generate Code" was named the above and under a different tab?&lt;/P&gt;</description>
      <pubDate>Wed, 09 Mar 2022 18:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5775E-D-Examples-and-How-Tos/m-p/1425541#M8314</guid>
      <dc:creator>bchang32</dc:creator>
      <dc:date>2022-03-09T18:37:54Z</dc:date>
    </item>
  </channel>
</rss>