<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Rappid Bootloader on MPC5777C in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Rappid-Bootloader-on-MPC5777C/m-p/1414182#M8205</link>
    <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I would like to consult you for rappid bootloader. I want to summarize my process step by step below.&lt;/P&gt;&lt;P&gt;1) We can load RBF file with JTAG successfully. We changed JTAG algorithms for that. There is no problem here.&lt;/P&gt;&lt;P&gt;2) Then, we can send our s-record with rappid bootloader utility application using uart interface.&lt;/P&gt;&lt;P&gt;However, Our application is not running. In my opinion, rappid bootloader cannot jump to application code.&lt;/P&gt;&lt;P&gt;After observing that, I tried to send same s-record to MPC5777C with JTAG and I saw the collecation as "no need to reprogram" in console but my application have run. As far as I understand, JTAG make the program jump to application code.&lt;/P&gt;&lt;P&gt;By the way, I attached my linker settings below. You should look at:)&lt;/P&gt;&lt;P&gt;To sum up, what could be reason for rappid bootloader cannot jump to application code? Or what is the reason causing this situation? Which point could not I notice?&lt;/P&gt;&lt;P&gt;I am looking forward to hearing your responses.&lt;/P&gt;&lt;P&gt;//////////////////////// main.c&lt;/P&gt;&lt;P&gt;#define MPC57xx_ID 0x005A0000&lt;BR /&gt;#define VLE_ENABLE 0x01000000&lt;BR /&gt;#define RCHW_VAL (MPC57xx_ID /*| VLE_ENABLE*/)&lt;/P&gt;&lt;P&gt;extern void _start(void);&lt;BR /&gt;const volatile uint32_t APPKEY __attribute__ ((section(".appkey"))) = 0x55AA55AA;&lt;BR /&gt;const uint32_t __attribute__ ((section(".rchw"))) RCHW [] = {&lt;BR /&gt;RCHW_VAL,&lt;BR /&gt;/* cpu0_reset_vector */ (uint32_t)_start,&lt;BR /&gt;/* delay */ 0x2DC6C0, // 3 sec&lt;BR /&gt;/* application key */ (uint32_t)&amp;amp;APPKEY&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;///////////////////// linker&lt;/P&gt;&lt;P&gt;FLASH_BASE_ADDR = DEFINED(__flash_base_addr__) ? __flash_base_addr__ : 0x00840024;&lt;BR /&gt;FLASH_SIZE = DEFINED(__flash_size__) ? __flash_size__ : 4096K - 0x24;&lt;/P&gt;&lt;P&gt;/* Define SRAM */&lt;BR /&gt;SRAM_BASE_ADDR = DEFINED(__sram_base_addr__) ? __sram_base_addr__ : 0x40000000;&lt;BR /&gt;SRAM_SIZE = DEFINED(__sram_size__) ? __sram_size__ : 256K;&lt;/P&gt;&lt;P&gt;MEMORY&lt;BR /&gt;{&lt;BR /&gt;/*&lt;BR /&gt;flash_rchw : org = 0x00800000, len = 0x4&lt;BR /&gt;cpu0_reset_vec : org = 0x00800000+0x04, len = 0x4&lt;BR /&gt;&lt;BR /&gt;*/&lt;BR /&gt;flash_rchw : org = 0x00840000, len = 0x20&lt;BR /&gt;cpu0_reset_vec : org = 0x00840000+0x20, len = 0x4&lt;/P&gt;&lt;P&gt;m_text : org = FLASH_BASE_ADDR, len = FLASH_SIZE&lt;BR /&gt;m_data : org = SRAM_BASE_ADDR, len = SRAM_SIZE&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;Sincerely.&lt;/P&gt;</description>
    <pubDate>Wed, 16 Feb 2022 06:41:43 GMT</pubDate>
    <dc:creator>berat24</dc:creator>
    <dc:date>2022-02-16T06:41:43Z</dc:date>
    <item>
      <title>Rappid Bootloader on MPC5777C</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Rappid-Bootloader-on-MPC5777C/m-p/1414182#M8205</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I would like to consult you for rappid bootloader. I want to summarize my process step by step below.&lt;/P&gt;&lt;P&gt;1) We can load RBF file with JTAG successfully. We changed JTAG algorithms for that. There is no problem here.&lt;/P&gt;&lt;P&gt;2) Then, we can send our s-record with rappid bootloader utility application using uart interface.&lt;/P&gt;&lt;P&gt;However, Our application is not running. In my opinion, rappid bootloader cannot jump to application code.&lt;/P&gt;&lt;P&gt;After observing that, I tried to send same s-record to MPC5777C with JTAG and I saw the collecation as "no need to reprogram" in console but my application have run. As far as I understand, JTAG make the program jump to application code.&lt;/P&gt;&lt;P&gt;By the way, I attached my linker settings below. You should look at:)&lt;/P&gt;&lt;P&gt;To sum up, what could be reason for rappid bootloader cannot jump to application code? Or what is the reason causing this situation? Which point could not I notice?&lt;/P&gt;&lt;P&gt;I am looking forward to hearing your responses.&lt;/P&gt;&lt;P&gt;//////////////////////// main.c&lt;/P&gt;&lt;P&gt;#define MPC57xx_ID 0x005A0000&lt;BR /&gt;#define VLE_ENABLE 0x01000000&lt;BR /&gt;#define RCHW_VAL (MPC57xx_ID /*| VLE_ENABLE*/)&lt;/P&gt;&lt;P&gt;extern void _start(void);&lt;BR /&gt;const volatile uint32_t APPKEY __attribute__ ((section(".appkey"))) = 0x55AA55AA;&lt;BR /&gt;const uint32_t __attribute__ ((section(".rchw"))) RCHW [] = {&lt;BR /&gt;RCHW_VAL,&lt;BR /&gt;/* cpu0_reset_vector */ (uint32_t)_start,&lt;BR /&gt;/* delay */ 0x2DC6C0, // 3 sec&lt;BR /&gt;/* application key */ (uint32_t)&amp;amp;APPKEY&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;///////////////////// linker&lt;/P&gt;&lt;P&gt;FLASH_BASE_ADDR = DEFINED(__flash_base_addr__) ? __flash_base_addr__ : 0x00840024;&lt;BR /&gt;FLASH_SIZE = DEFINED(__flash_size__) ? __flash_size__ : 4096K - 0x24;&lt;/P&gt;&lt;P&gt;/* Define SRAM */&lt;BR /&gt;SRAM_BASE_ADDR = DEFINED(__sram_base_addr__) ? __sram_base_addr__ : 0x40000000;&lt;BR /&gt;SRAM_SIZE = DEFINED(__sram_size__) ? __sram_size__ : 256K;&lt;/P&gt;&lt;P&gt;MEMORY&lt;BR /&gt;{&lt;BR /&gt;/*&lt;BR /&gt;flash_rchw : org = 0x00800000, len = 0x4&lt;BR /&gt;cpu0_reset_vec : org = 0x00800000+0x04, len = 0x4&lt;BR /&gt;&lt;BR /&gt;*/&lt;BR /&gt;flash_rchw : org = 0x00840000, len = 0x20&lt;BR /&gt;cpu0_reset_vec : org = 0x00840000+0x20, len = 0x4&lt;/P&gt;&lt;P&gt;m_text : org = FLASH_BASE_ADDR, len = FLASH_SIZE&lt;BR /&gt;m_data : org = SRAM_BASE_ADDR, len = SRAM_SIZE&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;Sincerely.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Feb 2022 06:41:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Rappid-Bootloader-on-MPC5777C/m-p/1414182#M8205</guid>
      <dc:creator>berat24</dc:creator>
      <dc:date>2022-02-16T06:41:43Z</dc:date>
    </item>
    <item>
      <title>Re: Rappid Bootloader on MPC5777C</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Rappid-Bootloader-on-MPC5777C/m-p/1417040#M8223</link>
      <description>&lt;P&gt;&lt;FONT size="4"&gt;Hello Berat,&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT size="4"&gt;Here are some details on the MPC5777C implementation for RAppID Bootloader, which you may find useful:&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;H2&gt;4.6&amp;nbsp;&lt;SPAN&gt;MPC5777C&lt;/SPAN&gt; Family&lt;/H2&gt;
&lt;TABLE width="684"&gt;
&lt;TBODY&gt;
&lt;TR&gt;
&lt;TD rowspan="2" width="96"&gt;
&lt;P&gt;&lt;STRONG&gt;Device&lt;/STRONG&gt;&lt;/P&gt;
&lt;/TD&gt;
&lt;TD colspan="2" width="180"&gt;
&lt;P&gt;&lt;STRONG&gt;Communication supported&lt;/STRONG&gt;&lt;/P&gt;
&lt;/TD&gt;
&lt;TD rowspan="2" width="114"&gt;
&lt;P&gt;&lt;STRONG&gt;Device tested&lt;/STRONG&gt;&lt;/P&gt;
&lt;/TD&gt;
&lt;TD rowspan="2" width="102"&gt;
&lt;P&gt;&lt;STRONG&gt;RBF file&lt;/STRONG&gt;&lt;/P&gt;
&lt;/TD&gt;
&lt;TD colspan="2" width="192"&gt;
&lt;P&gt;&lt;STRONG&gt;Boot-loader areas&lt;/STRONG&gt;&lt;/P&gt;
&lt;/TD&gt;
&lt;/TR&gt;
&lt;TR&gt;
&lt;TD width="90"&gt;
&lt;P&gt;CAN&lt;/P&gt;
&lt;P&gt;(500Kb/s)&lt;/P&gt;
&lt;/TD&gt;
&lt;TD width="90"&gt;
&lt;P&gt;UART&lt;/P&gt;
&lt;P&gt;(115200b/s)&lt;/P&gt;
&lt;/TD&gt;
&lt;TD width="90"&gt;
&lt;P&gt;rchw&lt;/P&gt;
&lt;/TD&gt;
&lt;TD width="102"&gt;
&lt;P&gt;m_text&lt;/P&gt;
&lt;/TD&gt;
&lt;/TR&gt;
&lt;TR&gt;
&lt;TD width="96"&gt;
&lt;P&gt;MPC5777C&lt;/P&gt;
&lt;/TD&gt;
&lt;TD width="90"&gt;
&lt;P&gt;CAN0&lt;/P&gt;
&lt;P&gt;(PB0-PB1)&lt;/P&gt;
&lt;/TD&gt;
&lt;TD width="90"&gt;
&lt;P&gt;UART0&lt;/P&gt;
&lt;P&gt;(PC8-PC9)&lt;/P&gt;
&lt;/TD&gt;
&lt;TD width="114"&gt;
&lt;P&gt;MPC5777CTMME3 – 1N45H&lt;/P&gt;
&lt;P&gt;MPC5777CTMME3 – 0N45H&lt;/P&gt;
&lt;/TD&gt;
&lt;TD width="102"&gt;
&lt;P&gt;MPC5777C.rbf&lt;/P&gt;
&lt;/TD&gt;
&lt;TD width="90"&gt;
&lt;P&gt;0x00800000-&lt;/P&gt;
&lt;P&gt;0x008003FF&lt;/P&gt;
&lt;/TD&gt;
&lt;TD width="102"&gt;
&lt;P&gt;0x00800400-&lt;/P&gt;
&lt;P&gt;0x0083FFFF&lt;/P&gt;
&lt;/TD&gt;
&lt;/TR&gt;
&lt;/TBODY&gt;
&lt;/TABLE&gt;
&lt;UL class="lia-list-style-type-square"&gt;
&lt;LI&gt;&lt;STRONG&gt;RCHW and KEY used in the application&lt;/STRONG&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P data-unlink="true"&gt;Please refer to section 5.2&amp;nbsp;for defining the value of RCHW and KEY&lt;/P&gt;
&lt;P data-unlink="true"&gt;Please refer to section &lt;SPAN&gt;6.2&amp;nbsp;&lt;/SPAN&gt;for setting up the application project with S32DS tool&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;STRONG&gt;Notes&lt;/STRONG&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;The MPC5777C RBF boot-loader occupies 16K memory blocks starting at 0x00800000.&lt;/P&gt;
&lt;P&gt;The user application is allowed on RAM from the base address + 0x1400 to the end of RAM&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;H1&gt;&lt;FONT size="6"&gt;5. How to use RCHW and KEY in the application&lt;/FONT&gt;&lt;/H1&gt;
&lt;H2&gt;5.2. PowerPC Targets&lt;/H2&gt;
&lt;P&gt;Before starting the application, the boot-loader will search for RCHW and KEY value in the application. If found, the boot-loader will consider the application suitable and run it. Otherwise, the boot-loader will not run the application and stay in waiting mode.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;RCHW: the value of this variable will be programmed into the first 4 bytes of the application.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;The only value for RCHW is 0x005A0000&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The KEY value is set at the last position of the application.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;The only value for KEY is 0x55AA55AA&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;H1&gt;&lt;FONT size="6"&gt;6. Project setup on S32 Design Studio&lt;/FONT&gt;&lt;/H1&gt;
&lt;H2&gt;6.2. PowerPC Architecture&lt;/H2&gt;
&lt;UL&gt;
&lt;LI&gt;Open S32DS for Power Architecture&lt;/LI&gt;
&lt;LI&gt;Create a new default project wizard&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 594px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171280i8F9ACEE0D0201E38/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;image.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Figure 6.2.1&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Change the “flashchw.c” file by adding the following piece of code:&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;STRONG&gt;#if&lt;/STRONG&gt; defined(START_FROM_FLASH)&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;#include&lt;/STRONG&gt; "typedefs.h"&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt; MPC57xx_ID 0x005A0000 /* RCHW boot ID for MPC57xx devices */&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt; VLE_ENABLE 0x01000000 /* VLE is enabled */&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt; CPU2_ENABLED 0x00000001&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt; CPU0_ENABLED 0x00000002&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt; CPU1_ENABLED 0x00000008&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;extern&lt;/STRONG&gt; &lt;STRONG&gt;void&lt;/STRONG&gt; &lt;STRONG&gt;_start&lt;/STRONG&gt;(&lt;STRONG&gt;void&lt;/STRONG&gt;);&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;extern&lt;/STRONG&gt; &lt;STRONG&gt;void&lt;/STRONG&gt; &lt;STRONG&gt;_startcore1&lt;/STRONG&gt;(&lt;STRONG&gt;void&lt;/STRONG&gt;);&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;extern&lt;/STRONG&gt; &lt;STRONG&gt;void&lt;/STRONG&gt; &lt;STRONG&gt;_startcore2&lt;/STRONG&gt;(&lt;STRONG&gt;void&lt;/STRONG&gt;);&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt; TARGET_CORES (CPU0_ENABLED | CPU1_ENABLED | CPU2_ENABLED)&lt;/P&gt;
&lt;P&gt;//#define RCHW_VAL (MPC57xx_ID | TARGET_CORES)&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt; RCHW_VAL 0x005A0000&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;const&lt;/STRONG&gt; &lt;STRONG&gt;volatile&lt;/STRONG&gt; uint32_t APPKEY &lt;STRONG&gt;__attribute__&lt;/STRONG&gt; ((section(".&lt;U&gt;appkey&lt;/U&gt;"))) = 0x55AA55AA;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;const&lt;/STRONG&gt; uint32_t &lt;STRONG&gt;__attribute__&lt;/STRONG&gt; ((section(".&lt;U&gt;rchw&lt;/U&gt;"))) RCHW [] = {&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RCHW_VAL,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* cpu0_reset_vector */ (uint32_t)_start,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* delay */&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x2DC6C0,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // 3 &lt;U&gt;sec&lt;/U&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* application key */ (uint32_t)&amp;amp;APPKEY,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* cpu2_reset_vector */ (uint32_t)_startcore2,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* cpu1_reset_vector */ (uint32_t)_startcore1};&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;#endif&lt;/STRONG&gt; /* defined(START_FROM_FLASH) */&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Modify the linker file as shown below by adding a new line *(.appKey) into the .text segment:&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 592px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171281i881AEC94D5393DCC/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;image.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Figure 6.2.2 &lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The example output .srec file generated by the compiler integrated in S32 Design Studio:&lt;/LI&gt;
&lt;LI&gt;The first part of the file:&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 586px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171285iAE31B090D4FDC4EC/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;image.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Figure 6.2.3&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The last part of the file:&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 584px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171283iCB0C6E50974B78A3/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;image.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Figure 6.2.4&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I have also attached an example MPC5777C application example setup for RAppID Bootloader as well as some images of the steps required to implement it in a new application. I hope that you will find those useful as well. Your issue is not obvious, but I think with these provided details and example, you should be able to identify where the issue is with your setup.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 00:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Rappid-Bootloader-on-MPC5777C/m-p/1417040#M8223</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2022-02-22T00:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: Rappid Bootloader on MPC5777C</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Rappid-Bootloader-on-MPC5777C/m-p/1417533#M8236</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/83694"&gt;@mikedoidge&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;First of all, I appreciate you for your precious answer.&lt;/P&gt;&lt;P&gt;I downloaded your example for rappid bootloader. Firstly, I loaded it to MPC with JTAG and it worked.&lt;/P&gt;&lt;P&gt;Then, I tried to load your code with rappid. As I did before, I loaded rappid bootloader s-record with JTAG. Then, I built your code again and I sent s-record by utility app. However, it did not run and I saw same behaviour.&lt;/P&gt;&lt;P&gt;You added s-record pictures on your response. When I looked at these photos, you generated the kind of s2 and s3 record with together but I generated S3. This could be reason?&lt;/P&gt;&lt;P&gt;I attached my s-record below. Could you check it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 14:03:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Rappid-Bootloader-on-MPC5777C/m-p/1417533#M8236</guid>
      <dc:creator>berat24</dc:creator>
      <dc:date>2022-02-22T14:03:57Z</dc:date>
    </item>
  </channel>
</rss>