<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックHow to change device package for existing project?</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-change-device-package-for-existing-project/m-p/1413295#M8199</link>
    <description>&lt;P&gt;Once a project is created in S32DS, how is it possible to change the device package?&lt;/P&gt;&lt;P&gt;For example, the i2c_HLD_Example_S32K148 uses the LQFP176 package. What if I want to use a smaller package, such as LQFP64? Where do I change this setting?&lt;/P&gt;&lt;P&gt;A similar question was asked and answered on the forum in 2018, but the software has changed a lot since then and the answer no longer applies.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 14 Feb 2022 23:38:05 GMT</pubDate>
    <dc:creator>hns80</dc:creator>
    <dc:date>2022-02-14T23:38:05Z</dc:date>
    <item>
      <title>How to change device package for existing project?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-change-device-package-for-existing-project/m-p/1413295#M8199</link>
      <description>&lt;P&gt;Once a project is created in S32DS, how is it possible to change the device package?&lt;/P&gt;&lt;P&gt;For example, the i2c_HLD_Example_S32K148 uses the LQFP176 package. What if I want to use a smaller package, such as LQFP64? Where do I change this setting?&lt;/P&gt;&lt;P&gt;A similar question was asked and answered on the forum in 2018, but the software has changed a lot since then and the answer no longer applies.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Feb 2022 23:38:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-change-device-package-for-existing-project/m-p/1413295#M8199</guid>
      <dc:creator>hns80</dc:creator>
      <dc:date>2022-02-14T23:38:05Z</dc:date>
    </item>
    <item>
      <title>Re: How to change device package for existing project?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-change-device-package-for-existing-project/m-p/1413317#M8200</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is no &lt;SPAN&gt;LQFP64&amp;nbsp;&lt;/SPAN&gt;S32K148, so you can not change the package to it. Since you did not mention the version of S32DS, it is assumed that you are using the latest version of &lt;A href="https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for-s32-platform:S32DS-S32PLATFORM" target="_self"&gt;S32 design studio for S32 platform 3.4&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Please change the package by using &lt;EM class="qkunPe"&gt;S32 Configuration Tool -&amp;gt;&amp;nbsp;&lt;/EM&gt;&lt;STRONG&gt;Switch package for the Processor&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Switch package for the Processor.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/170502iAA1D180528800CA2/image-size/large?v=v2&amp;amp;px=999" role="button" title="Switch package for the Processor.png" alt="Switch package for the Processor.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Switch package for the Processor.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 15 Feb 2022 00:55:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-change-device-package-for-existing-project/m-p/1413317#M8200</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-02-15T00:55:57Z</dc:date>
    </item>
  </channel>
</rss>