<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Use windriver diab to create library project in S32DS</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Use-windriver-diab-to-create-library-project-in-S32DS/m-p/1401091#M8150</link>
    <description>&lt;P&gt;I am running into this same issue. I am able to create an application project and select the diab tools but when I try to create a library there is no option to select the diab tools. Is there a way to do this? I'm using the latest version of S32 DS for Power Architecture.&lt;/P&gt;</description>
    <pubDate>Tue, 18 Jan 2022 17:44:05 GMT</pubDate>
    <dc:creator>elizabeth_gerag</dc:creator>
    <dc:date>2022-01-18T17:44:05Z</dc:date>
    <item>
      <title>Use windriver diab to create library project in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Use-windriver-diab-to-create-library-project-in-S32DS/m-p/836933#M3983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Now,I can create a "Elf S32DS project" with windriver diab toolchain.But I want to create a "Library project" with windriver diab.I have no choice but gcc.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;So, how can I create library project in S32DS with windriver toochain?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Image 2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65995i026FEB920C93FED4/image-size/large?v=v2&amp;amp;px=999" role="button" title="Image 2.png" alt="Image 2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Image 3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65996iF0EE93AA4FE18EE5/image-size/large?v=v2&amp;amp;px=999" role="button" title="Image 3.png" alt="Image 3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help will be appreciated!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2018 09:14:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Use-windriver-diab-to-create-library-project-in-S32DS/m-p/836933#M3983</guid>
      <dc:creator>xiaofangu</dc:creator>
      <dc:date>2018-07-20T09:14:39Z</dc:date>
    </item>
    <item>
      <title>Re: Use windriver diab to create library project in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Use-windriver-diab-to-create-library-project-in-S32DS/m-p/1401091#M8150</link>
      <description>&lt;P&gt;I am running into this same issue. I am able to create an application project and select the diab tools but when I try to create a library there is no option to select the diab tools. Is there a way to do this? I'm using the latest version of S32 DS for Power Architecture.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jan 2022 17:44:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Use-windriver-diab-to-create-library-project-in-S32DS/m-p/1401091#M8150</guid>
      <dc:creator>elizabeth_gerag</dc:creator>
      <dc:date>2022-01-18T17:44:05Z</dc:date>
    </item>
    <item>
      <title>Re: Use windriver diab to create library project in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Use-windriver-diab-to-create-library-project-in-S32DS/m-p/1455075#M8552</link>
      <description>&lt;P&gt;Any updates on this? I'm facing the same problem right now. I cannot create a new project for a library using DIAB as a compiler, it only allows the Standard S32DS toolchain&lt;/P&gt;</description>
      <pubDate>Mon, 09 May 2022 15:33:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Use-windriver-diab-to-create-library-project-in-S32DS/m-p/1455075#M8552</guid>
      <dc:creator>mikel1</dc:creator>
      <dc:date>2022-05-09T15:33:24Z</dc:date>
    </item>
    <item>
      <title>Re: Use windriver diab to create library project in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Use-windriver-diab-to-create-library-project-in-S32DS/m-p/1455109#M8553</link>
      <description>&lt;P&gt;What I ended up doing was creating the library project with the default tools. I then went into the Tool Chain Editor in the Project Properties under C/C++Build to change it. I had to unselect the "Display compatible toolchains only" options and then I could select diab. It's been awhile so I think there may have been a couple of other changes like setting the compiler path too. I don't understand why it's considered an incompatible toolchain and not selectable when the project is created, seems like a bug. &amp;nbsp;Hope this helps you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="elizabeth_gerag_1-1652113055775.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/179229iCAEF428AFECA1DC9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="elizabeth_gerag_1-1652113055775.png" alt="elizabeth_gerag_1-1652113055775.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 09 May 2022 16:24:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Use-windriver-diab-to-create-library-project-in-S32DS/m-p/1455109#M8553</guid>
      <dc:creator>elizabeth_gerag</dc:creator>
      <dc:date>2022-05-09T16:24:36Z</dc:date>
    </item>
    <item>
      <title>Re: Use windriver diab to create library project in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Use-windriver-diab-to-create-library-project-in-S32DS/m-p/1455471#M8558</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I can confirm that for library project DIAB can't be selected. You can create executable project and change project type in Project Properties:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jiri_kral_0-1652169197853.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/179314iCF93B26D861BD545/image-size/large?v=v2&amp;amp;px=999" role="button" title="jiri_kral_0-1652169197853.png" alt="jiri_kral_0-1652169197853.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 May 2022 07:53:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Use-windriver-diab-to-create-library-project-in-S32DS/m-p/1455471#M8558</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2022-05-10T07:53:38Z</dc:date>
    </item>
  </channel>
</rss>