<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Flash linker file generated for MCP5748G is incorrect</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-linker-file-generated-for-MCP5748G-is-incorrect/m-p/1397550#M8129</link>
    <description>&lt;P&gt;If the issue is related to SDK projects only, you can reinstall only the SDK, you don't need perform full S32DS reinstall.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 11 Jan 2022 18:06:52 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2022-01-11T18:06:52Z</dc:date>
    <item>
      <title>Flash linker file generated for MCP5748G is incorrect</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-linker-file-generated-for-MCP5748G-is-incorrect/m-p/1395050#M8117</link>
      <description>&lt;P&gt;When I create a new project for the MPC5748G and select the S32_SDK_S32PA_RTM_3.0.3 or the S32_SDK_S32PA_RTM_3.0.0 as the SDK the Flash linker file does not match what I configured the file to be. No matter what I do the following is generated&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/* Define FLASH */&lt;/P&gt;&lt;P&gt;FLASH_BASE_ADDR = DEFINED(__flash_base_addr__) ? __flash_base_addr__ : 0x012C0000;&lt;/P&gt;&lt;P&gt;FLASH_SIZE =&amp;nbsp; DEFINED(__flash_size__) ? __flash_size__ : 1856K;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/* Define SRAM */&lt;/P&gt;&lt;P&gt;SRAM_BASE_ADDR = DEFINED(__sram_base_addr__) ? __sram_base_addr__ : 0x40000000;&lt;/P&gt;&lt;P&gt;SRAM_SIZE = DEFINED(__sram_size__) ? __sram_size__ : 256K;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 20:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Flash-linker-file-generated-for-MCP5748G-is-incorrect/m-p/1395050#M8117</guid>
      <dc:creator>MattJCole</dc:creator>
      <dc:date>2022-01-05T20:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: Flash linker file generated for MCP5748G is incorrect</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-linker-file-generated-for-MCP5748G-is-incorrect/m-p/1397435#M8128</link>
      <description>&lt;P&gt;Hi Matt,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Looks that your linker file script template was modified - on my side is used Large block NVM (0x01000000). You can try to reinstall S32DS. With SDK are files used as linked resource - once you modify it - it is modified for all examples/projects which uses SDK. If you like to use your own linker script file, make a copy and add it into your project.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jiri&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jan 2022 14:15:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Flash-linker-file-generated-for-MCP5748G-is-incorrect/m-p/1397435#M8128</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2022-01-11T14:15:34Z</dc:date>
    </item>
    <item>
      <title>Re: Flash linker file generated for MCP5748G is incorrect</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-linker-file-generated-for-MCP5748G-is-incorrect/m-p/1397550#M8129</link>
      <description>&lt;P&gt;If the issue is related to SDK projects only, you can reinstall only the SDK, you don't need perform full S32DS reinstall.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jan 2022 18:06:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Flash-linker-file-generated-for-MCP5748G-is-incorrect/m-p/1397550#M8129</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2022-01-11T18:06:52Z</dc:date>
    </item>
  </channel>
</rss>