<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: download program via PE error</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/download-program-via-PE-error/m-p/1388657#M8078</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Sorry for the late reply&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;the VERSION of SD32DS we are using now should be ok (it has been successfully used on the development board), we used SBC chip (FS8510) to power in debug mode &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 17 Dec 2021 08:38:22 GMT</pubDate>
    <dc:creator>wxf</dc:creator>
    <dc:date>2021-12-17T08:38:22Z</dc:date>
    <item>
      <title>download program via PE error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/download-program-via-PE-error/m-p/1367270#M7935</link>
      <description>&lt;P&gt;dear all,&lt;BR /&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&amp;nbsp; When I download the program to MPC5775E through PE, the following error is generated:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;"error during flash programming. Terminating debug session."&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;with the console information as follows:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;"Once Status Register Result = $0209&lt;BR /&gt;REM Set up MMU for Periph A Modules&lt;BR /&gt;REM Base address = $C3E0_0000&lt;BR /&gt;REM TLB4, 2 MByte Memory Space, Guarded, Don't Cache, All Access&lt;BR /&gt;Once Status Register Result = $0209&lt;BR /&gt;REM Initialize all of the Main SRAM - 512KB&lt;BR /&gt;Initializing RAM from $40000000 to $4007FFFF.&lt;BR /&gt;&lt;BR /&gt;Reset script (D:\Program Files\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.7.201906071634\win32\gdi\P&amp;amp;E\s32e200_mpc5777c.mac) completed.&lt;BR /&gt;&lt;BR /&gt;MPC5777C Device detected.&lt;BR /&gt;PE-ERROR: Error downloading to the device.&lt;BR /&gt;Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "59345" from 7224&lt;BR /&gt;Target Disconnected."&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Can you tell me how this happened and how to resolve it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;tank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;XiufengWang&lt;/P&gt;</description>
      <pubDate>Fri, 05 Nov 2021 09:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/download-program-via-PE-error/m-p/1367270#M7935</guid>
      <dc:creator>wxf</dc:creator>
      <dc:date>2021-11-05T09:38:57Z</dc:date>
    </item>
    <item>
      <title>download program via PE error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/download-program-via-PE-error/m-p/1367828#M7936</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Are you using a custom board or an NXP evaluation board?&lt;/P&gt;
&lt;P&gt;I'd recommend you to create a new dummy single core project for MPC57775E.&lt;/P&gt;
&lt;P&gt;Build the project and debug via PE.&lt;/P&gt;
&lt;P&gt;First I'd start with Debug_RAM build configuration - no flash programming involved.&lt;/P&gt;
&lt;P&gt;Then I'd repeat the test with Debug_FLASH build configuration&lt;/P&gt;
&lt;P&gt;If you are able to debug&amp;nbsp; both - the issue is related to your custom project . Typically could be an issue in linker&amp;nbsp;file (e.g. section placement into unavailable memory) causing programming algorithm to fail.&lt;/P&gt;
&lt;P&gt;Hope it&amp;nbsp; helps.&lt;/P&gt;
&lt;P&gt;Stan&lt;/P&gt;</description>
      <pubDate>Mon, 08 Nov 2021 09:56:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/download-program-via-PE-error/m-p/1367828#M7936</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2021-11-08T09:56:41Z</dc:date>
    </item>
    <item>
      <title>Re: download program via PE error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/download-program-via-PE-error/m-p/1367853#M7937</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Thank you for your reply&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;I created an empty project, and I can download the program with Debug_Ram successfully, but the result is still the same error with Debug_Flash.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;The board we use is a custom board&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Nov 2021 10:44:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/download-program-via-PE-error/m-p/1367853#M7937</guid>
      <dc:creator>wxf</dc:creator>
      <dc:date>2021-11-08T10:44:59Z</dc:date>
    </item>
    <item>
      <title>Re: download program via PE error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/download-program-via-PE-error/m-p/1375613#M7993</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;could you check the reset signal while programming flash? Do you use SBC chip on your custom board?&lt;/P&gt;
&lt;P&gt;Also I'd recommend you to instal the latest S32DS update (it includes the latest version of pemicro plugin):&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-Power-Architecture-v2-1-Update-14/ta-p/1195749" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-Power-Architecture-v2-1-Update-14/ta-p/1195749&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Stan&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Nov 2021 12:06:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/download-program-via-PE-error/m-p/1375613#M7993</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2021-11-23T12:06:48Z</dc:date>
    </item>
    <item>
      <title>Re: download program via PE error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/download-program-via-PE-error/m-p/1388657#M8078</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Sorry for the late reply&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;the VERSION of SD32DS we are using now should be ok (it has been successfully used on the development board), we used SBC chip (FS8510) to power in debug mode &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Dec 2021 08:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/download-program-via-PE-error/m-p/1388657#M8078</guid>
      <dc:creator>wxf</dc:creator>
      <dc:date>2021-12-17T08:38:22Z</dc:date>
    </item>
  </channel>
</rss>