<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Bootloader for MPC5748G</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/1359691#M7896</link>
    <description>&lt;P&gt;Hi!&amp;nbsp; I am trying to follow Stanish's instruction to try the BootLoader_MPC5748G example on my DEVKit-MPC5748G board.&amp;nbsp; But I got the following error when trying to flash the BootLoader_MPC5748G.RBF to the board.&amp;nbsp; Could someone please help me?&amp;nbsp; Thanks!&lt;/P&gt;&lt;P&gt;Connection from "127.0.0.1" via 127.0.0.1. Connection from port "55762" to 7224&lt;BR /&gt;Copyright 2018 P&amp;amp;E Microcomputer Systems,Inc.&lt;BR /&gt;Command Line :C:\nxp\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\win32\pegdbserver_power_console -device=MPC5748G -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=OPENSDA -speed=5000 -port=USB1Ø&lt;BR /&gt;OpenSDA detected - Flash Version 1.10&lt;BR /&gt;Flash Data in range 0x00F8C000-0x00F8C01B.&lt;BR /&gt;Flash Data in range 0x00F8C020-0x00F8DC0B.&lt;BR /&gt;&lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000082&lt;BR /&gt;Device ID revision is $00000000&lt;BR /&gt;Initializing Ram Block 0x40000000-0x40007FFF.&lt;BR /&gt;MPC574xC Device detected.&lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;CMD&amp;gt;CM C:\nxp\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\win32\gdi\P&amp;amp;E\nxp_mpc5748g_1x32x1520k_cflash.pcp&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000082&lt;BR /&gt;Device ID revision is $00000000&lt;BR /&gt;Initializing Ram Block 0x40000000-0x40007FFF.&lt;BR /&gt;MPC574xC Device detected.&lt;BR /&gt;&lt;BR /&gt;DOUBLE BUFFERING enabled.&lt;BR /&gt;Initialized.&lt;BR /&gt;&lt;BR /&gt;;version 1.05, 06/26/2017, Copyright P&amp;amp;E Microcomputer Systems, &lt;A href="http://www.pemicro.com" target="_blank"&gt;www.pemicro.com&lt;/A&gt; [5748G_6080k]&lt;BR /&gt;&lt;BR /&gt;;device NXP, MPC5748G, 1x32x1520k, desc=CFlash&lt;BR /&gt;&lt;BR /&gt;;begin_cs device=$00F90000, length=$005F0000, ram=$40000000&lt;BR /&gt;&lt;BR /&gt;Loading programming algorithm ...&lt;BR /&gt;Done.&lt;BR /&gt;Programming sequency is : erase, blank check, program, and verify {default}&lt;BR /&gt;CMD&amp;gt;VC&lt;BR /&gt;Verifying object file CRC-16 to device ranges ...&lt;BR /&gt;Error - no valid data in range of module.&lt;BR /&gt;Current content of flash does not match application to be programmed&lt;BR /&gt;CMD&amp;gt;EM&lt;BR /&gt;&lt;BR /&gt;Erasing.&lt;BR /&gt;Module has been erased.&lt;BR /&gt;CMD&amp;gt;PM&lt;BR /&gt;&lt;BR /&gt;Programming.&lt;BR /&gt;Processing Object File Data ...&lt;BR /&gt;&lt;BR /&gt;No data to program.&lt;BR /&gt;&lt;BR /&gt;.&lt;BR /&gt;Error during programming.&lt;BR /&gt;Error Programming flash of device&lt;BR /&gt;Error occured during Flash programming.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000082&lt;BR /&gt;Device ID revision is $00000000&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000082&lt;BR /&gt;Device ID revision is $00000000&lt;BR /&gt;&lt;BR /&gt;Starting reset script (C:\nxp\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\win32\gdi\P&amp;amp;E\s32e200_mpc574xg.mac) ...&lt;BR /&gt;REM This script is compatible with MPC574xG devices.&lt;BR /&gt;REM Clean GPRs to remove residual data after using algorithm&lt;BR /&gt;REM Initialize all of the Main SRAM - 768KB&lt;BR /&gt;Initializing RAM from $40000000 to $400BFFFF.&lt;BR /&gt;Initializing Ram Block 0x40000000-0x400BFFFF.&lt;BR /&gt;&lt;BR /&gt;Reset script (C:\nxp\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\win32\gdi\P&amp;amp;E\s32e200_mpc574xg.mac) completed.&lt;BR /&gt;&lt;BR /&gt;MPC574xG Device detected.&lt;/P&gt;&lt;P&gt;PEmicro GDB Launch Failure : Error during flash programming. Terminating debug session.&lt;/P&gt;</description>
    <pubDate>Thu, 21 Oct 2021 20:16:19 GMT</pubDate>
    <dc:creator>jzhang</dc:creator>
    <dc:date>2021-10-21T20:16:19Z</dc:date>
    <item>
      <title>Bootloader for MPC5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/677237#M1403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see a 'BootLoader_MPC5748G' example in S32. It compiles successfully.&lt;/P&gt;&lt;P&gt;"BootLoader_MPC5748G.elf" and "BootLoader_MPC5748G.srec" is generated. Bit I do not see a binary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to flash the bootloader to devkit? And what is the expected output?&lt;/P&gt;&lt;P&gt;Also can you throw some light on what kind of bootloader it is?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Tiju&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 19:16:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/677237#M1403</guid>
      <dc:creator>tiju</dc:creator>
      <dc:date>2017-07-20T19:16:42Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader for MPC5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/677238#M1404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Tiju,&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is txt document - description which explains this boot loader. &amp;nbsp;&lt;/P&gt;&lt;P&gt;You need have openSDA interface for your hardware to get this boot loader working.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Udit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Jul 2017 11:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/677238#M1404</guid>
      <dc:creator>uditsalunke</dc:creator>
      <dc:date>2017-07-23T11:33:55Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader for MPC5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/677239#M1405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Udit,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking for a bootloader that can run directly on MPC5748G without using OpenSDA. Can you help me with that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Tiju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Jul 2017 21:15:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/677239#M1405</guid>
      <dc:creator>tiju</dc:creator>
      <dc:date>2017-07-23T21:15:21Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader for MPC5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/677240#M1406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;bootloader example project "BootLoader_MPC5748G" is the template project that demonstrate how to use RAppID Bootloader with MPC5748G DevKit and S32DS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more details about the bootlader and it's features I'd recommend you to see the document below:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/files-static/training_pdf/FTF/2014/americas/WBNR_FTF2014-AUT-F0014-B_PDF.pdf" title="http://www.nxp.com/files-static/training_pdf/FTF/2014/americas/WBNR_FTF2014-AUT-F0014-B_PDF.pdf"&gt;http://www.nxp.com/files-static/training_pdf/FTF/2014/americas/WBNR_FTF2014-AUT-F0014-B_PDF.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First you need to program /rbf file which is actually the bootloader binary. This could be done by OpenSDA (see the screenshot below) or any other Debug cable you have (PEmicro Multilink, Universal, FX..)&lt;/P&gt;&lt;P&gt;There is pre-configured debug configuration that loads the bootloader binary:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27399i2370FA05E175320D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_18.png" alt="pastedImage_18.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27186i903C8D7102B38869/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then you can build the Application which basically blinks LEDs on the board. The generated project + its SREC is located here:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27263i244399114145612F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now download install and run RAppID Bootlader utility:&lt;/P&gt;&lt;P&gt;(&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&amp;amp;appType=license&amp;amp;Parent_nodeId=1158334484323728285086&amp;amp;Parent_pageType=product&amp;amp;Parent_nodeId=1158334484323728285086&amp;amp;Parent_pageType=product" title="https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&amp;amp;appType=license&amp;amp;Parent_nodeId=1158334484323728285086&amp;amp;Parent_pageType=product&amp;amp;Parent_nodeId=1158334484323728285086&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&amp;amp;appType=license&amp;amp;Parent_nodeId=11583344843237282850…&lt;/A&gt;&amp;nbsp;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27444iC6B1DE5885779BE3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_19.png" alt="pastedImage_19.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you should be now able download the generated application project (s-record) via Virtual COM over USB cable (COM15 on my machine) into the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 16:04:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/677240#M1406</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2017-07-24T16:04:54Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader for MPC5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/677241#M1407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Tiju,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see Stan has provideed all information to get boot loader in action.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Udit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jul 2017 05:16:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/677241#M1407</guid>
      <dc:creator>uditsalunke</dc:creator>
      <dc:date>2017-07-25T05:16:12Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader for MPC5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/677242#M1408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62552iBECD9B06F0069A07/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;correct trace as above show;&lt;/P&gt;&lt;P&gt;but I print trace cyclly report as fellow:&lt;/P&gt;&lt;P&gt;Tx: 01 00 00 00 00 AA AA AA AA&lt;/P&gt;&lt;P&gt;Rx: FE 00 00 FE 00 00 00 00 00 &amp;nbsp;init&amp;nbsp;&lt;/P&gt;&lt;P&gt;no other Erasing APP....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2018 13:56:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/677242#M1408</guid>
      <dc:creator>chengxueyuan021</dc:creator>
      <dc:date>2018-06-27T13:56:00Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader for MPC5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/1278615#M7519</link>
      <description>&lt;P&gt;Hi Tiju,&lt;/P&gt;&lt;P&gt;Can you please share the serial bootloader code zip for the MPC5748G as I am unable to find it in the S32DS or MCU expresso IDE. Maybe they have removed it from SDK example codes.&lt;/P&gt;&lt;P&gt;It would be great if you share the zip at sood04sonny@gmail.com&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 04:53:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/1278615#M7519</guid>
      <dc:creator>maharajshreekum</dc:creator>
      <dc:date>2021-05-19T04:53:34Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader for MPC5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/1359691#M7896</link>
      <description>&lt;P&gt;Hi!&amp;nbsp; I am trying to follow Stanish's instruction to try the BootLoader_MPC5748G example on my DEVKit-MPC5748G board.&amp;nbsp; But I got the following error when trying to flash the BootLoader_MPC5748G.RBF to the board.&amp;nbsp; Could someone please help me?&amp;nbsp; Thanks!&lt;/P&gt;&lt;P&gt;Connection from "127.0.0.1" via 127.0.0.1. Connection from port "55762" to 7224&lt;BR /&gt;Copyright 2018 P&amp;amp;E Microcomputer Systems,Inc.&lt;BR /&gt;Command Line :C:\nxp\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\win32\pegdbserver_power_console -device=MPC5748G -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=OPENSDA -speed=5000 -port=USB1Ø&lt;BR /&gt;OpenSDA detected - Flash Version 1.10&lt;BR /&gt;Flash Data in range 0x00F8C000-0x00F8C01B.&lt;BR /&gt;Flash Data in range 0x00F8C020-0x00F8DC0B.&lt;BR /&gt;&lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000082&lt;BR /&gt;Device ID revision is $00000000&lt;BR /&gt;Initializing Ram Block 0x40000000-0x40007FFF.&lt;BR /&gt;MPC574xC Device detected.&lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;CMD&amp;gt;CM C:\nxp\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\win32\gdi\P&amp;amp;E\nxp_mpc5748g_1x32x1520k_cflash.pcp&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000082&lt;BR /&gt;Device ID revision is $00000000&lt;BR /&gt;Initializing Ram Block 0x40000000-0x40007FFF.&lt;BR /&gt;MPC574xC Device detected.&lt;BR /&gt;&lt;BR /&gt;DOUBLE BUFFERING enabled.&lt;BR /&gt;Initialized.&lt;BR /&gt;&lt;BR /&gt;;version 1.05, 06/26/2017, Copyright P&amp;amp;E Microcomputer Systems, &lt;A href="http://www.pemicro.com" target="_blank"&gt;www.pemicro.com&lt;/A&gt; [5748G_6080k]&lt;BR /&gt;&lt;BR /&gt;;device NXP, MPC5748G, 1x32x1520k, desc=CFlash&lt;BR /&gt;&lt;BR /&gt;;begin_cs device=$00F90000, length=$005F0000, ram=$40000000&lt;BR /&gt;&lt;BR /&gt;Loading programming algorithm ...&lt;BR /&gt;Done.&lt;BR /&gt;Programming sequency is : erase, blank check, program, and verify {default}&lt;BR /&gt;CMD&amp;gt;VC&lt;BR /&gt;Verifying object file CRC-16 to device ranges ...&lt;BR /&gt;Error - no valid data in range of module.&lt;BR /&gt;Current content of flash does not match application to be programmed&lt;BR /&gt;CMD&amp;gt;EM&lt;BR /&gt;&lt;BR /&gt;Erasing.&lt;BR /&gt;Module has been erased.&lt;BR /&gt;CMD&amp;gt;PM&lt;BR /&gt;&lt;BR /&gt;Programming.&lt;BR /&gt;Processing Object File Data ...&lt;BR /&gt;&lt;BR /&gt;No data to program.&lt;BR /&gt;&lt;BR /&gt;.&lt;BR /&gt;Error during programming.&lt;BR /&gt;Error Programming flash of device&lt;BR /&gt;Error occured during Flash programming.&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000082&lt;BR /&gt;Device ID revision is $00000000&lt;BR /&gt;&lt;BR /&gt;Device IDCODE is $00000082&lt;BR /&gt;Device ID revision is $00000000&lt;BR /&gt;&lt;BR /&gt;Starting reset script (C:\nxp\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\win32\gdi\P&amp;amp;E\s32e200_mpc574xg.mac) ...&lt;BR /&gt;REM This script is compatible with MPC574xG devices.&lt;BR /&gt;REM Clean GPRs to remove residual data after using algorithm&lt;BR /&gt;REM Initialize all of the Main SRAM - 768KB&lt;BR /&gt;Initializing RAM from $40000000 to $400BFFFF.&lt;BR /&gt;Initializing Ram Block 0x40000000-0x400BFFFF.&lt;BR /&gt;&lt;BR /&gt;Reset script (C:\nxp\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\win32\gdi\P&amp;amp;E\s32e200_mpc574xg.mac) completed.&lt;BR /&gt;&lt;BR /&gt;MPC574xG Device detected.&lt;/P&gt;&lt;P&gt;PEmicro GDB Launch Failure : Error during flash programming. Terminating debug session.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Oct 2021 20:16:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Bootloader-for-MPC5748G/m-p/1359691#M7896</guid>
      <dc:creator>jzhang</dc:creator>
      <dc:date>2021-10-21T20:16:19Z</dc:date>
    </item>
  </channel>
</rss>