<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32144K FTM Timer 0 in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32144K-FTM-Timer-0/m-p/1355704#M7865</link>
    <description>&lt;P&gt;We have tried&lt;/P&gt;&lt;P&gt;FTM1 Channel 0 - PTB2 , Channel 1 - PTA1&amp;nbsp;&lt;/P&gt;&lt;P&gt;FTM3 Channel 0 - PTA2&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And the peak is occurring right after the reset .&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 14 Oct 2021 08:46:45 GMT</pubDate>
    <dc:creator>amansinghaljpr</dc:creator>
    <dc:date>2021-10-14T08:46:45Z</dc:date>
    <item>
      <title>S32144K FTM Timer 0</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32144K-FTM-Timer-0/m-p/1355628#M7863</link>
      <description>&lt;P&gt;So we are trying to generate PWM on PC1 using FTM1 but the problem is ,&amp;nbsp; in the initial stage , the moment the code starts after resets we are getting a random pulse every single time . It almost feels like during the boot there is a very small pulse which is either coming out of the GPIO or out of the FTM which is triggering the GPIO . we have tried changing the different GPIO(channels) as well but same spike is coming.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is affecting our PWM behavior , any recommendations on how to avoid this ?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please refer to the pulse on Channel 2 in the attached image .&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Oct 2021 07:12:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32144K-FTM-Timer-0/m-p/1355628#M7863</guid>
      <dc:creator>amansinghaljpr</dc:creator>
      <dc:date>2021-10-14T07:12:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32144K FTM Timer 0</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32144K-FTM-Timer-0/m-p/1355648#M7864</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;which particular pin are you using? In your app - are you first configuring FTM or GPIO? The peak occurs right after reset or during init (clock/ftm/gpio) phase?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Oct 2021 07:41:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32144K-FTM-Timer-0/m-p/1355648#M7864</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2021-10-14T07:41:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32144K FTM Timer 0</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32144K-FTM-Timer-0/m-p/1355704#M7865</link>
      <description>&lt;P&gt;We have tried&lt;/P&gt;&lt;P&gt;FTM1 Channel 0 - PTB2 , Channel 1 - PTA1&amp;nbsp;&lt;/P&gt;&lt;P&gt;FTM3 Channel 0 - PTA2&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And the peak is occurring right after the reset .&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Oct 2021 08:46:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32144K-FTM-Timer-0/m-p/1355704#M7865</guid>
      <dc:creator>amansinghaljpr</dc:creator>
      <dc:date>2021-10-14T08:46:45Z</dc:date>
    </item>
  </channel>
</rss>