<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックIs building Fortran code available for MPC5748G?</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Is-building-Fortran-code-available-for-MPC5748G/m-p/1351485#M7839</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm investigating whether it is possible to build and run a Fortran&amp;nbsp;project code&amp;nbsp; (BLAS/LAPACK, a famous matrix library) on&amp;nbsp;MPC5748G; though MPC5748G officially supports either C or C++, I thought it is possible as S32DS, an IDE for the microcontroller, contains a Fortran compiler named `powerpc-eabivle-gfortran` but it has failed so far. I am just wondering if:&lt;/P&gt;&lt;P&gt;- I can build a Fortran code on S32S for MPC5748G&lt;/P&gt;&lt;P&gt;- If yes, I can run the resulting executable file on&amp;nbsp;MPC5748G&lt;/P&gt;&lt;P&gt;I'm looking forward to answers or opinions from any pundits who are working on it and/or have relevant experience.&lt;/P&gt;</description>
    <pubDate>Wed, 06 Oct 2021 21:03:24 GMT</pubDate>
    <dc:creator>jlee4</dc:creator>
    <dc:date>2021-10-06T21:03:24Z</dc:date>
    <item>
      <title>Is building Fortran code available for MPC5748G?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Is-building-Fortran-code-available-for-MPC5748G/m-p/1351485#M7839</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm investigating whether it is possible to build and run a Fortran&amp;nbsp;project code&amp;nbsp; (BLAS/LAPACK, a famous matrix library) on&amp;nbsp;MPC5748G; though MPC5748G officially supports either C or C++, I thought it is possible as S32DS, an IDE for the microcontroller, contains a Fortran compiler named `powerpc-eabivle-gfortran` but it has failed so far. I am just wondering if:&lt;/P&gt;&lt;P&gt;- I can build a Fortran code on S32S for MPC5748G&lt;/P&gt;&lt;P&gt;- If yes, I can run the resulting executable file on&amp;nbsp;MPC5748G&lt;/P&gt;&lt;P&gt;I'm looking forward to answers or opinions from any pundits who are working on it and/or have relevant experience.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Oct 2021 21:03:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Is-building-Fortran-code-available-for-MPC5748G/m-p/1351485#M7839</guid>
      <dc:creator>jlee4</dc:creator>
      <dc:date>2021-10-06T21:03:24Z</dc:date>
    </item>
    <item>
      <title>Re: Is building Fortran code available for MPC5748G?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Is-building-Fortran-code-available-for-MPC5748G/m-p/1352607#M7846</link>
      <description>&lt;P&gt;Already answered here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/Can-I-build-Fortran-code-for-MPC5748G-on-S32DS/m-p/1351486#M7841" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio/Can-I-build-Fortran-code-for-MPC5748G-on-S32DS/m-p/1351486#M7841&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Oct 2021 10:22:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Is-building-Fortran-code-available-for-MPC5748G/m-p/1352607#M7846</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-10-08T10:22:16Z</dc:date>
    </item>
  </channel>
</rss>