<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Is there a script available which flashes one or multiple .elf files in the MPC5748G without usi</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Is-there-a-script-available-which-flashes-one-or-multiple-elf/m-p/1332695#M7773</link>
    <description>&lt;P&gt;Use the following to flash multiple .elf files without erasing flash between each load:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;target remote localhost:7224&lt;/P&gt;&lt;P&gt;monitor startmultiload&lt;/P&gt;&lt;P&gt;load file1.elf&lt;/P&gt;&lt;P&gt;load file2.elf&lt;/P&gt;&lt;P&gt;load file3.elf&lt;/P&gt;&lt;P&gt;monitor endmultiload&lt;/P&gt;</description>
    <pubDate>Tue, 31 Aug 2021 20:40:04 GMT</pubDate>
    <dc:creator>jmart23</dc:creator>
    <dc:date>2021-08-31T20:40:04Z</dc:date>
    <item>
      <title>Is there a script available which flashes one or multiple .elf files in the MPC5748G without using the S32 design studio IDE?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Is-there-a-script-available-which-flashes-one-or-multiple-elf/m-p/960397#M5347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been using the S32 design studio IDE for implementing/debugging/flashing the MPC5748G&amp;nbsp;and I'm wondering if there is a script available which flashes&amp;nbsp;one or multiple .elf files in the MPC5748G &lt;STRONG&gt;without&lt;/STRONG&gt; using the S32 design studio IDE?&lt;/P&gt;&lt;P&gt;This can be useful for engineers who only want to flash the device, without having to install / open the S32 design studio IDE.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jul 2019 07:40:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Is-there-a-script-available-which-flashes-one-or-multiple-elf/m-p/960397#M5347</guid>
      <dc:creator>f_merkus</dc:creator>
      <dc:date>2019-07-24T07:40:41Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a script available which flashes one or multiple .elf files in the MPC5748G without using the S32 design studio IDE?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Is-there-a-script-available-which-flashes-one-or-multiple-elf/m-p/960398#M5348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use command line tools ( part of S32DS Installation). More details you can find in these threads:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/482680"&gt;s32k144 command line flash&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/1123376"&gt;https://community.nxp.com/message/1123376&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jul 2019 14:07:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Is-there-a-script-available-which-flashes-one-or-multiple-elf/m-p/960398#M5348</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-07-24T14:07:02Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a script available which flashes one or multiple .elf files in the MPC5748G without using the S32 design studio IDE?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Is-there-a-script-available-which-flashes-one-or-multiple-elf/m-p/960399#M5349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the information. I now can flash using these threads.&lt;/P&gt;&lt;P&gt;I still have one question. I'm flashing three .elf files for multiple cores of the MPC5748G and notice that the program sequence of each elf file consist of erase, black check, program and verify.&lt;/P&gt;&lt;P&gt;How do I know that the next programming action is not erasing the previous programmed elf file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jul 2019 13:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Is-there-a-script-available-which-flashes-one-or-multiple-elf/m-p/960399#M5349</guid>
      <dc:creator>f_merkus</dc:creator>
      <dc:date>2019-07-26T13:26:02Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a script available which flashes one or multiple .elf files in the MPC5748G without usi</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Is-there-a-script-available-which-flashes-one-or-multiple-elf/m-p/1332695#M7773</link>
      <description>&lt;P&gt;Use the following to flash multiple .elf files without erasing flash between each load:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;target remote localhost:7224&lt;/P&gt;&lt;P&gt;monitor startmultiload&lt;/P&gt;&lt;P&gt;load file1.elf&lt;/P&gt;&lt;P&gt;load file2.elf&lt;/P&gt;&lt;P&gt;load file3.elf&lt;/P&gt;&lt;P&gt;monitor endmultiload&lt;/P&gt;</description>
      <pubDate>Tue, 31 Aug 2021 20:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Is-there-a-script-available-which-flashes-one-or-multiple-elf/m-p/1332695#M7773</guid>
      <dc:creator>jmart23</dc:creator>
      <dc:date>2021-08-31T20:40:04Z</dc:date>
    </item>
  </channel>
</rss>