<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32 Design Studio won't talk to S32K3X4EVB-Q257 evaluation boards in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-won-t-talk-to-S32K3X4EVB-Q257-evaluation/m-p/1331804#M7765</link>
    <description>&lt;P&gt;We resolved this ourselves, it turns out S32 Design Studio has to run as Admin on Windows 10, still don't know why, thinking maybe it can't open ports/protocols or USB. &amp;nbsp;Somewhat disappointing, Lauterbach Trace32 talks to the board just fine as Power User, may end up using that.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 30 Aug 2021 13:12:43 GMT</pubDate>
    <dc:creator>chad_privafy</dc:creator>
    <dc:date>2021-08-30T13:12:43Z</dc:date>
    <item>
      <title>S32 Design Studio won't talk to S32K3X4EVB-Q257 evaluation boards</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-won-t-talk-to-S32K3X4EVB-Q257-evaluation/m-p/1329618#M7760</link>
      <description>&lt;P&gt;S32 Design Studio won't talk to&amp;nbsp;S32K3X4EVB-Q257 evaluation boards, trying Windows and Linux, getting stuck at 52% on Windows,&lt;/P&gt;&lt;P&gt;Both on the latest S32 Design Studio version, 3.4.1 (update 1)&lt;/P&gt;&lt;P&gt;Linux succeeds with&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="im"&gt;&amp;nbsp; Finished building: test.siz&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;11:15:32 Build Finished. 0 errors, 0 warnings. (took 1s.67ms)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Windows fails with:&lt;/P&gt;&lt;P&gt;&amp;nbsp; Finished building: test.siz&lt;/P&gt;&lt;P&gt;&amp;nbsp; "make -j12 all" terminated with exit code -1. Build might be incomplete.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;09:06:37 Build Finished. 0 errors, 0 warnings. (took 7s.830ms)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; Launching test_Debug_Flash_PNE&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; (green bar stuck at 52%)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; Launching: Invoking command make -j12 all&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Trying lots of things, currently looking for Windows firewall logs to see if it's blocked.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Cannot find test.siz file on either windows or linux, is that supposed to be written out to the board?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Both .elf files say the same output sizes,&amp;nbsp;&amp;nbsp;2652&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; 1180&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 40&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; 3872&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; f20&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; test.elf&lt;/P&gt;&lt;P&gt;both using the same main.c&amp;nbsp;but a hex diff shows some differences in the .elf output and we're not seeing a JTAG Device ID on Windows.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Full Windows console output:&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;09:06:29 **** Build of configuration Debug_FLASH for project test ****&lt;/P&gt;&lt;P&gt;make -j12 all&lt;/P&gt;&lt;P&gt;Building file: ../src/main.c&lt;/P&gt;&lt;P&gt;Building file: ../Project_Settings/Startup_Code/boot_header.c&lt;/P&gt;&lt;P&gt;Building file: ../Project_Settings/Startup_Code/startup_ARMCM7.c&lt;/P&gt;&lt;P&gt;Building file: ../Project_Settings/Startup_Code/system_ARMCM7.c&lt;/P&gt;&lt;P&gt;Invoking: Standard S32DS C Compiler&lt;/P&gt;&lt;P&gt;arm-none-eabi-gcc "@src/main.args" -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.c"&lt;/P&gt;&lt;P&gt;Invoking: Standard S32DS C Compiler&lt;/P&gt;&lt;P&gt;arm-none-eabi-gcc "@Project_Settings/Startup_Code/boot_header.args" -MMD -MP -MF"Project_Settings/Startup_Code/boot_header.d" -MT"Project_Settings/Startup_Code/boot_header.o" -o "Project_Settings/Startup_Code/boot_header.o" "../Project_Settings/Startup_Code/boot_header.c"&lt;/P&gt;&lt;P&gt;Invoking: Standard S32DS C Compiler&lt;/P&gt;&lt;P&gt;arm-none-eabi-gcc "@Project_Settings/Startup_Code/boot_header.args" -MMD -MP -MF"Project_Settings/Startup_Code/system_ARMCM7.d" -MT"Project_Settings/Startup_Code/system_ARMCM7.o" -o "Project_Settings/Startup_Code/system_ARMCM7.o" "../Project_Settings/Startup_Code/system_ARMCM7.c"&lt;/P&gt;&lt;P&gt;Invoking: Standard S32DS C Compiler&lt;/P&gt;&lt;P&gt;arm-none-eabi-gcc "@Project_Settings/Startup_Code/boot_header.args" -MMD -MP -MF"Project_Settings/Startup_Code/startup_ARMCM7.d" -MT"Project_Settings/Startup_Code/startup_ARMCM7.o" -o "Project_Settings/Startup_Code/startup_ARMCM7.o" "../Project_Settings/Startup_Code/startup_ARMCM7.c"&lt;/P&gt;&lt;P&gt;Finished building: ../Project_Settings/Startup_Code/boot_header.c&lt;/P&gt;&lt;P&gt;Finished building: ../Project_Settings/Startup_Code/system_ARMCM7.c&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Finished building: ../src/main.c&lt;/P&gt;&lt;P&gt;Finished building: ../Project_Settings/Startup_Code/startup_ARMCM7.c&lt;/P&gt;&lt;P&gt;Building target: test.elf&lt;/P&gt;&lt;P&gt;Invoking: Standard S32DS C Linker&lt;/P&gt;&lt;P&gt;arm-none-eabi-gcc -o "test.elf" "@test.args"&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Finished building target: test.elf&lt;/P&gt;&lt;P&gt;Invoking: Standard S32DS Print Size&lt;/P&gt;&lt;P&gt;arm-none-eabi-size --format=berkeley test.elf&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; text&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; data&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; bss&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; dec&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; hex&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; filename&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 2652&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; 1180&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 40&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; 3872&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; f20&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; test.elf&lt;/P&gt;&lt;P&gt;Finished building: test.siz&lt;/P&gt;&lt;P&gt;"make -j12 all" terminated with exit code -1. Build might be incomplete.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;09:06:37 Build Finished. 0 errors, 0 warnings. (took 7s.830ms)&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 17:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-won-t-talk-to-S32K3X4EVB-Q257-evaluation/m-p/1329618#M7760</guid>
      <dc:creator>chad_privafy</dc:creator>
      <dc:date>2021-08-25T17:09:42Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design Studio won't talk to S32K3X4EVB-Q257 evaluation boards</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-won-t-talk-to-S32K3X4EVB-Q257-evaluation/m-p/1331804#M7765</link>
      <description>&lt;P&gt;We resolved this ourselves, it turns out S32 Design Studio has to run as Admin on Windows 10, still don't know why, thinking maybe it can't open ports/protocols or USB. &amp;nbsp;Somewhat disappointing, Lauterbach Trace32 talks to the board just fine as Power User, may end up using that.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Aug 2021 13:12:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-won-t-talk-to-S32K3X4EVB-Q257-evaluation/m-p/1331804#M7765</guid>
      <dc:creator>chad_privafy</dc:creator>
      <dc:date>2021-08-30T13:12:43Z</dc:date>
    </item>
  </channel>
</rss>