<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックS32DS AND CODEWORRIER Assembler programming. Please help URGENT</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-AND-CODEWORRIER-Assembler-programming-Please-help-URGENT/m-p/1317566#M7698</link>
    <description>&lt;P&gt;Hi guys, serious problem here. I'm an assembler programmer and I've designed a standalone board with the PDX20 which is also a MPC5645S. I've checked ALL voltages and GND and all is correct, my board is working fine with downloading code using codeworrier via the JTAG interface.&lt;/P&gt;&lt;P&gt;I've created a C project and called my assembler program via a extern function in C. Now this works fine. I've done this is S32DS and Codeworrier.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Using Codeworrier -&amp;gt; When typing in assembler instructions codeworrier hardly recognises any of the assembler instructions. It does accept a few like add r3,r4,r5 but won't accept addi r3,r4,50. It won't accept &amp;nbsp;stw r5,0(r3) so I can't even store data anywhere, and load instructions don't work either. I can say that codeworrier does download my code to my standalone via the JTAG interface so I know that my standalone board is fine. Can someone help with codeworrier recognising the PowerPC assembler instructions.&lt;/P&gt;&lt;P&gt;Using S32DS -&amp;gt; S32DS accepts ALL the PowerPC assembler instructions so I'm happy about that but here's the problem. When I build the program is all good but when I choose debug it won't down load the code to my standalone board yet codeworrier does download the code. The error I'm getting in SD32 is "Launching PDX20_TEST.elf" has encountered a problem. Error with command: gdb -- version.&lt;/P&gt;&lt;P&gt;I have NO idea what that means, can someone help me on that. I'd rather use SD32 than codeworrier.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks guys and hope to hear from you soon.&lt;/P&gt;&lt;P&gt;Pete&lt;/P&gt;</description>
    <pubDate>Tue, 03 Aug 2021 21:45:30 GMT</pubDate>
    <dc:creator>peteradamcik</dc:creator>
    <dc:date>2021-08-03T21:45:30Z</dc:date>
    <item>
      <title>S32DS AND CODEWORRIER Assembler programming. Please help URGENT</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-AND-CODEWORRIER-Assembler-programming-Please-help-URGENT/m-p/1317566#M7698</link>
      <description>&lt;P&gt;Hi guys, serious problem here. I'm an assembler programmer and I've designed a standalone board with the PDX20 which is also a MPC5645S. I've checked ALL voltages and GND and all is correct, my board is working fine with downloading code using codeworrier via the JTAG interface.&lt;/P&gt;&lt;P&gt;I've created a C project and called my assembler program via a extern function in C. Now this works fine. I've done this is S32DS and Codeworrier.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Using Codeworrier -&amp;gt; When typing in assembler instructions codeworrier hardly recognises any of the assembler instructions. It does accept a few like add r3,r4,r5 but won't accept addi r3,r4,50. It won't accept &amp;nbsp;stw r5,0(r3) so I can't even store data anywhere, and load instructions don't work either. I can say that codeworrier does download my code to my standalone via the JTAG interface so I know that my standalone board is fine. Can someone help with codeworrier recognising the PowerPC assembler instructions.&lt;/P&gt;&lt;P&gt;Using S32DS -&amp;gt; S32DS accepts ALL the PowerPC assembler instructions so I'm happy about that but here's the problem. When I build the program is all good but when I choose debug it won't down load the code to my standalone board yet codeworrier does download the code. The error I'm getting in SD32 is "Launching PDX20_TEST.elf" has encountered a problem. Error with command: gdb -- version.&lt;/P&gt;&lt;P&gt;I have NO idea what that means, can someone help me on that. I'd rather use SD32 than codeworrier.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks guys and hope to hear from you soon.&lt;/P&gt;&lt;P&gt;Pete&lt;/P&gt;</description>
      <pubDate>Tue, 03 Aug 2021 21:45:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-AND-CODEWORRIER-Assembler-programming-Please-help-URGENT/m-p/1317566#M7698</guid>
      <dc:creator>peteradamcik</dc:creator>
      <dc:date>2021-08-03T21:45:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS AND CODEWORRIER Assembler programming. Please help URGENT</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-AND-CODEWORRIER-Assembler-programming-Please-help-URGENT/m-p/1318226#M7702</link>
      <description>&lt;P&gt;Hi Pete,&lt;/P&gt;
&lt;P&gt;Regarding s32 Design Studio - please check this thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/Cannot-run-program-quot-gdb-quot-Launching-failed/m-p/802139#M3403" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio/Cannot-run-program-quot-gdb-quot-Launching-failed/m-p/802139#M3403&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regarding CodeWarrior - Seems you are using 32bit BOOKE instruction set instead of VLE. One reason why CodeWarrior may not recognize the instructions is that it is switched to accept VLE instructions only.&lt;/P&gt;
&lt;P&gt;Please check if the option below is enabled for your CodeWarrior project:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="stanish_1-1628087441145.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/151803i1C3E6D547F3C7EF0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="stanish_1-1628087441145.png" alt="stanish_1-1628087441145.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it helps,&lt;/P&gt;
&lt;P&gt;Stan&lt;/P&gt;</description>
      <pubDate>Wed, 04 Aug 2021 14:35:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-AND-CODEWORRIER-Assembler-programming-Please-help-URGENT/m-p/1318226#M7702</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2021-08-04T14:35:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS AND CODEWORRIER Assembler programming. Please help URGENT</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-AND-CODEWORRIER-Assembler-programming-Please-help-URGENT/m-p/1318554#M7704</link>
      <description>&lt;P&gt;Hi Stan, thank you for the info. I could not find the Tool Settings in Codeworrier, You must have a different version than I. Anyway I found when you create a new project it gives you the option to use VLE in a checkbox and its ON at default, so I created a new project and unchecked the VLE box and now its accepting all the PPC assembler instruction. A BIG THANK YOU for that. Codeworrier is not a FULL FREE IDE so I would rather use SD32. Codeworrier only allows 64k of code which is useless with our project. Our microcontroller has 2MB of flash and we will need almost ALL of that.&lt;/P&gt;&lt;P&gt;I'll check out the thread that you said for S32DS.&lt;/P&gt;&lt;P&gt;Thank you so much for your help, I totally appreciate the support NXP Community does for its developers.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Aug 2021 00:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-AND-CODEWORRIER-Assembler-programming-Please-help-URGENT/m-p/1318554#M7704</guid>
      <dc:creator>peteradamcik</dc:creator>
      <dc:date>2021-08-05T00:22:02Z</dc:date>
    </item>
  </channel>
</rss>