<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックS32DS3.4 + debug probe not able to restart/relaunch a process</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS3-4-debug-probe-not-able-to-restart-relaunch-a-process/m-p/1310489#M7655</link>
    <description>&lt;P&gt;Using S32G2 CM7 cores with debug probe and latest DS3.4.&lt;/P&gt;
&lt;P&gt;When I'm debugging, I would like to restart the running process without terminating and relaunch the debugger (which will force code to be re-downloaded, etc).&lt;/P&gt;
&lt;P&gt;Using the DS IDE, there is a 'restart' button on the debugger, as well as 'relaunch' menu entry.&amp;nbsp; It allows either of these to be selected, but they break the debug session and do not have the intended affect.&amp;nbsp; I can also hang DS sometimes using these, requiring a full restart.&lt;/P&gt;
&lt;P&gt;Is this behavior intended to be supported with S32G2 Cortex-M using S32 debug probe?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Justin&lt;/P&gt;</description>
    <pubDate>Tue, 20 Jul 2021 13:59:41 GMT</pubDate>
    <dc:creator>justinlydick</dc:creator>
    <dc:date>2021-07-20T13:59:41Z</dc:date>
    <item>
      <title>S32DS3.4 + debug probe not able to restart/relaunch a process</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS3-4-debug-probe-not-able-to-restart-relaunch-a-process/m-p/1310489#M7655</link>
      <description>&lt;P&gt;Using S32G2 CM7 cores with debug probe and latest DS3.4.&lt;/P&gt;
&lt;P&gt;When I'm debugging, I would like to restart the running process without terminating and relaunch the debugger (which will force code to be re-downloaded, etc).&lt;/P&gt;
&lt;P&gt;Using the DS IDE, there is a 'restart' button on the debugger, as well as 'relaunch' menu entry.&amp;nbsp; It allows either of these to be selected, but they break the debug session and do not have the intended affect.&amp;nbsp; I can also hang DS sometimes using these, requiring a full restart.&lt;/P&gt;
&lt;P&gt;Is this behavior intended to be supported with S32G2 Cortex-M using S32 debug probe?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Justin&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jul 2021 13:59:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS3-4-debug-probe-not-able-to-restart-relaunch-a-process/m-p/1310489#M7655</guid>
      <dc:creator>justinlydick</dc:creator>
      <dc:date>2021-07-20T13:59:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS3.4 + debug probe not able to restart/relaunch a process</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS3-4-debug-probe-not-able-to-restart-relaunch-a-process/m-p/1311490#M7665</link>
      <description>&lt;P&gt;Hey Justin,&lt;/P&gt;
&lt;P&gt;We're going to create a ticket for this. As I understand, it is expected to work.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jul 2021 19:55:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS3-4-debug-probe-not-able-to-restart-relaunch-a-process/m-p/1311490#M7665</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2021-07-21T19:55:20Z</dc:date>
    </item>
  </channel>
</rss>