<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: Build time is very high with S32DS for ARM V2.0</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Build-time-is-very-high-with-S32DS-for-ARM-V2-0/m-p/1290440#M7561</link>
    <description>&lt;P&gt;Hello Ben,&lt;/P&gt;
&lt;P&gt;Can you see any TCP reconnection packet in captured TCP packet stream?&lt;/P&gt;
&lt;P&gt;Are you using a version control software/plugin such as SVN?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Stan&lt;/P&gt;</description>
    <pubDate>Thu, 10 Jun 2021 05:49:50 GMT</pubDate>
    <dc:creator>stanish</dc:creator>
    <dc:date>2021-06-10T05:49:50Z</dc:date>
    <item>
      <title>Build time is very high with S32DS for ARM V2.0</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Build-time-is-very-high-with-S32DS-for-ARM-V2-0/m-p/721069#M2072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="background: white;"&gt;Dear All,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-left: .5in;"&gt;&lt;BR /&gt; &lt;SPAN style="background: white;"&gt;I have installed S32DS for ARM 2.0. It was working fine. I don’t know what happened suddenly it’s not building then I reinstalled somehow its building the source code but it’s taking so much time…..&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-left: .5in;"&gt;&lt;SPAN style="background: white;"&gt;Then I referred this link &lt;A _jive_internal="true" href="https://community.nxp.com/thread/460814"&gt;&lt;SPAN style="color: windowtext;"&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;A href="https://community.nxp.com/thread/460814" target="test_blank"&gt;https://community.nxp.com/thread/460814&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-left: .5in;"&gt;&lt;SPAN style="background: white;"&gt;I tried to build without network connection, its fast.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-left: .5in;"&gt;&lt;SPAN style="background: white;"&gt;I’m sure that S32DS ARM v2.00 build time has some dependency with network&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-left: .5in;"&gt;&lt;SPAN style="background: white;"&gt;Then I have installed update 1 and update 2 for S32DS ARM v2.00. No improvement.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-left: .5in;"&gt;&lt;SPAN style="background: white;"&gt;Please give me some helpful suggestion.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white;"&gt;Looking forward to hear from you&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white;"&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white;"&gt;Yusup Khan&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Nov 2017 08:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Build-time-is-very-high-with-S32DS-for-ARM-V2-0/m-p/721069#M2072</guid>
      <dc:creator>yusupkhany</dc:creator>
      <dc:date>2017-11-18T08:40:23Z</dc:date>
    </item>
    <item>
      <title>Re: Build time is very high with S32DS for ARM V2.0</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Build-time-is-very-high-with-S32DS-for-ARM-V2-0/m-p/721070#M2073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the report.&lt;/P&gt;&lt;P&gt;Could you possibly provide us with more details since we are not able to reproduce it on our side.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;does the build slow down occurs every time when you click the build or it is sort of random (e.g. one a 10 attempts)?&lt;/LI&gt;&lt;LI&gt;is the same problem with previous version of S32DS ARM v1.3 (&lt;A href="https://community.nxp.com/docs/DOC-333485"&gt;S32 Design Studio for ARM v1.3 (Windows/Linux) released!&lt;/A&gt;&amp;nbsp;)?&lt;/LI&gt;&lt;LI&gt;is it specific to your project or it is reproducible even with empty (non-SDK) project?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;Perhaps you could try to capture network traffic until the build process is finished (e.g. via a network sniffer like&amp;nbsp;&lt;A href="https://www.wireshark.org/"&gt;Wireshark&lt;/A&gt;)?&amp;nbsp; Then you might also try to identify which&amp;nbsp; process owns the TCP connection suspected for the&amp;nbsp;&lt;/P&gt;&lt;P&gt;build delays (e.g. &lt;A href="https://docs.microsoft.com/en-us/sysinternals/downloads/tcpview"&gt;TCPView&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This info will help us to resolve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Nov 2017 09:41:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Build-time-is-very-high-with-S32DS-for-ARM-V2-0/m-p/721070#M2073</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2017-11-24T09:41:02Z</dc:date>
    </item>
    <item>
      <title>Re: Build time is very high with S32DS for ARM V2.0</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Build-time-is-very-high-with-S32DS-for-ARM-V2-0/m-p/1288092#M7548</link>
      <description>&lt;P&gt;Hello there,&lt;/P&gt;&lt;P&gt;I'm new to µC-programming with S32 Design Studio for ARM and faced the same problem like Yusup. I attached two images where the build time is shown and the network connection symbol from Windows.&lt;/P&gt;&lt;P&gt;- The build slows down at every project from "Hello World" to bigger example projects, if I'm connected to the network.&lt;/P&gt;&lt;P&gt;- I didn't try S32DS ARM v1.3&lt;/P&gt;&lt;P&gt;It seems that localhost which is used for debugging has a problem. I can't see anything special in TCPView. Maybe there's already a solution? Or is it a firewal/antivirus problem?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Benjamin&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jun 2021 08:44:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Build-time-is-very-high-with-S32DS-for-ARM-V2-0/m-p/1288092#M7548</guid>
      <dc:creator>Ben_Akleva</dc:creator>
      <dc:date>2021-06-07T08:44:02Z</dc:date>
    </item>
    <item>
      <title>Re: Build time is very high with S32DS for ARM V2.0</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Build-time-is-very-high-with-S32DS-for-ARM-V2-0/m-p/1290440#M7561</link>
      <description>&lt;P&gt;Hello Ben,&lt;/P&gt;
&lt;P&gt;Can you see any TCP reconnection packet in captured TCP packet stream?&lt;/P&gt;
&lt;P&gt;Are you using a version control software/plugin such as SVN?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Stan&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 05:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Build-time-is-very-high-with-S32DS-for-ARM-V2-0/m-p/1290440#M7561</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2021-06-10T05:49:50Z</dc:date>
    </item>
  </channel>
</rss>