<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Write using Flash Tool with eMMC in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1287981#M7546</link>
    <description>&lt;P&gt;&amp;nbsp; I want to download the bianry to device(S32G274A RDB2) with eMMC using flashtool;&lt;/P&gt;&lt;P&gt;When i run below command:&lt;/P&gt;&lt;P&gt;sudo ./bin/S32FlashTool -t ./targets/S32G2xxx.bin -a ./flash/EMMC.bin -i uart -p /dev/ttyUSB0&lt;/P&gt;&lt;P&gt;then there are below errors:&lt;/P&gt;&lt;P&gt;Initializing Target.&lt;/P&gt;&lt;P&gt;Error: Target image load is failed!&lt;/P&gt;&lt;P&gt;Error: Response error&lt;/P&gt;&lt;P&gt;from above error, the targets bin file of s32g2xxx has some wrong?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you help check this issue, thanks&lt;/P&gt;</description>
    <pubDate>Mon, 07 Jun 2021 06:15:10 GMT</pubDate>
    <dc:creator>wufan2</dc:creator>
    <dc:date>2021-06-07T06:15:10Z</dc:date>
    <item>
      <title>Write using Flash Tool with eMMC</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1287981#M7546</link>
      <description>&lt;P&gt;&amp;nbsp; I want to download the bianry to device(S32G274A RDB2) with eMMC using flashtool;&lt;/P&gt;&lt;P&gt;When i run below command:&lt;/P&gt;&lt;P&gt;sudo ./bin/S32FlashTool -t ./targets/S32G2xxx.bin -a ./flash/EMMC.bin -i uart -p /dev/ttyUSB0&lt;/P&gt;&lt;P&gt;then there are below errors:&lt;/P&gt;&lt;P&gt;Initializing Target.&lt;/P&gt;&lt;P&gt;Error: Target image load is failed!&lt;/P&gt;&lt;P&gt;Error: Response error&lt;/P&gt;&lt;P&gt;from above error, the targets bin file of s32g2xxx has some wrong?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you help check this issue, thanks&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jun 2021 06:15:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1287981#M7546</guid>
      <dc:creator>wufan2</dc:creator>
      <dc:date>2021-06-07T06:15:10Z</dc:date>
    </item>
    <item>
      <title>Re: Write using Flash Tool with eMMC</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1287984#M7547</link>
      <description>&lt;P&gt;I have set below setting in my board:&lt;/P&gt;&lt;P&gt;eMMC Boot:&lt;BR /&gt;– SW9 -&amp;gt; ALL-OFF&lt;BR /&gt;– SW10 -&amp;gt; 1-ON, 2-OFF&lt;BR /&gt;– SW3 -&amp;gt; OFF&lt;BR /&gt;– SW4 -&amp;gt; 6-ON, 7-ON, Rest-OFF&lt;BR /&gt;– SW5 -&amp;gt; ALL-OFF&lt;BR /&gt;– SW6 -&amp;gt; ALL-OFF&lt;BR /&gt;– SW7 -&amp;gt; ALL-OFF&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jun 2021 06:19:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1287984#M7547</guid>
      <dc:creator>wufan2</dc:creator>
      <dc:date>2021-06-07T06:19:46Z</dc:date>
    </item>
    <item>
      <title>Re: Write using Flash Tool with eMMC</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1291180#M7572</link>
      <description>&lt;P&gt;You set your board to boot from eMMC, while the processor has to be in the&lt;BR /&gt;Serial boot mode to communicate with the host part of the Flash Tool.&amp;nbsp; &lt;BR /&gt;In addition to the settings specified in Section 3.6 of S32G-VNP-RDB2 User &lt;BR /&gt;Guide, you should set SW3 to OFF to make eMMC visible to the processor/tool.&lt;BR /&gt;Details behind this setting can be found in Section 3.7.3 of S32G-VNP-RDB2&lt;BR /&gt;Reference Manual.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 07:37:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1291180#M7572</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-06-11T07:37:46Z</dc:date>
    </item>
    <item>
      <title>Re: Write using Flash Tool with eMMC</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1494537#M8843</link>
      <description>&lt;P&gt;hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/43353"&gt;@bpe&lt;/a&gt;&amp;nbsp;I am facing a similar issue with SBC S32G274A EVB, I am trying to directly flash the binary image into the SRAM of the device which is SoM (MPX-S32G274A) through the S32 debug probe which I have connected to the JTAG module ST7. I have configured the onboard SW2 and SW3 in the following fashion :&amp;nbsp;&lt;BR /&gt;SW2 : 1,2,3 - OFF &amp;amp; 4-ON&lt;BR /&gt;SW3 : 1,2 - OFF&lt;/P&gt;&lt;P&gt;I prepared the bootable binary image using the following sources :&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Use-IVT-Tool-To-Create-A-Blob-Image-S32G274A/ta-p/1125675" target="_blank"&gt;HOWTO: Use IVT Tool To Create A Blob Image S32G274... - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;S32DS flashing attempt through IVT mode :&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="prabhatpandey_1-1658730304546.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/187642iF0906DFDDCD0C8DF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="prabhatpandey_1-1658730304546.png" alt="prabhatpandey_1-1658730304546.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;prabhatpandey_1-1658730304546.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;S32 flash tool :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="prabhatpandey_0-1658730105375.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/187641i9355DFDA0E0D3715/image-size/medium?v=v2&amp;amp;px=400" role="button" title="prabhatpandey_0-1658730105375.png" alt="prabhatpandey_0-1658730105375.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;prabhatpandey_0-1658730105375.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jul 2022 06:27:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1494537#M8843</guid>
      <dc:creator>prabhat_</dc:creator>
      <dc:date>2022-07-25T06:27:44Z</dc:date>
    </item>
    <item>
      <title>Re: Write using Flash Tool with eMMC</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1579908#M9638</link>
      <description>&lt;P&gt;hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/43353"&gt;@bpe&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/129880"&gt;@wufan2&lt;/a&gt;, any update on this issue ? I am trying to do a flash write using the S32 Flash Tool by keeping the boot option as serial download on the EVAL board. I am still facing the very same issues.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Jan 2023 09:12:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1579908#M9638</guid>
      <dc:creator>prabhat_</dc:creator>
      <dc:date>2023-01-10T09:12:34Z</dc:date>
    </item>
    <item>
      <title>Re: Write using Flash Tool with eMMC</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1597275#M9728</link>
      <description>&lt;P&gt;Even I am facing the same issue. Any updates on this?&lt;/P&gt;</description>
      <pubDate>Fri, 10 Feb 2023 10:53:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Write-using-Flash-Tool-with-eMMC/m-p/1597275#M9728</guid>
      <dc:creator>puravp</dc:creator>
      <dc:date>2023-02-10T10:53:37Z</dc:date>
    </item>
  </channel>
</rss>