<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic [S32DS 3.4] S32FlashTool for S32G in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-3-4-S32FlashTool-for-S32G/m-p/1260038#M7403</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;A Debug tool vendor who is working for S32G is asking question about S32FlashTools.&lt;BR /&gt;They would like to perform Read/Write/Erase Flash by loading S32G2xxx.bin and MX25UW51245G.bin on SRAM via JTAG debugger. Is it possible? If yes, following questions are popped up.&lt;BR /&gt;Q1: Which address should they be stored in? &lt;BR /&gt;Q2: Which address is starting address?&lt;BR /&gt;Reading MX25UW51245G.bin, they found the address of FA_Init() and FA_ExecCmd(). Should they call FA_Init()? If so, the What value of argument "apParams" for FA_Init should be configured?&lt;BR /&gt;Q3: After calling FA_Init(), should they call FA_ExecCmd()?&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Masataka Yakashiro&lt;/P&gt;</description>
    <pubDate>Sun, 11 Apr 2021 05:32:32 GMT</pubDate>
    <dc:creator>masatakayakashi</dc:creator>
    <dc:date>2021-04-11T05:32:32Z</dc:date>
    <item>
      <title>[S32DS 3.4] S32FlashTool for S32G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-3-4-S32FlashTool-for-S32G/m-p/1260038#M7403</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;A Debug tool vendor who is working for S32G is asking question about S32FlashTools.&lt;BR /&gt;They would like to perform Read/Write/Erase Flash by loading S32G2xxx.bin and MX25UW51245G.bin on SRAM via JTAG debugger. Is it possible? If yes, following questions are popped up.&lt;BR /&gt;Q1: Which address should they be stored in? &lt;BR /&gt;Q2: Which address is starting address?&lt;BR /&gt;Reading MX25UW51245G.bin, they found the address of FA_Init() and FA_ExecCmd(). Should they call FA_Init()? If so, the What value of argument "apParams" for FA_Init should be configured?&lt;BR /&gt;Q3: After calling FA_Init(), should they call FA_ExecCmd()?&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Masataka Yakashiro&lt;/P&gt;</description>
      <pubDate>Sun, 11 Apr 2021 05:32:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-3-4-S32FlashTool-for-S32G/m-p/1260038#M7403</guid>
      <dc:creator>masatakayakashi</dc:creator>
      <dc:date>2021-04-11T05:32:32Z</dc:date>
    </item>
    <item>
      <title>Re: [S32DS 3.4] S32FlashTool for S32G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-3-4-S32FlashTool-for-S32G/m-p/1262292#M7405</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/153337"&gt;@masatakayakashi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;We have a document regarding the command line use of the Flash Programmer within the S32 Debugger. It uses JTAG connection with S32 Debug Probe.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/INTERNAL-S32-Design-Studio/HOWTO-Command-Line-JTAG-flash-programming-with-S32-Debug-Probe/ta-p/1102702" target="_blank"&gt;https://community.nxp.com/t5/INTERNAL-S32-Design-Studio/HOWTO-Command-Line-JTAG-flash-programming-with-S32-Debug-Probe/ta-p/1102702&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 20:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-3-4-S32FlashTool-for-S32G/m-p/1262292#M7405</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2021-04-14T20:04:47Z</dc:date>
    </item>
    <item>
      <title>Re: [S32DS 3.4] S32FlashTool for S32G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-3-4-S32FlashTool-for-S32G/m-p/1262358#M7406</link>
      <description>&lt;P&gt;Thanks, I will recommend to try S32Debugger.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Masataka&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 01:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-3-4-S32FlashTool-for-S32G/m-p/1262358#M7406</guid>
      <dc:creator>masatakayakashi</dc:creator>
      <dc:date>2021-04-15T01:02:58Z</dc:date>
    </item>
  </channel>
</rss>