<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Cannot compile the built-in example</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Cannot-compile-the-built-in-example/m-p/1248275#M7337</link>
    <description>&lt;P&gt;I am wanting a good example for the Watchdog on the S32K146 so I selected New-&amp;gt;S32DS Project from Example and installed the wdog_interrupt_S32k146 project.&lt;/P&gt;&lt;P&gt;I then tried building the project and I get compile errors on main.c not being able to find include files such as Cpu.h, clockMan1.h, pin_mux.h.&amp;nbsp; When I perform a search of the entire NXP/S32DS_ARM_v2.2 directory those files don't seem to exist anywhere.&amp;nbsp; I have a good install because I have been using the setup for various projects.&lt;/P&gt;&lt;P&gt;I almost don't care if the project actually builds because all I want is to be able to get it to generate the WDOG_DRV_xxx functions, or any other WDOG function, so that I can see how it works to incorporate it into my project.&lt;/P&gt;&lt;P&gt;So, I just want to get past the errors on the includes to be able to build the example and look at the generated code.&lt;/P&gt;&lt;P&gt;I also noticed that the project "include paths" in Tool Settings expects S32_SDK_Path to be defined. I have no way of knowing if it is.&lt;/P&gt;</description>
    <pubDate>Thu, 18 Mar 2021 15:37:18 GMT</pubDate>
    <dc:creator>roger_davis</dc:creator>
    <dc:date>2021-03-18T15:37:18Z</dc:date>
    <item>
      <title>Cannot compile the built-in example</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Cannot-compile-the-built-in-example/m-p/1248275#M7337</link>
      <description>&lt;P&gt;I am wanting a good example for the Watchdog on the S32K146 so I selected New-&amp;gt;S32DS Project from Example and installed the wdog_interrupt_S32k146 project.&lt;/P&gt;&lt;P&gt;I then tried building the project and I get compile errors on main.c not being able to find include files such as Cpu.h, clockMan1.h, pin_mux.h.&amp;nbsp; When I perform a search of the entire NXP/S32DS_ARM_v2.2 directory those files don't seem to exist anywhere.&amp;nbsp; I have a good install because I have been using the setup for various projects.&lt;/P&gt;&lt;P&gt;I almost don't care if the project actually builds because all I want is to be able to get it to generate the WDOG_DRV_xxx functions, or any other WDOG function, so that I can see how it works to incorporate it into my project.&lt;/P&gt;&lt;P&gt;So, I just want to get past the errors on the includes to be able to build the example and look at the generated code.&lt;/P&gt;&lt;P&gt;I also noticed that the project "include paths" in Tool Settings expects S32_SDK_Path to be defined. I have no way of knowing if it is.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Mar 2021 15:37:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Cannot-compile-the-built-in-example/m-p/1248275#M7337</guid>
      <dc:creator>roger_davis</dc:creator>
      <dc:date>2021-03-18T15:37:18Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot compile the built-in example</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Cannot-compile-the-built-in-example/m-p/1248288#M7338</link>
      <description>&lt;P&gt;I figured out the problem. When I selected&amp;nbsp;&lt;SPAN&gt;New-&amp;gt;S32DS Project from Example, I should have selected New-&amp;gt;S32DS Application Project and then followed to dialogs to select the processor family and which example project.&amp;nbsp; From there, everything worked.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Mar 2021 15:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Cannot-compile-the-built-in-example/m-p/1248288#M7338</guid>
      <dc:creator>roger_davis</dc:creator>
      <dc:date>2021-03-18T15:57:27Z</dc:date>
    </item>
  </channel>
</rss>