<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックS32 Design studio - Debugger and linker folder disabled in the project</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-studio-Debugger-and-linker-folder-disabled-in-the/m-p/1246040#M7331</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I installed S32 Design Studio V2.2 yesterday and tried to create a new application project. Project was created but the debugger and linker folder got disabled (please refer the screenshot attached for the reference). I added the source files and include files then added library paths. Build also able to do (no errors) and also able to flash the software to the Hardware board. When I try to keep a breakpoint before executing the program on board, it is not allowing me to keep a breakpoint. I thought due to this folder disabled, I could not keep a breakpoint before executing the program on board.&lt;/P&gt;&lt;P&gt;Kindly suggest me if I am doing anything wrong or anything is missed out during creation of new application project and also in adding library paths.&lt;/P&gt;&lt;P&gt;Thanks in advance for any support to resolve this.&lt;/P&gt;</description>
    <pubDate>Tue, 16 Mar 2021 04:55:56 GMT</pubDate>
    <dc:creator>Parthasarathi_Pandiyan</dc:creator>
    <dc:date>2021-03-16T04:55:56Z</dc:date>
    <item>
      <title>S32 Design studio - Debugger and linker folder disabled in the project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-studio-Debugger-and-linker-folder-disabled-in-the/m-p/1246040#M7331</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I installed S32 Design Studio V2.2 yesterday and tried to create a new application project. Project was created but the debugger and linker folder got disabled (please refer the screenshot attached for the reference). I added the source files and include files then added library paths. Build also able to do (no errors) and also able to flash the software to the Hardware board. When I try to keep a breakpoint before executing the program on board, it is not allowing me to keep a breakpoint. I thought due to this folder disabled, I could not keep a breakpoint before executing the program on board.&lt;/P&gt;&lt;P&gt;Kindly suggest me if I am doing anything wrong or anything is missed out during creation of new application project and also in adding library paths.&lt;/P&gt;&lt;P&gt;Thanks in advance for any support to resolve this.&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 04:55:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-studio-Debugger-and-linker-folder-disabled-in-the/m-p/1246040#M7331</guid>
      <dc:creator>Parthasarathi_Pandiyan</dc:creator>
      <dc:date>2021-03-16T04:55:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design studio - Debugger and linker folder disabled in the project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-studio-Debugger-and-linker-folder-disabled-in-the/m-p/1246231#M7332</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the folders are "disabled" because files inside aren't part of build process. There is no relation with breakpoints. So, can you share more details about your break point issue? If you set break point to some line and start debug session, the BP disappears or what's exactly your issue?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 08:22:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-studio-Debugger-and-linker-folder-disabled-in-the/m-p/1246231#M7332</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2021-03-16T08:22:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design studio - Debugger and linker folder disabled in the project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-studio-Debugger-and-linker-folder-disabled-in-the/m-p/1846004#M12147</link>
      <description>&lt;P&gt;I add new folder to project and my folder also be disabled like that. How can I resolve this problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Apr 2024 09:38:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-Design-studio-Debugger-and-linker-folder-disabled-in-the/m-p/1846004#M12147</guid>
      <dc:creator>HungNguyen1001</dc:creator>
      <dc:date>2024-04-12T09:38:46Z</dc:date>
    </item>
  </channel>
</rss>