<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: fenv - undefined reference to `__FSL__ieee_status'</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/fenv-undefined-reference-to-FSL-ieee-status/m-p/1227156#M7226</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;sorry for delay.I went through the EWL C library, and&amp;nbsp; the library is compiled in way, that&amp;nbsp; &amp;nbsp;_FSL_ieee_status (and other HW float point stuff) is implemented by user application.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 05 Feb 2021 13:38:26 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2021-02-05T13:38:26Z</dc:date>
    <item>
      <title>fenv - undefined reference to `__FSL__ieee_status'</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/fenv-undefined-reference-to-FSL-ieee-status/m-p/1221145#M7195</link>
      <description>&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;I try to use standard C99 fesetround function to change Cortex-M4F (S32K144) rounding mode.&lt;/P&gt;&lt;P&gt;Unfortunately, the linker return the following errors :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;S32DS/arm_ewl2/EWL_C/src/arm/fenv_arm.c:234: undefined reference to `__FSL__ieee_status'
S32DS/arm_ewl2/EWL_C/src/arm/fenv_arm.c:235: undefined reference to `__FSL__ieee_status'&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did anyone see that already ?&lt;/P&gt;&lt;P&gt;My project is configured to use C99 standard in Properties-&amp;gt;C/C++Build-&amp;gt;Settings-&amp;gt;Standard S32DS C Compiler-&amp;gt;Dialect&lt;/P&gt;&lt;P&gt;I use s32DS 2018.R1.&lt;/P&gt;&lt;P&gt;Thanks by advance !&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jan 2021 09:12:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/fenv-undefined-reference-to-FSL-ieee-status/m-p/1221145#M7195</guid>
      <dc:creator>agardiol</dc:creator>
      <dc:date>2021-01-26T09:12:39Z</dc:date>
    </item>
    <item>
      <title>Re: fenv - undefined reference to `__FSL__ieee_status'</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/fenv-undefined-reference-to-FSL-ieee-status/m-p/1227156#M7226</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;sorry for delay.I went through the EWL C library, and&amp;nbsp; the library is compiled in way, that&amp;nbsp; &amp;nbsp;_FSL_ieee_status (and other HW float point stuff) is implemented by user application.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Feb 2021 13:38:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/fenv-undefined-reference-to-FSL-ieee-status/m-p/1227156#M7226</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2021-02-05T13:38:26Z</dc:date>
    </item>
  </channel>
</rss>