<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to create and use static library in S32DS in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-create-and-use-static-library-in-S32DS/m-p/1167868#M6894</link>
    <description>&lt;P&gt;Hi Nxp!&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN&gt;Recently, I encountered a problem when using S32DS_v2.2 to compile my project with other static library. I refer to guidance of HOWTO:Add a static library file into S32DS GCC projectiles&lt;FONT size="4" color="#ba0087"&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Add-a-static-library-file-into-S32DS-GCC-project/ta-p/1110308" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Add-a-static-library-file-into-S32DS-GCC-project/ta-p/1110308&lt;/A&gt;&lt;/FONT&gt;; I think I have no problem setting it up, but the following error occurs during compilation.&lt;/SPAN&gt; &lt;SPAN&gt;Can you help find the cause of the problem?&lt;/SPAN&gt; &lt;SPAN&gt;thank you very much&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Description Resource Path Location Type&lt;BR /&gt;Ld error: can_pal_s32k142.elf uses VFP register arguments, E:/DeskTop/1234/S32DS/testFunction1/Debug\libtestFunction1.a(mylibrary.o) does not C/C++ Problem&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 15 Oct 2020 01:33:50 GMT</pubDate>
    <dc:creator>1450132053</dc:creator>
    <dc:date>2020-10-15T01:33:50Z</dc:date>
    <item>
      <title>How to create and use static library in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-create-and-use-static-library-in-S32DS/m-p/1167868#M6894</link>
      <description>&lt;P&gt;Hi Nxp!&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN&gt;Recently, I encountered a problem when using S32DS_v2.2 to compile my project with other static library. I refer to guidance of HOWTO:Add a static library file into S32DS GCC projectiles&lt;FONT size="4" color="#ba0087"&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Add-a-static-library-file-into-S32DS-GCC-project/ta-p/1110308" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Add-a-static-library-file-into-S32DS-GCC-project/ta-p/1110308&lt;/A&gt;&lt;/FONT&gt;; I think I have no problem setting it up, but the following error occurs during compilation.&lt;/SPAN&gt; &lt;SPAN&gt;Can you help find the cause of the problem?&lt;/SPAN&gt; &lt;SPAN&gt;thank you very much&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Description Resource Path Location Type&lt;BR /&gt;Ld error: can_pal_s32k142.elf uses VFP register arguments, E:/DeskTop/1234/S32DS/testFunction1/Debug\libtestFunction1.a(mylibrary.o) does not C/C++ Problem&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Oct 2020 01:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-create-and-use-static-library-in-S32DS/m-p/1167868#M6894</guid>
      <dc:creator>1450132053</dc:creator>
      <dc:date>2020-10-15T01:33:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to create and use static library in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-create-and-use-static-library-in-S32DS/m-p/1168212#M6895</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;your issue is probably caused by different compilator settings for library and executable. You can find more details for example here -&amp;nbsp;&lt;A href="https://stackoverflow.com/questions/9753749/arm-compilation-error-vfp-registers-used-by-executable-not-object-file" target="_blank"&gt;https://stackoverflow.com/questions/9753749/arm-compilation-error-vfp-registers-used-by-executable-not-object-file&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The float point settings you can find in project properties:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jiri_kral_0-1602762241495.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/127521i277CA0E7EB975DC9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jiri_kral_0-1602762241495.png" alt="jiri_kral_0-1602762241495.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jiri&lt;/P&gt;</description>
      <pubDate>Thu, 15 Oct 2020 11:47:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-create-and-use-static-library-in-S32DS/m-p/1168212#M6895</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2020-10-15T11:47:01Z</dc:date>
    </item>
    <item>
      <title>Re: How to create and use static library in S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-create-and-use-static-library-in-S32DS/m-p/1848572#M12157</link>
      <description>Hello, I follow the normal methods of generating and adding static libraries. When I added static libraries, the following error appeared. May I ask what caused it?&lt;BR /&gt;&lt;BR /&gt;Building target: BMS_2_2.elf&lt;BR /&gt;Invoking: Standard S32DS C Linker&lt;BR /&gt;arm-none-eabi-gcc -o "BMS_2_2.elf" "@BMS_2_2.args"&lt;BR /&gt;arm-none-eabi-gcc.exe: error: : No such file or directory&lt;BR /&gt;make: *** [makefile:86: BMS_2_2.elf] Error 1&lt;BR /&gt;"make -j16 all" terminated with exit code 2. Build might be incomplete.</description>
      <pubDate>Wed, 17 Apr 2024 01:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-create-and-use-static-library-in-S32DS/m-p/1848572#M12157</guid>
      <dc:creator>NXP2</dc:creator>
      <dc:date>2024-04-17T01:34:12Z</dc:date>
    </item>
  </channel>
</rss>