<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: S32 download program can run in debug and cannot be run offline</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1166679#M6883</link>
    <description>&lt;P&gt;I can see what happened because the program can run normally in the debug state, but after exiting debug and resetting it, it cannot work or even change the state of a G P I O&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;ARM ：S 9 K E A Z 128&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;DEBUG ：s e g g e r J-Link Debugging&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 13 Oct 2020 10:58:41 GMT</pubDate>
    <dc:creator>Alien浩文</dc:creator>
    <dc:date>2020-10-13T10:58:41Z</dc:date>
    <item>
      <title>S32 download program can run in debug and cannot be run offline</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1166429#M6881</link>
      <description>&lt;P&gt;使用S32的Debug功能可以在开发板上运行程序，功能正常，但是断开JTAG连接后，重新供电，程序不会运行。使用J-Flash下载程序，也无法运行。请问如何解决？&lt;/P&gt;&lt;P&gt;Google Translate:&lt;/P&gt;&lt;P&gt;The Debug function of S32 can be used to run the program on the development board, and the function is normal. However, after the JTAG connection is disconnected and the power is supplied again, the program will not run. Using J-Flash to download the program can not run.How to solve this problem?&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 02:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1166429#M6881</guid>
      <dc:creator>Alien浩文</dc:creator>
      <dc:date>2020-10-13T02:56:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32 download program can run in debug and cannot be run offline</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1166674#M6882</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;are you able attach into running program and see what's going on? Anyway, what's your MCU?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jiri_kral_0-1602585539047.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/127325i0BA6F695327B0AB6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jiri_kral_0-1602585539047.png" alt="jiri_kral_0-1602585539047.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jiri_kral_0-1602585539047.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 10:41:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1166674#M6882</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2020-10-13T10:41:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32 download program can run in debug and cannot be run offline</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1166679#M6883</link>
      <description>&lt;P&gt;I can see what happened because the program can run normally in the debug state, but after exiting debug and resetting it, it cannot work or even change the state of a G P I O&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;ARM ：S 9 K E A Z 128&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;DEBUG ：s e g g e r J-Link Debugging&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 10:58:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1166679#M6883</guid>
      <dc:creator>Alien浩文</dc:creator>
      <dc:date>2020-10-13T10:58:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32 download program can run in debug and cannot be run offline</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1166691#M6884</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;what about attach to running target? At last you can see on which address is program stuck - some unhandled interrupt or exception?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 11:32:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1166691#M6884</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2020-10-13T11:32:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32 download program can run in debug and cannot be run offline</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1472834#M8688</link>
      <description>&lt;P&gt;hello 浩文&amp;nbsp;&lt;/P&gt;&lt;P&gt;我遇到了和你同样的问题 请问你解决了吗？&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jun 2022 10:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1472834#M8688</guid>
      <dc:creator>xuewenchen</dc:creator>
      <dc:date>2022-06-13T10:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32 download program can run in debug and cannot be run offline</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1713874#M10895</link>
      <description>&lt;P&gt;Hi Alien!&lt;/P&gt;&lt;P&gt;Sorry for the late response. I had the same issue and I found out that the problem is the NMI interrupt which is sometimes triggered after reset in standalone mode but not in debug mode with probe connected. The walkaround I've used is to simply add disable NMI interrupt instruction in NMI interrupt rutine itself (in my case it is located in a file "events.c":&lt;/P&gt;&lt;DIV&gt;void Cpu_OnNMI(void)&lt;/DIV&gt;&lt;DIV&gt;{&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;SIM_SOPT0=SIM_SOPT0 &amp;amp; ~SIM_SOPT0_NMIE_MASK; // here you disable NMI interrupt&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;}&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Best regards,&lt;/DIV&gt;&lt;DIV&gt;Florijan&lt;/DIV&gt;</description>
      <pubDate>Wed, 30 Aug 2023 08:34:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-download-program-can-run-in-debug-and-cannot-be-run-offline/m-p/1713874#M10895</guid>
      <dc:creator>Florijan</dc:creator>
      <dc:date>2023-08-30T08:34:06Z</dc:date>
    </item>
  </channel>
</rss>