<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Update S32 Design Studio for Arm to SDK RTM 4.0 in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Update-S32-Design-Studio-for-Arm-to-SDK-RTM-4-0/m-p/1162799#M6851</link>
    <description>&lt;P&gt;Hi Revinio,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;you are right - SDK S32K1XX RTM 4.0.0 is for S32DS v3.3.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jiri&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 05 Oct 2020 08:23:20 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2020-10-05T08:23:20Z</dc:date>
    <item>
      <title>Update S32 Design Studio for Arm to SDK RTM 4.0</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Update-S32-Design-Studio-for-Arm-to-SDK-RTM-4-0/m-p/1162053#M6847</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I try to use the SDK RTM 4.0 in the S32 Design Studio for Arm V2.2 because of the "Processor Expert CAN ISR bug". But I don't manage to include it. For example I removed the SDK 3.0 und installed the SDK 4.0 .exe. The path variable should be added automaticly but it does not. When I try to add the SDK with SDK Management, there is no "sources.xml" to add. In the foldes its named "sources_S32K1xx_SDK.xml". I think that is the reason why i can't add it. If i rename it to "sources.xml" it does not work.&lt;/P&gt;&lt;P&gt;Do you have an idea how to fix this problem?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Revinio&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;EDIT:&lt;/P&gt;&lt;P&gt;It seems, that SDK RTM V4.0 is not compatible at the moment with Design Studio for Arm 2.2.&lt;/P&gt;&lt;P&gt;I downloaded Design Studio For S32 Platform 3.3 and now I can use SDK RTM V4.0.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Revinio&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 03 Oct 2020 22:53:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Update-S32-Design-Studio-for-Arm-to-SDK-RTM-4-0/m-p/1162053#M6847</guid>
      <dc:creator>Revinio</dc:creator>
      <dc:date>2020-10-03T22:53:12Z</dc:date>
    </item>
    <item>
      <title>Re: Update S32 Design Studio for Arm to SDK RTM 4.0</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Update-S32-Design-Studio-for-Arm-to-SDK-RTM-4-0/m-p/1162799#M6851</link>
      <description>&lt;P&gt;Hi Revinio,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;you are right - SDK S32K1XX RTM 4.0.0 is for S32DS v3.3.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jiri&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Oct 2020 08:23:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Update-S32-Design-Studio-for-Arm-to-SDK-RTM-4-0/m-p/1162799#M6851</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2020-10-05T08:23:20Z</dc:date>
    </item>
  </channel>
</rss>