<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32DS V2018.R1 Breakpoints Stopped Working in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V2018-R1-Breakpoints-Stopped-Working/m-p/1146160#M6762</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yesterday breakpoints stopped working to me as wall. No matter which connection, OpenSDA or Multilink, no matter which project, flash or&amp;nbsp;RAM,&amp;nbsp;all breakpoints bullets set in editor windows&amp;nbsp;are crossed and don't work though are enabled.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Deleting workspace .metadata folder, then and re-adding existing projects fixes the issue. Would be nice to know better solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Edward&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 04 Sep 2020 07:01:04 GMT</pubDate>
    <dc:creator>kef2</dc:creator>
    <dc:date>2020-09-04T07:01:04Z</dc:date>
    <item>
      <title>S32DS V2018.R1 Breakpoints Stopped Working</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V2018-R1-Breakpoints-Stopped-Working/m-p/1048666#M6201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. I was using S32DS for ARM Version 2018.R1 Build 180815 with processor S32K116. I installed S32DS Version 2.2 and saw a message that it was updating my pemicro FX debugger. Did that actually update the firmware in the pemicro FX? Is there a method to undo this? I also noticed that the debugger no longer deactivates the watchdog. I uninstalled V2.2 and went back to V2018.R1. Now V2018.R1 doesn't stop on breakpoints that I set. It initially stops inside main(), and stops when I click "Suspend". Using c:\nxp\s32ds_arm_v2018.r1\drivers\pedrivers_install.exe I reinstalled c:\pemicro\pedrivers\supportfiles\Drivers_12_7_0, but this made no difference. Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2020 12:53:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V2018-R1-Breakpoints-Stopped-Working/m-p/1048666#M6201</guid>
      <dc:creator>lleviton</dc:creator>
      <dc:date>2020-04-02T12:53:52Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS V2018.R1 Breakpoints Stopped Working</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V2018-R1-Breakpoints-Stopped-Working/m-p/1146160#M6762</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yesterday breakpoints stopped working to me as wall. No matter which connection, OpenSDA or Multilink, no matter which project, flash or&amp;nbsp;RAM,&amp;nbsp;all breakpoints bullets set in editor windows&amp;nbsp;are crossed and don't work though are enabled.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Deleting workspace .metadata folder, then and re-adding existing projects fixes the issue. Would be nice to know better solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Edward&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Sep 2020 07:01:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V2018-R1-Breakpoints-Stopped-Working/m-p/1146160#M6762</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2020-09-04T07:01:04Z</dc:date>
    </item>
  </channel>
</rss>