<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Breakpoints fail after NMI in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Breakpoints-fail-after-NMI/m-p/1086474#M6594</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a board with an FS45 SBC that generates an NMI on a problem to an S32K144, in a similar arrangement to the NewTec BMS reference design. As I apply power to 5V peripherals, it causes a momentary power dip, which triggers the SBC and generates an NMI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The NMI is handled OK, and normal code operation is then resumed and the program continues to execute correctly, with all interrupts etc OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However while breakpoints function up until this point, they cease to operate after the NMI, until the next time the code is restarted in the debugger.&lt;/P&gt;&lt;P&gt;On occasions - under less clear circumstances - sometimes get the 'failed to write breakpoints' error as well as previously reported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SDK S32 Design Studio S32K1xx RTM SDK 3.0.3 Patch for SDK 3.0.0 1.0.0.202005140959&lt;/P&gt;&lt;P&gt;S32DS 2.0.0.202001161704&lt;/P&gt;&lt;P&gt;PE Micro debugger.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 May 2020 18:05:07 GMT</pubDate>
    <dc:creator>mnewton</dc:creator>
    <dc:date>2020-05-28T18:05:07Z</dc:date>
    <item>
      <title>Breakpoints fail after NMI</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Breakpoints-fail-after-NMI/m-p/1086474#M6594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a board with an FS45 SBC that generates an NMI on a problem to an S32K144, in a similar arrangement to the NewTec BMS reference design. As I apply power to 5V peripherals, it causes a momentary power dip, which triggers the SBC and generates an NMI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The NMI is handled OK, and normal code operation is then resumed and the program continues to execute correctly, with all interrupts etc OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However while breakpoints function up until this point, they cease to operate after the NMI, until the next time the code is restarted in the debugger.&lt;/P&gt;&lt;P&gt;On occasions - under less clear circumstances - sometimes get the 'failed to write breakpoints' error as well as previously reported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SDK S32 Design Studio S32K1xx RTM SDK 3.0.3 Patch for SDK 3.0.0 1.0.0.202005140959&lt;/P&gt;&lt;P&gt;S32DS 2.0.0.202001161704&lt;/P&gt;&lt;P&gt;PE Micro debugger.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2020 18:05:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Breakpoints-fail-after-NMI/m-p/1086474#M6594</guid>
      <dc:creator>mnewton</dc:creator>
      <dc:date>2020-05-28T18:05:07Z</dc:date>
    </item>
  </channel>
</rss>