<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Multiple debug on one PC in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Multiple-debug-on-one-PC/m-p/1074154#M6468</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Deepak,&lt;/P&gt;&lt;P&gt;It is possible to run two instances of S32 Design Studio under Window environment.&lt;/P&gt;&lt;P&gt;The limitation is you cannot open the same workspace twice. Therefore for the second instance of S32DS must open a different workspace with project you want to works with.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you intend to debug both project at the same time you should also adjust GDB server ports + select a different P&amp;amp;E Interface instance.&lt;/P&gt;&lt;P&gt;e.g. one instance uses default GDBMI + Server port and the second instance uses 6324, 7324 ports (if these are not use by another program)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109757i1776371435775440/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Aug 2020 10:49:52 GMT</pubDate>
    <dc:creator>stanish</dc:creator>
    <dc:date>2020-08-07T10:49:52Z</dc:date>
    <item>
      <title>Multiple debug on one PC</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Multiple-debug-on-one-PC/m-p/1074153#M6467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using IDE S32 Design Studio power architecture V2.1 on MS-Windows 10 OS and DEVKIT MPC5748G development board for debugging.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to debug two&amp;nbsp;&lt;SPAN&gt;DEVKIT MPC5748G at the same time on one PC (Using two USB ports) will it be possible?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In case if it is not possible then will it work on two OS e.g. MS-Windows 10 and Linux if my PC has both OS?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I tried with MS-Windows 10 but when I try to debug 2nd board then first board is terminating debugging.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2020 09:42:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Multiple-debug-on-one-PC/m-p/1074153#M6467</guid>
      <dc:creator>Deepak1</dc:creator>
      <dc:date>2020-08-07T09:42:05Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple debug on one PC</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Multiple-debug-on-one-PC/m-p/1074154#M6468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Deepak,&lt;/P&gt;&lt;P&gt;It is possible to run two instances of S32 Design Studio under Window environment.&lt;/P&gt;&lt;P&gt;The limitation is you cannot open the same workspace twice. Therefore for the second instance of S32DS must open a different workspace with project you want to works with.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you intend to debug both project at the same time you should also adjust GDB server ports + select a different P&amp;amp;E Interface instance.&lt;/P&gt;&lt;P&gt;e.g. one instance uses default GDBMI + Server port and the second instance uses 6324, 7324 ports (if these are not use by another program)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109757i1776371435775440/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2020 10:49:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Multiple-debug-on-one-PC/m-p/1074154#M6468</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2020-08-07T10:49:52Z</dc:date>
    </item>
  </channel>
</rss>