<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックS32G serial boot</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32G-serial-boot/m-p/1065132#M6348</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am a new user of S32DS and S32G-VNP-EVB, which i am trying to boot using serial boot. I have set the BMODE pins accordingly. and have tried to load a U-boot binary supplied for booting from SDcard using a terminal program (Hterm). As a result, a trace of received bytes on the port is seen I cannot understand what they represent. I have also set some blob images from a DiagnosticTest_CM7 project. I also receive a trace of bytes that I cannot intepret. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are my questions:&lt;/P&gt;&lt;P&gt;1. Is there a USB Loader(for Windows) that can be used to directly load the U-Boot file on to the board ?&lt;/P&gt;&lt;P&gt;2. What alternative bootloader can be used or that could be specific to the s32G serial boot?&lt;/P&gt;&lt;P&gt;3. How can I create a serial image in S32DS? &lt;/P&gt;&lt;P&gt;4. Are these received bytes to be expected? Or what is to be expected before and after serial boot has successfully completed?&lt;/P&gt;&lt;P&gt;5. If there is no available bootloader, where do I start on designing my own bootloader?&lt;/P&gt;&lt;P&gt;6. How can I load an image onto board from S32DS on serial connection?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Aug 2020 08:27:07 GMT</pubDate>
    <dc:creator>samantham</dc:creator>
    <dc:date>2020-08-25T08:27:07Z</dc:date>
    <item>
      <title>S32G serial boot</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32G-serial-boot/m-p/1065132#M6348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am a new user of S32DS and S32G-VNP-EVB, which i am trying to boot using serial boot. I have set the BMODE pins accordingly. and have tried to load a U-boot binary supplied for booting from SDcard using a terminal program (Hterm). As a result, a trace of received bytes on the port is seen I cannot understand what they represent. I have also set some blob images from a DiagnosticTest_CM7 project. I also receive a trace of bytes that I cannot intepret. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are my questions:&lt;/P&gt;&lt;P&gt;1. Is there a USB Loader(for Windows) that can be used to directly load the U-Boot file on to the board ?&lt;/P&gt;&lt;P&gt;2. What alternative bootloader can be used or that could be specific to the s32G serial boot?&lt;/P&gt;&lt;P&gt;3. How can I create a serial image in S32DS? &lt;/P&gt;&lt;P&gt;4. Are these received bytes to be expected? Or what is to be expected before and after serial boot has successfully completed?&lt;/P&gt;&lt;P&gt;5. If there is no available bootloader, where do I start on designing my own bootloader?&lt;/P&gt;&lt;P&gt;6. How can I load an image onto board from S32DS on serial connection?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Aug 2020 08:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32G-serial-boot/m-p/1065132#M6348</guid>
      <dc:creator>samantham</dc:creator>
      <dc:date>2020-08-25T08:27:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32G serial boot</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32G-serial-boot/m-p/1242800#M7314</link>
      <description>&lt;P&gt;Dears, any of progress on that? Please would you share with me on how to resolve those?&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 00:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32G-serial-boot/m-p/1242800#M7314</guid>
      <dc:creator>unixboy99</dc:creator>
      <dc:date>2021-03-10T00:19:10Z</dc:date>
    </item>
    <item>
      <title>Re: S32G serial boot</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32G-serial-boot/m-p/1243691#M7316</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/156423"&gt;@samantham&lt;/a&gt;&amp;nbsp;,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184294"&gt;@unixboy99&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;The tool we provide for you to load the BLOB image to the&amp;nbsp;&lt;SPAN&gt;S32G-VNP-EVB is the S32 Flash Tool. It is included with the S32 Design Studio install.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For the S32 Design Studio v3.4, it is located at:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;C:\NXP\S32DS.3.4\S32DS\tools\S32FlashTool&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There is both GUI and command line versions.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;A user guide is provided which details how it should be used.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The included document shows how to create the BLOB image:&lt;BR /&gt;"C:\NXP\S32DS.3.4\S32DS\help\resources\howto\g2dev\HOWTO_Use_IVT_Tool_To_Create_A_Blob_Image_S32G274A_EVB.pdf"&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can also locate this document from the Help-&amp;gt;Getting Started page.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There is complete instructions for creating BLOBs, flashing to the target, etc included in the Getting Started doc:&lt;BR /&gt;"C:\NXP\S32DS.3.4\S32DS\help\resources\howto\g2dev\Getting_started_with_S32G_S32DS.pdf"&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;It has many important details, highly recommend you look through it.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 23:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32G-serial-boot/m-p/1243691#M7316</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2021-03-10T23:29:52Z</dc:date>
    </item>
    <item>
      <title>Re: S32G serial boot</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32G-serial-boot/m-p/1244308#M7317</link>
      <description>&lt;P&gt;Thank you Mike.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Mar 2021 17:24:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32G-serial-boot/m-p/1244308#M7317</guid>
      <dc:creator>unixboy99</dc:creator>
      <dc:date>2021-03-11T17:24:05Z</dc:date>
    </item>
  </channel>
</rss>