<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Why placing .noinit section in Linker messes up the RAM vector table? in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Why-placing-noinit-section-in-Linker-messes-up-the-RAM-vector/m-p/1059381#M6290</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having a problem after adding a `.noinit` section in Linker script as mentioned in this &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-342136"&gt;Example&lt;/A&gt;, after adding it variables in this section dont get init as intended but as a consequence i realized that the ADC0 interrupt was not being triggered anymore after triggering a conversion (it works if the .noinit section is removed) , after deeper analysis i realized that the the interrupt actually is fired but the DMA7 handler is being called instead, so i thought that the VTOR register might hold a wrong address of the offset-ed RAM vector table, i checked it and it hold the correct address (as per the .map file) .&lt;/P&gt;&lt;P&gt;So i believe that the RAM vector table is offset-ed/messed up in a way by this section (as this section is placed right before the RAM interrupts table).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i would appreciate any help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am using S32K146&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;s32k146‌ s32k146 boot‌ #s32&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Apr 2020 11:10:10 GMT</pubDate>
    <dc:creator>islam1</dc:creator>
    <dc:date>2020-04-21T11:10:10Z</dc:date>
    <item>
      <title>Why placing .noinit section in Linker messes up the RAM vector table?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Why-placing-noinit-section-in-Linker-messes-up-the-RAM-vector/m-p/1059381#M6290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having a problem after adding a `.noinit` section in Linker script as mentioned in this &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-342136"&gt;Example&lt;/A&gt;, after adding it variables in this section dont get init as intended but as a consequence i realized that the ADC0 interrupt was not being triggered anymore after triggering a conversion (it works if the .noinit section is removed) , after deeper analysis i realized that the the interrupt actually is fired but the DMA7 handler is being called instead, so i thought that the VTOR register might hold a wrong address of the offset-ed RAM vector table, i checked it and it hold the correct address (as per the .map file) .&lt;/P&gt;&lt;P&gt;So i believe that the RAM vector table is offset-ed/messed up in a way by this section (as this section is placed right before the RAM interrupts table).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i would appreciate any help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am using S32K146&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;s32k146‌ s32k146 boot‌ #s32&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2020 11:10:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Why-placing-noinit-section-in-Linker-messes-up-the-RAM-vector/m-p/1059381#M6290</guid>
      <dc:creator>islam1</dc:creator>
      <dc:date>2020-04-21T11:10:10Z</dc:date>
    </item>
    <item>
      <title>Re: Why placing .noinit section in Linker messes up the RAM vector table?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Why-placing-noinit-section-in-Linker-messes-up-the-RAM-vector/m-p/1059382#M6291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for report. There is a bug in the example - Vector table needs to be put on address aligned to 0x400. I'm going to fix the example. Quick fix:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42087i2F96977B8780AAEF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2020 11:23:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Why-placing-noinit-section-in-Linker-messes-up-the-RAM-vector/m-p/1059382#M6291</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2020-04-22T11:23:06Z</dc:date>
    </item>
  </channel>
</rss>